Memory header for copy functions. More...
Go to the source code of this file.
Macros | |
| #define | MCUXCLMEMORY_FP_MEMORY_COPY(pTarget, pSource, byteLen) |
| Helper macro to call mcuxClMemory_copy with flow protection. | |
| #define | MCUXCLMEMORY_FP_MEMORY_COPY_WITH_BUFF(pTarget, pSource, byteLen, buffLen) |
| Helper macro to call mcuxClMemory_copy with flow protection with buffer. | |
Functions | |
| void | mcuxClMemory_copy (uint8_t *pDst, uint8_t const *pSrc, size_t length, size_t bufLength) |
| Copies a memory buffer to another location. | |
Memory header for copy functions.
This header exposes functions that enable using memory copy function.