MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClMemory_Types.h
Go to the documentation of this file.
1/*--------------------------------------------------------------------------*/
2/* Copyright 2020-2021, 2023 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
17
24
25#ifndef MCUXCLMEMORY_TYPES_H
26#define MCUXCLMEMORY_TYPES_H
27
28#include <stdint.h>
29#include <stddef.h>
30#include <mcuxClConfig.h> // Exported features flags header
33
34/**********************************************
35 * MACROS
36 **********************************************/
43#define MCUXCLMEMORY_API extern
44
48
49/**********************************************
50 * TYPEDEFS
51 **********************************************/
57typedef uint32_t mcuxClMemory_Status_t;
58
63
64#endif /* #MCUXCLMEMORY_TYPES_H */
65
Definition of function identifiers for the flow protection mechanism.
Provides the API for the CSSL flow protection mechanism.
mcuxClMemory_Status_t mcuxClMemory_Status_Protected_t
Deprecated type for error codes used by code-flow protected mcuxClMemory component functions.
Definition mcuxClMemory_Types.h:62
uint32_t mcuxClMemory_Status_t
Type for error codes of mcuxClMemory component functions.
Definition mcuxClMemory_Types.h:57
#define MCUX_CSSL_FP_PROTECTED_TYPE(resultType)
Based on a given base type, builds a return type with flow protection.
Definition mcuxCsslFlowProtection.h:138