MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClPadding_Types.h
Go to the documentation of this file.
1/*--------------------------------------------------------------------------*/
2/* Copyright 2022 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
18
19
20#ifndef MCUXCLPADDING_TYPES_H_
21#define MCUXCLPADDING_TYPES_H_
22
23#include <stdint.h>
24#include <mcuxClConfig.h> // Exported features flags header
25
26
27#ifdef __cplusplus
28extern "C" {
29#endif
30
37
38
45typedef uint32_t mcuxClPadding_Status_t;
46
48
49#ifdef __cplusplus
50} /* extern "C" */
51#endif
52
53#endif /* MCUXCLPADDING_TYPES_H_ */
uint32_t mcuxClPadding_Status_t
Padding status code.
Definition mcuxClPadding_Types.h:45