MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClRandomModes_Functions_TestMode.h
1/*--------------------------------------------------------------------------*/
2/* Copyright 2021-2023 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
14#ifndef MCUXCLRANDOM_FUNCTIONS_TESTMODE_H_
15#define MCUXCLRANDOM_FUNCTIONS_TESTMODE_H_
16
17#include <mcuxClConfig.h> // Exported features flags header
18
19#include <mcuxClSession.h>
20#include <mcuxClRandom_Types.h>
21
22#ifdef __cplusplus
23extern "C" {
24#endif
25
32
46// TODO: Create defines for custom seed sizes using object size filler
50 mcuxClRandom_Mode_t normalMode,
51 const uint32_t * const pCustomSeed
52);
53
66 const uint32_t * const pCustomSeed
67);
68
70
71#ifdef __cplusplus
72} /* extern "C" */
73#endif
74
75#endif /* MCUXCLRANDOM_FUNCTIONS_TESTMODE_H_ */
Type definitions of mcuxClRandom component.
Top-level include file for the mcuxClSession component.
const mcuxClRandom_ModeDescriptor_t * mcuxClRandom_Mode_t
Random data generation mode/algorithm type.
Definition mcuxClRandom_Types.h:94
uint32_t mcuxClRandom_Status_t
Type for status codes of mcuxClRandom component functions.
Definition mcuxClRandom_Types.h:48
struct mcuxClRandom_ModeDescriptor mcuxClRandom_ModeDescriptor_t
Random data generation mode/algorithm descriptor type.
Definition mcuxClRandom_Types.h:87
mcuxClRandom_Status_t mcuxClRandomModes_createTestFromNormalMode(mcuxClRandom_ModeDescriptor_t *pTestMode, mcuxClRandom_Mode_t normalMode, const uint32_t *const pCustomSeed)
This function creates a TEST_MODE descriptor from an existing NORMAL_MODE one.
mcuxClRandom_Status_t mcuxClRandomModes_updateEntropyInput(mcuxClRandom_ModeDescriptor_t *pTestMode, const uint32_t *const pCustomSeed)
This function updates the custom seed pointer in a TEST_MODE descriptor.
#define MCUX_CSSL_FP_FUNCTION_DECL(...)
Declaration of a flow protected function.
Definition mcuxCsslFlowProtection.h:166
#define MCUX_CSSL_FP_PROTECTED_TYPE(resultType)
Based on a given base type, builds a return type with flow protection.
Definition mcuxCsslFlowProtection.h:138