20#ifndef MCUXCLRESOURCE_FUNCTIONS_H_
21#define MCUXCLRESOURCE_FUNCTIONS_H_
23#include <mcuxClCore_Platform.h>
86 mcuxClResource_Interrupt_t interrupt
Definition of function identifiers for the flow protection mechanism.
Type definitions for the mcuxClResource component.
Provides the API for the CSSL flow protection mechanism.
mcuxClResource_Status_t mcuxClResource_init(mcuxClResource_Context_t *pResourceCtx, mcuxClResource_MutexAcquire_Callback_t pMutexAcquire, mcuxClResource_MutexRelease_Callback_t pMutexRelease)
Resource context initialization function.
mcuxClResource_Status_t mcuxClResource_handle_interrupt(const mcuxClResource_Context_t *pResourceCtx, mcuxClResource_Interrupt_t interrupt)
Resource interrupt handler.
struct mcuxClResource_Context mcuxClResource_Context_t
Resource context type.
Definition mcuxClResource_Types.h:47
uint32_t(* mcuxClResource_MutexRelease_Callback_t)(uint32_t value)
Callback type for releasing a mutex.
Definition mcuxClResource_Types.h:57
uint32_t(* mcuxClResource_MutexAcquire_Callback_t)(uint32_t value)
Callback type for acquiring a mutex.
Definition mcuxClResource_Types.h:52
uint32_t mcuxClResource_Status_t
Type for mcuxClResource status codes.
Definition mcuxClResource_Types.h:42
#define MCUX_CSSL_FP_FUNCTION_DECL(...)
Declaration of a flow protected function.
Definition mcuxCsslFlowProtection.h:166
#define MCUX_CSSL_FP_PROTECTED_TYPE(resultType)
Based on a given base type, builds a return type with flow protection.
Definition mcuxCsslFlowProtection.h:138