MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClRsa.h
Go to the documentation of this file.
1/*--------------------------------------------------------------------------*/
2/* Copyright 2020-2021, 2024, 2026 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
66
67#ifndef MCUXCLRSA_H_
68#define MCUXCLRSA_H_
69
70#include <mcuxClConfig.h> // Exported features flags header
71#include <mcuxClRsa_Functions.h>
73#include <mcuxClRsa_Types.h>
74#include <mcuxClRsa_KeyTypes.h>
75#include <mcuxClRsa_ModeConstructors.h>
76#endif /* MCUXCLRSA_H_ */
Top-level API of the mcuxClRsa component.
Definition of supported key types in mcuxClRsa component, see also mcuxClKey component.
Type definitions for the mcuxClRsa component.
Defines the memory consumption for the mcuxClRsa component.