MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClRsa_Functions.h
Go to the documentation of this file.
1/*--------------------------------------------------------------------------*/
2/* Copyright 2020-2024 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
18
19#ifndef MCUXCLRSA_FUNCTIONS_H_
20#define MCUXCLRSA_FUNCTIONS_H_
21
22#include <mcuxClConfig.h> // Exported features flags header
23#include <mcuxClSession.h>
26#include <mcuxClRsa_Types.h>
27#include <mcuxClBuffer.h>
28
29#ifdef __cplusplus
30extern "C" {
31#endif
32
39
40 /* mcuxClRsa_Functions */
44
45#ifdef __cplusplus
46} /* extern "C" */
47#endif
48
49#endif /* MCUXCLRSA_FUNCTIONS_H_ */
50
Top-level include file for the mcuxClBuffer component.
Definition of function identifiers for the flow protection mechanism.
Type definitions for the mcuxClRsa component.
Top-level include file for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.