MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClSgi_Types.h
Go to the documentation of this file.
1/*--------------------------------------------------------------------------*/
2/* Copyright 2023 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
18
19#ifndef MCUXCLSGI_TYPES_H_
20#define MCUXCLSGI_TYPES_H_
21
22#include <mcuxClCore_Platform.h>
24
25#ifdef __cplusplus
26extern "C" {
27#endif
28
35
42typedef uint32_t mcuxClSgi_Status_t;
43 /* mcuxClSgi_Types */
47
48#ifdef __cplusplus
49} /* extern "C" */
50#endif
51
52#endif /* MCUXCLSGI_TYPES_H_ */
Provides the API for the CSSL flow protection mechanism.
uint32_t mcuxClSgi_Status_t
SGI status code.
Definition mcuxClSgi_Types.h:42