MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxCl_clns.h
Go to the documentation of this file.
1
/*--------------------------------------------------------------------------*/
2
/* Copyright 2020 NXP */
3
/* */
4
/* NXP Confidential and Proprietary. This software is owned or controlled */
5
/* by NXP and may only be used strictly in accordance with the applicable */
6
/* license terms. By expressly accepting such terms or by downloading, */
7
/* installing, activating and/or otherwise using the software, you are */
8
/* agreeing that you have read, and that you agree to comply with and are */
9
/* bound by, such license terms. If you do not agree to be bound by the */
10
/* applicable license terms, then you may not retain, install, activate or */
11
/* otherwise use the software. */
12
/*--------------------------------------------------------------------------*/
13
16
17
#ifndef MCUXCL_CLNS_H_
18
#define MCUXCL_CLNS_H_
19
20
#include <mcuxClConfig.h>
// Exported features flags header
21
22
/**********************************************
23
* CONSTANTS
24
**********************************************/
25
26
#define MCUXCL_VERSION_MAX_SIZE ((size_t) 32U)
27
31
#define MCUXCL_VERSION "DCI_SDK_V4.0.0"
32
33
/**********************************************
34
* FUNCTIONS
35
**********************************************/
36
43
static
inline
char
const
*
mcuxCl_GetVersion
(
void
)
44
{
45
return
MCUXCL_VERSION
;
46
}
47
48
#endif
/* MCUXCL_CLNS_H_ */
MCUXCL_VERSION
#define MCUXCL_VERSION
String literal for the version string of CLNS release that this header is part of.
Definition
mcuxCl_clns.h:31
mcuxCl_GetVersion
static char const * mcuxCl_GetVersion(void)
Gets the CLNS version string that uniquely identifies this release of the CLNS.
Definition
mcuxCl_clns.h:43
mcuxCl_clns.h
Generated by
1.16.1