MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxCsslDataIntegrity.h File Reference

Provides the API for the CSSL data integrity mechanism. More...

Go to the source code of this file.

Macros

#define MCUX_CSSL_DI_CHECK_PASSED
 Positive comparison result value.
#define MCUX_CSSL_DI_CHECK_FAILED
 Negative comparison result value.
#define MCUX_CSSL_DI_INIT(backupValue)
 Backup of the current data integrity value, that will be checked later on with MCUX_CSSL_SC_CHECK.
#define MCUX_CSSL_DI_CHECK(reference)
 Comparison operation for the data integrity.
#define MCUX_CSSL_DI_CHECK_EXIT(id, reference, fail)
 Comparison operation for the data integrity.
#define MCUX_CSSL_DI_RECORD(identifier, value)
 Record the value for data integrity checking.
#define MCUX_CSSL_DI_EXPUNGE(identifier, value)
 Expunge the record for value.
#define MCUX_CSSL_DI_DONOTOPTIMIZE(val)
 Prevent compiler from pre-calculating the DI-protected variable value.

Detailed Description

Provides the API for the CSSL data integrity mechanism.