Configuration of the implementation for the data integrity mechanism. More...
Go to the source code of this file.
Macros | |
| #define | MCUX_CSSL_DI_USE_SECURE_COUNTER |
| If set to 1, use the data integrity mechanism implementation based on the CSSL secure counter mechanism. | |
| #define | MCUX_CSSL_DI_USE_NONE |
| If set to 1, do not use the data integrity mechanism. | |
Configuration of the implementation for the data integrity mechanism.