MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxCsslDataIntegrity_Impl.h
Go to the documentation of this file.
1/*--------------------------------------------------------------------------*/
2/* Copyright 2023 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
18
19#ifndef MCUXCSSLDATAINTEGRITY_IMPL_H_
20#define MCUXCSSLDATAINTEGRITY_IMPL_H_
21
22/* Include the configuration for the data integrity mechanism. */
24
25/* Include the selected implementation of the data integrity mechanism. */
26#if defined(MCUX_CSSL_DI_USE_SECURE_COUNTER) && (1 == MCUX_CSSL_DI_USE_SECURE_COUNTER)
28#elif defined(MCUX_CSSL_DI_USE_NONE) && (1 == MCUX_CSSL_DI_USE_NONE)
30#else
31 #error "No data integrity implementation found/configured."
32#endif
33
34#endif /* MCUXCSSLDATAINTEGRITY_IMPL_H_ */
Configuration of the implementation for the data integrity mechanism.
Implementation that disables the CSSL data integrity mechanism.
Implementation that enables the CSSL data integrity mechanism, based on secure counter.