Provides the API for the CSSL flow protection mechanism. More...
Go to the source code of this file.
Macros | |
| #define | MCUX_CSSL_FP_COUNTER_STMT(statement) |
| A statement which is only evaluated if a secure counter is used. | |
| #define | MCUX_CSSL_FP_PROTECTED_TYPE(resultType) |
| Based on a given base type, builds a return type with flow protection. | |
| #define | MCUX_CSSL_FP_FUNCTION_DECL(...) |
| Declaration of a flow protected function. | |
| #define | MCUX_CSSL_FP_FUNCTION_DEF(...) |
| Definition of a flow protected function. | |
| #define | MCUX_CSSL_FP_FUNCTION_POINTER(type, definition) |
| Definition of a flow protected function pointer. | |
| #define | MCUX_CSSL_FP_FUNCTION_ENTRY(...) |
| Flow protection handler for the function entry point. | |
| #define | MCUX_CSSL_FP_FUNCTION_EXIT(...) |
| Flow protection handler for the function exit point. | |
| #define | MCUX_CSSL_FP_FUNCTION_EXIT_WITH_CHECK(...) |
| Flow protection handler for the function exit point which includes an actual check of the code flow. | |
| #define | MCUX_CSSL_FP_FUNCTION_EXIT_VOID(...) |
Flow protection handler for the exit point of functions with the return type void. | |
| #define | MCUX_CSSL_FP_RESULT(...) |
Extract the result value from a protected return value. | |
| #define | MCUX_CSSL_FP_PROTECTION_TOKEN(return) |
Extract the protection token value from a protected return value. | |
| #define | MCUX_CSSL_FP_FUNCTION_CALL(...) |
| Call a flow protected function. | |
| #define | MCUX_CSSL_FP_FUNCTION_CALL_VOID(...) |
| Call a flow protected void function. | |
| #define | MCUX_CSSL_FP_FUNCTION_CALL_PROTECTED(...) |
| Call a flow protected function from unprotected code. | |
| #define | MCUX_CSSL_FP_FUNCTION_CALL_VOID_PROTECTED(...) |
| Call a flow protected void function from unprotected code. | |
| #define | MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...) |
| Call a flow protected function and check the protection token. | |
| #define | MCUX_CSSL_FP_FUNCTION_CALL_END(...) |
| End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN. | |
| #define | MCUX_CSSL_FP_FUNCTION_CALL_VOID_BEGIN(...) |
| Call a flow protected void function and check the protection token. | |
| #define | MCUX_CSSL_FP_FUNCTION_CALL_VOID_END(...) |
| End a void function call section started by MCUX_CSSL_FP_FUNCTION_CALL_VOID_BEGIN. | |
| #define | MCUX_CSSL_FP_FUNCTION_CALLED(...) |
| Expectation of a called function. | |
| #define | MCUX_CSSL_FP_FUNCTION_ENTERED(id) |
| Expectation implementation of an entered (but not exited) function. | |
| #define | MCUX_CSSL_FP_LOOP_DECL(id) |
| Declaration of a flow protected loop. | |
| #define | MCUX_CSSL_FP_LOOP_ITERATION(...) |
| Perform a loop iteration. | |
| #define | MCUX_CSSL_FP_LOOP_ITERATIONS(id, count) |
| Expected number of loop iterations. | |
| #define | MCUX_CSSL_FP_BRANCH_DECL(id) |
| Declaration of a flow protected branch. | |
| #define | MCUX_CSSL_FP_BRANCH_POSITIVE(...) |
| Positive scenario for a branch is executed. | |
| #define | MCUX_CSSL_FP_BRANCH_NEGATIVE(...) |
| Negative scenario of a branch is executed. | |
| #define | MCUX_CSSL_FP_BRANCH_TAKEN_POSITIVE(...) |
| Expectation that positive branch has been taken. | |
| #define | MCUX_CSSL_FP_BRANCH_TAKEN_NEGATIVE(...) |
| Expectation that negative branch has been taken. | |
| #define | MCUX_CSSL_FP_SWITCH_DECL(id) |
| Declaration of a flow protected switch. | |
| #define | MCUX_CSSL_FP_SWITCH_CASE(...) |
| Case that is being handled from a switch. | |
| #define | MCUX_CSSL_FP_SWITCH_DEFAULT(...) |
| Case that is being handled from a switch. | |
| #define | MCUX_CSSL_FP_SWITCH_TAKEN(...) |
| Expected that a specific case is handled from a switch. | |
| #define | MCUX_CSSL_FP_SWITCH_TAKEN_DEFAULT(...) |
| Expected that default case is handled from a switch. | |
| #define | MCUX_CSSL_FP_EXPECT(...) |
| Declaration(s) of expected code flow behavior. | |
| #define | MCUX_CSSL_FP_CONDITIONAL(condition, ...) |
| Handling of conditionally expected code flow behavior. | |
| #define | MCUX_CSSL_FP_ASSERT(...) |
| Assert an expected state of the code flow. | |
Provides the API for the CSSL flow protection mechanism.