MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxCsslFlowProtection_Impl.h
Go to the documentation of this file.
1/*--------------------------------------------------------------------------*/
2/* Copyright 2020-2022, 2025 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
18
19#ifndef MCUX_CSSL_FLOW_PROTECTION_IMPL_H_
20#define MCUX_CSSL_FLOW_PROTECTION_IMPL_H_
21
22/* Include the configuration for the flow protection mechanism. */
24
25/* Include the selected implementation of the flow protection mechanism. */
26#if defined(MCUX_CSSL_FP_USE_CODE_SIGNATURE) && (1 == MCUX_CSSL_FP_USE_CODE_SIGNATURE)
27# include <mcuxCsslFlowProtection_CodeSignature.h>
28#elif defined(MCUX_CSSL_FP_USE_SECURE_COUNTER) \
29 && (1 == MCUX_CSSL_FP_USE_SECURE_COUNTER)
32# if defined(MCUX_CSSL_SC_USE_SW_LOCAL) && (1 == MCUX_CSSL_SC_USE_SW_LOCAL)
34# else
35# include <mcuxCsslFlowProtection_SecureCounter_Global.h>
36# endif
37#elif defined(MCUX_CSSL_FP_USE_NONE) && (1 == MCUX_CSSL_FP_USE_NONE)
39#else
40 #error "No flow protection implementation found/configured."
41#endif
42
43#endif /* MCUX_CSSL_FLOW_PROTECTION_IMPL_H_ */
Configuration of the implementation for the flow protection mechanism.
Disabled implementation for the flow protection mechanism.
Counter based implementation for the flow protection mechanism, for a local security counter.
Counter based implementation for the flow protection mechanism, for a local security counter.
Configuration of the implementation for the secure counter mechanism.