MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxCsslMemory.h
Go to the documentation of this file.
1/*--------------------------------------------------------------------------*/
2/* Copyright 2020-2025 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
18
19#ifndef MCUXCSSLMEMORY_H
20#define MCUXCSSLMEMORY_H
21
30
31
33
35
36#include <mcuxCsslMemory_Copy.h>
37
38#include <mcuxCsslMemory_Set.h>
39
40
41
43
44
45
46#endif /* MCUXCSSLMEMORY_H */
header file of memory clear function
Include file for constant time memory compare function.
Constants definitions for the mcuxCsslMemory component.
Include file for memory copy function.
header file of secure memory set function
header file of memory set function
Type definitions for the mcuxCsslMemory component.