19#ifndef MCUXCSSLMEMORY_COMPARE_H
20#define MCUXCSSLMEMORY_COMPARE_H
Provides the API for the CSSL flow protection mechanism.
Definition of function identifiers for the flow protection mechanism.
Type definitions for the mcuxCsslMemory component.
Top-level include file for the parameter integrity protection mechanism.
#define MCUX_CSSL_FP_FUNCTION_DECL(...)
Declaration of a flow protected function.
Definition mcuxCsslFlowProtection.h:166
#define MCUX_CSSL_FP_PROTECTED_TYPE(resultType)
Based on a given base type, builds a return type with flow protection.
Definition mcuxCsslFlowProtection.h:138
mcuxCsslMemory_Status_t mcuxCsslMemory_Compare(mcuxCsslParamIntegrity_Checksum_t chk, void const *pLhs, void const *pRhs, uint32_t length)
Compares the two memory regions lhs and rhs.
uint32_t mcuxCsslMemory_Status_t
Type for CSSL Memory status codes.
Definition mcuxCsslMemory_Types.h:45
uint32_t mcuxCsslParamIntegrity_Checksum_t
Type of a parameter checksum.
Definition mcuxCsslParamIntegrity.h:81