MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxCsslMemory_Copy.h File Reference

Include file for memory copy function. More...

Go to the source code of this file.

Functions

mcuxCsslMemory_Status_t mcuxCsslMemory_Copy (mcuxCsslParamIntegrity_Checksum_t chk, void const *pSrc, void *pDst, uint32_t dstLength, uint32_t length)
 Copies length bytes of data from pSrc to pDst.

Detailed Description

Include file for memory copy function.