MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxCsslMemory_Set.h File Reference

header file of memory set function More...

Go to the source code of this file.

Functions

mcuxCsslMemory_Status_t mcuxCsslMemory_Set (mcuxCsslParamIntegrity_Checksum_t chk, void *pDst, uint8_t val, uint32_t length, uint32_t bufLength)
 Set length bytes of data at pDst.

Detailed Description

header file of memory set function