MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxCsslMemory_Set.h
Go to the documentation of this file.
1/*--------------------------------------------------------------------------*/
2/* Copyright 2021, 2023, 2025 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
18
19
20#ifndef MCUXCSSLMEMORY_SET_H_
21#define MCUXCSSLMEMORY_SET_H_
22
27
35
43
65(
67 void * pDst,
68 uint8_t val,
69 uint32_t length,
70 uint32_t bufLength
71);
72
76
80
81#endif /* MCUXCSSLMEMORY_SET_H_ */
Provides the API for the CSSL flow protection mechanism.
Definition of function identifiers for the flow protection mechanism.
Type definitions for the mcuxCsslMemory component.
Top-level include file for the parameter integrity protection mechanism.
#define MCUX_CSSL_FP_FUNCTION_DECL(...)
Declaration of a flow protected function.
Definition mcuxCsslFlowProtection.h:166
#define MCUX_CSSL_FP_PROTECTED_TYPE(resultType)
Based on a given base type, builds a return type with flow protection.
Definition mcuxCsslFlowProtection.h:138
mcuxCsslMemory_Status_t mcuxCsslMemory_Set(mcuxCsslParamIntegrity_Checksum_t chk, void *pDst, uint8_t val, uint32_t length, uint32_t bufLength)
Set length bytes of data at pDst.
uint32_t mcuxCsslMemory_Status_t
Type for CSSL Memory status codes.
Definition mcuxCsslMemory_Types.h:45
uint32_t mcuxCsslParamIntegrity_Checksum_t
Type of a parameter checksum.
Definition mcuxCsslParamIntegrity.h:81