MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxCsslParamIntegrity.h File Reference

Top-level include file for the parameter integrity protection mechanism. More...

#include <stdint.h>
#include <stddef.h>
#include <stdbool.h>
#include <mcuxCsslFlowProtection.h>
#include <mcuxCsslFlowProtection_FunctionIdentifiers.h>

Go to the source code of this file.

Macros

#define MCUXCSSLPARAMINTEGRITY_BASE_CHECKSUM
 First eight hex digits of Eulers number.
#define MCUXCSSLPARAMINTEGRITY_CHECK_VALID
 Return value of mcuxCsslParamIntegrity_Validate if the parameter checksum was correct.
#define MCUXCSSLPARAMINTEGRITY_CHECK_INVALID
 Return value of mcuxCsslParamIntegrity_Validate if the parameter checksum was incorrect.
#define MCUX_CSSL_PI_PARAM_ADD_CASTED_ARG(x)
#define MCUX_CSSL_PI_VALIDATE(chk, ...)
#define MCUX_CSSL_PI_PROTECT(...)

Typedefs

typedef void * mcuxCsslParamIntegrity_AssertionCpuWordSize_t[(4u==sizeof(size_t)) ?(+1) :(-1)]
 Build time assertion to ensure CPU word size of 32 bit.
typedef uint32_t mcuxCsslParamIntegrity_Checksum_t
 Type of a parameter checksum.
typedef uint32_t mcuxCsslParamIntegrity_Param_t
 Type of a parameter for the checksum calculation.

Functions

mcuxCsslParamIntegrity_Checksum_t mcuxCsslParamIntegrity_Protect (uint32_t nargs,...)
 Calculates a parameter checksum.
mcuxCsslParamIntegrity_Checksum_t mcuxCsslParamIntegrity_Validate (mcuxCsslParamIntegrity_Checksum_t chk, uint32_t nargs,...)
 Verifies the correctness of a parameter checksum.

Detailed Description

Top-level include file for the parameter integrity protection mechanism.

The library exposes the following functions:

  1. Generation of parameter checksums: mcuxCsslParamIntegrity_Protect
  2. Validation of parameter checksums: mcuxCsslParamIntegrity_Validate