MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxCsslSecureCounter.h
Go to the documentation of this file.
1/*--------------------------------------------------------------------------*/
2/* Copyright 2020-2023 NXP */
3/* */
4/* NXP Confidential and Proprietary. This software is owned or controlled */
5/* by NXP and may only be used strictly in accordance with the applicable */
6/* license terms. By expressly accepting such terms or by downloading, */
7/* installing, activating and/or otherwise using the software, you are */
8/* agreeing that you have read, and that you agree to comply with and are */
9/* bound by, such license terms. If you do not agree to be bound by the */
10/* applicable license terms, then you may not retain, install, activate or */
11/* otherwise use the software. */
12/*--------------------------------------------------------------------------*/
13
18
19#ifndef MCUXCSSLSECURECOUNTER_H_
20#define MCUXCSSLSECURECOUNTER_H_
21
22/* Include the actual implementation of the secure counter mechanism. */
24
32
33
41
42/****************************************************************************/
43/* Constants */
44/****************************************************************************/
45
52#define MCUX_CSSL_SC_CHECK_PASSED \
53 MCUX_CSSL_SC_CHECK_PASSED_IMPL
54
61#define MCUX_CSSL_SC_CHECK_FAILED \
62 MCUX_CSSL_SC_CHECK_FAILED_IMPL
63
70#define MCUX_CSSL_SC_VALUE_TYPE \
71 MCUX_CSSL_SC_VALUE_TYPE_IMPL
72
73/****************************************************************************/
74/* Initialization */
75/****************************************************************************/
76
83#define MCUX_CSSL_SC_ALLOC() \
84 MCUX_CSSL_SC_ALLOC_IMPL()
85
94#define MCUX_CSSL_SC_INIT(value) \
95 MCUX_CSSL_SC_INIT_IMPL(value)
96
97/****************************************************************************/
98/* Check */
99/****************************************************************************/
100
111#define MCUX_CSSL_SC_CHECK(reference) \
112 MCUX_CSSL_SC_CHECK_IMPL(reference)
113
114/****************************************************************************/
115/* Counter increment */
116/****************************************************************************/
122
136#define MCUX_CSSL_SC_ADD(value) \
137 MCUX_CSSL_SC_ADD_IMPL(value)
138
149#define MCUX_CSSL_SC_ADD_ON_CALL(value) \
150 MCUX_CSSL_SC_ADD_ON_CALL_IMPL(value)
151
163#define MCUX_CSSL_SC_ADD_0x1() \
164 MCUX_CSSL_SC_ADD_0x1_IMPL()
165
177#define MCUX_CSSL_SC_ADD_0x10() \
178 MCUX_CSSL_SC_ADD_0x10_IMPL()
179
191#define MCUX_CSSL_SC_ADD_0x100() \
192 MCUX_CSSL_SC_ADD_0x100_IMPL()
193
194/****************************************************************************/
195/* Counter decrement */
196/****************************************************************************/
202
216#define MCUX_CSSL_SC_SUB(value) \
217 MCUX_CSSL_SC_SUB_IMPL(value)
218
230#define MCUX_CSSL_SC_SUB_0x1() \
231 MCUX_CSSL_SC_SUB_0x1_IMPL()
232
244#define MCUX_CSSL_SC_SUB_0x10() \
245 MCUX_CSSL_SC_SUB_0x10_IMPL()
246
258#define MCUX_CSSL_SC_SUB_0x100() \
259 MCUX_CSSL_SC_SUB_0x100_IMPL()
260
261/****************************************************************************/
262/* Direct access (optional) */
263/****************************************************************************/
272
285#define MCUX_CSSL_SC_VALUE() \
286 MCUX_CSSL_SC_VALUE_IMPL()
287
301#define MCUX_CSSL_SC_ASSIGN(value) \
302 MCUX_CSSL_SC_ASSIGN_IMPL(value)
303
304#endif /* MCUXCSSLSECURECOUNTER_H_ */
Selection of the implementation for the secure counter mechanism.