MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClBuffer

Buffer component. More...

Topics

 Buffer initialization functionality
 Buffer initialization functionality.
 Buffer manipulation functionality
 Input/output buffer manipulation functionality.
 mcuxClBuffer_Constants
 Buffer constants.
 Buffer type definitions
 Types used by the buffer operations.

Macros

#define MCUXCLBUFFER_USE_OBJECT
 If set to 1, use the object oriented buffer implementation.
#define MCUXCLBUFFER_USE_POINTER
 If set to 1, use the plain C pointer buffer implementation.

Detailed Description

Buffer component.

Macro Definition Documentation

◆ MCUXCLBUFFER_USE_OBJECT

#define MCUXCLBUFFER_USE_OBJECT

If set to 1, use the object oriented buffer implementation.

◆ MCUXCLBUFFER_USE_POINTER

#define MCUXCLBUFFER_USE_POINTER

If set to 1, use the plain C pointer buffer implementation.