MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
Buffer type definitions

Types used by the buffer operations. More...

Typedefs

typedef const uint8_t * mcuxCl_InputBuffer_t
 Input buffer type.
typedef uint8_t * mcuxCl_Buffer_t
 Input/output buffer type.

Detailed Description

Types used by the buffer operations.

Typedef Documentation

◆ mcuxCl_InputBuffer_t

◆ mcuxCl_Buffer_t