Types for use with the Glikey driver. More...
Typedefs | |
| typedef uint32_t | mcuxClGlikey_BaseAddress_t |
| typedef uint32_t | mcuxClGlikey_Status_t |
| typedef uint32_t | mcuxClGlikey_IntEnable_t |
| typedef uint32_t | mcuxClGlikey_GlikeyStatus_t |
Functions | |
| mcuxClGlikey_Status_t | mcuxClGlikey_GetStatus (mcuxClGlikey_BaseAddress_t *base, mcuxClGlikey_GlikeyStatus_t *result) |
| Retrieves the current status of Glikey. | |
| mcuxClGlikey_Status_t | mcuxClGlikey_SyncReset (mcuxClGlikey_BaseAddress_t *base) |
| Perform a synchronous reset of Glikey. | |
| mcuxClGlikey_Status_t | mcuxClGlikey_SetIntEnable (mcuxClGlikey_BaseAddress_t *base, mcuxClGlikey_IntEnable_t value) |
| Set interrupt enable flag of Glikey. | |
| mcuxClGlikey_Status_t | mcuxClGlikey_GetIntEnable (mcuxClGlikey_BaseAddress_t *base, mcuxClGlikey_IntEnable_t *value) |
| Get interrupt enable flag of Glikey. | |
| mcuxClGlikey_Status_t | mcuxClGlikey_ClearIntStatus (mcuxClGlikey_BaseAddress_t *base) |
| Clear the interrupt status flag of Glikey. | |
| mcuxClGlikey_Status_t | mcuxClGlikey_SetIntStatus (mcuxClGlikey_BaseAddress_t *base) |
| Set the interrupt status flag of Glikey. | |
| mcuxClGlikey_Status_t | mcuxClGlikey_Lock (mcuxClGlikey_BaseAddress_t *base) |
| Lock Glikey SFR interface. | |
| mcuxClGlikey_Status_t | mcuxClGlikey_IsLocked (mcuxClGlikey_BaseAddress_t *base) |
| Check if Glikey is locked. | |
| mcuxClGlikey_Status_t | mcuxClGlikey_IsIndexLocked (mcuxClGlikey_BaseAddress_t *base, uint32_t index) |
| Check if Glikey index is locked. | |
| mcuxClGlikey_Status_t | mcuxClGlikey_StartEnable (mcuxClGlikey_BaseAddress_t *base, uint32_t index) |
| Start Glikey enable. | |
| mcuxClGlikey_Status_t | mcuxClGlikey_ContinueEnable (mcuxClGlikey_BaseAddress_t *base, uint32_t codeword) |
| Continue Glikey enable. | |
| mcuxClGlikey_Status_t | mcuxClGlikey_LockIndex (mcuxClGlikey_BaseAddress_t *base) |
| Lock Glikey index. | |
| mcuxClGlikey_Status_t | mcuxClGlikey_ResetIndex (mcuxClGlikey_BaseAddress_t *base, uint32_t index) |
| Reset Glikey index. | |
| mcuxClGlikey_Status_t | mcuxClGlikey_EndOperation (mcuxClGlikey_BaseAddress_t *base) |
| End Glikey operation TODO: if we are in locked state we cannot exit(move to init) as curent index is locked. | |
Types for use with the Glikey driver.
| mcuxClGlikey_Status_t mcuxClGlikey_GetStatus | ( | mcuxClGlikey_BaseAddress_t * | base, |
| mcuxClGlikey_GlikeyStatus_t * | result ) |
Retrieves the current status of Glikey.
| [in] | base | The base address of the Glikey instance |
| [out] | result | Pointer which will be filled with the Glikey status information |
| #MCUXCLGLIKEY_STATUS_OK | The operation was successful |
| mcuxClGlikey_Status_t mcuxClGlikey_SyncReset | ( | mcuxClGlikey_BaseAddress_t * | base | ) |
Perform a synchronous reset of Glikey.
This function performs a synchronous reset of the Glikey. This results in:
| [in] | base | The base address of the Glikey instance |
| #MCUXCLGLIKEY_STATUS_OK | The operation was successful |
| #MCUXCLGLIKEY_STATUS_LOCKED_ERROR | Glikey is locked and cannot be reset by software |
| mcuxClGlikey_Status_t mcuxClGlikey_SetIntEnable | ( | mcuxClGlikey_BaseAddress_t * | base, |
| mcuxClGlikey_IntEnable_t | value ) |
Set interrupt enable flag of Glikey.
| [in] | base | The base address of the Glikey instance |
| [in] | value | Value to set the interrupt enable flag to, see #[TODO: add reference to constants] |
| #MCUXCLGLIKEY_STATUS_OK | The operation was successful |
| #MCUXCLGLIKEY_STATUS_LOCKED_ERROR | Glikey is locked and cannot be configured by software |
| mcuxClGlikey_Status_t mcuxClGlikey_GetIntEnable | ( | mcuxClGlikey_BaseAddress_t * | base, |
| mcuxClGlikey_IntEnable_t * | value ) |
Get interrupt enable flag of Glikey.
| [in] | base | The base address of the Glikey instance |
| [out] | value | Pointer which will be filled with the interrupt enable status, see #[TODO: add reference to constants] |
| #MCUXCLGLIKEY_STATUS_OK | The operation was successful |
| mcuxClGlikey_Status_t mcuxClGlikey_ClearIntStatus | ( | mcuxClGlikey_BaseAddress_t * | base | ) |
Clear the interrupt status flag of Glikey.
| #MCUXCLGLIKEY_STATUS_OK | The operation was successful |
| #MCUXCLGLIKEY_STATUS_LOCKED_ERROR | Glikey is locked and cannot be configured by software |
| mcuxClGlikey_Status_t mcuxClGlikey_SetIntStatus | ( | mcuxClGlikey_BaseAddress_t * | base | ) |
Set the interrupt status flag of Glikey.
| #MCUXCLGLIKEY_STATUS_OK | The operation was successful |
| #MCUXCLGLIKEY_STATUS_LOCKED_ERROR | Glikey is locked and cannot be configured by software |
| mcuxClGlikey_Status_t mcuxClGlikey_Lock | ( | mcuxClGlikey_BaseAddress_t * | base | ) |
Lock Glikey SFR interface.
This operation locks the Glikey SFR interface if it is not locked yet.
| #MCUXCLGLIKEY_STATUS_OK | The operation was successful |
| mcuxClGlikey_Status_t mcuxClGlikey_IsLocked | ( | mcuxClGlikey_BaseAddress_t * | base | ) |
Check if Glikey is locked.
This operation returns the locking status of Glikey.
| #MCUXCLGLIKEY_STATUS_NOT_LOCKED | Glikey is not locked |
| #MCUXCLGLIKEY_STATUS_LOCKED | Glikey is locked |
| mcuxClGlikey_Status_t mcuxClGlikey_IsIndexLocked | ( | mcuxClGlikey_BaseAddress_t * | base, |
| uint32_t | index ) |
Check if Glikey index is locked.
This operation returns the locking status of Glikey index. Using a wrong index (which is out of the bounds) leads to undefined program behavior.
| #MCUXCLGLIKEY_STATUS_NOT_LOCKED | The Glikey index is not locked |
| #MCUXCLGLIKEY_STATUS_LOCKED | The Glikey index is locked |
| mcuxClGlikey_Status_t mcuxClGlikey_StartEnable | ( | mcuxClGlikey_BaseAddress_t * | base, |
| uint32_t | index ) |
Start Glikey enable.
This operation is used to set a new index and start a the sequence to enable it. It needs to be started from the INIT state. If the new index is already locked Glikey will go to LOCKED state, otherwise it will go to STEP1 state. If this operation is used when Glikey is in any state other than INIT Glikey will go to WR_DIS state. It can only recover from this state through a reset (synchronous or asynchronous). If the Glikey SFR lock is active this operation will return an error. Using a wrong index (which is out of the bounds) leads to undefined program behavior.
| #MCUXCLGLIKEY_STATUS_OK | The operation was successful |
| #MCUXCLGLIKEY_STATUS_LOCKED | The Glikey index is locked |
| #MCUXCLGLIKEY_STATUS_LOCKED_ERROR | Glikey is locked and cannot be configured by software |
| mcuxClGlikey_Status_t mcuxClGlikey_ContinueEnable | ( | mcuxClGlikey_BaseAddress_t * | base, |
| uint32_t | codeword ) |
Continue Glikey enable.
This operation is used to progress through the different states of the state machine, starting from STEP1 until the state WR_EN is reached. Each next state of the state machine can only be reached by providing the right codeword to this function. The transition from a state to itself is always possible. The possible transitions are:
| #MCUXCLGLIKEY_STATUS_OK | The state transition was triggered successfully |
| #MCUXCLGLIKEY_STATUS_LOCKED_ERROR | Glikey is locked and cannot be configured by software |
| mcuxClGlikey_Status_t mcuxClGlikey_LockIndex | ( | mcuxClGlikey_BaseAddress_t * | base | ) |
Lock Glikey index.
This operation is used to lock a Glikey index. It can only be executed from the WR_EN state, executing it from any other state will result in Glikey entering WR_DIS state. When this happens Glikey requires a reset (synchronous or asynchronous) to go back to INIT state. If the Glikey SFR lock is active this operation will return an error.
| #MCUXCLGLIKEY_STATUS_LOCKED | The Glikey index is now locked |
| #MCUXCLGLIKEY_STATUS_LOCKED_ERROR | Glikey is locked and cannot be configured by software |
| mcuxClGlikey_Status_t mcuxClGlikey_ResetIndex | ( | mcuxClGlikey_BaseAddress_t * | base, |
| uint32_t | index ) |
Reset Glikey index.
This operation is used to reset a Glikey index. It can only be executed from the INIT state, executing it from any other state will result in Glikey entering WR_DIS state. When this happens Glikey requires a reset (synchronous or asynchronous) to go back to INIT state. If the Glikey SFR lock is active or the index is locked this operation will return an error. Using a wrong index (which is out of the bounds) leads to undefined program behavior.
| #MCUXCLGLIKEY_STATUS_OK | The operation was successful |
| #MCUXCLGLIKEY_STATUS_LOCKED | The Glikey index is locked |
| #MCUXCLGLIKEY_STATUS_LOCKED_ERROR | Glikey is locked and cannot be configured by software |
| mcuxClGlikey_Status_t mcuxClGlikey_EndOperation | ( | mcuxClGlikey_BaseAddress_t * | base | ) |
End Glikey operation TODO: if we are in locked state we cannot exit(move to init) as curent index is locked.
This operation is used to end a Glikey operation. It can only be executed from the WR_EN, LOCKED, RESET, and INIT states. Executing it from any other state will result in Glikey entering WR_DIS state. When this happens Glikey requires a reset (synchronous or asynchronous) to go back to INIT state. After this operation Glikey will go to INIT state or stay in LOCKED state when the index was locked. If the Glikey SFR lock is active this operation will return an error.
| #MCUXCLGLIKEY_STATUS_OK | The operation was successful |
| #MCUXCLGLIKEY_STATUS_LOCKED | The Glikey index is still locked |
| #MCUXCLGLIKEY_STATUS_LOCKED_ERROR | Glikey is locked and cannot be configured by software |