Defines all key load options (slots, others) of mcuxClKey. More...
Macros | |
| #define | MCUXCLKEY_LOADOPTION_MASK |
| #define | MCUXCLKEY_LOADOPTION_SLOT_MASK |
| Defines for supported key slots. | |
| #define | MCUXCLKEY_LOADOPTION_SLOT_INVALID |
| #define | MCUXCLKEY_LOADOPTION_SLOT_COPRO_MASK |
| #define | MCUXCLKEY_LOADOPTION_SLOT_COPRO_SHIFT |
| #define | MCUXCLKEY_LOADOPTION_SLOT_COPRO_SGI |
| #define | MCUXCLKEY_LOADOPTION_SLOT_SLOT_MASK |
| #define | MCUXCLKEY_LOADOPTION_SLOT_SLOT_SHIFT |
| #define | MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_0 |
| SGI key slot 0. Reserved for CL internal key usage. | |
| #define | MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_1 |
| SGI key slot 1. Reserved for CL internal key usage. | |
| #define | MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_2 |
| SGI key slot 2. | |
| #define | MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_3 |
| SGI key slot 3. | |
| #define | MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_4 |
| SGI key slot 4. | |
| #define | MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_5 |
| SGI key slot 5. | |
| #define | MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_6 |
| SGI key slot 6. | |
| #define | MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_7 |
| SGI key slot 7. | |
| #define | MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_UNWRAP |
| Sgi key slot containing an RFC3394 unwrapped key. | |
| #define | MCUXCLKEY_LOADOPTION_ALREADYLOADED_MASK |
| Defines for other key options that can be encoded in a slot. | |
| #define | MCUXCLKEY_LOADOPTION_ALREADYLOADED_SHIFT |
| #define | MCUXCLKEY_LOADOPTION_ALREADYLOADED |
| Option: the key is already loaded; only set the fields in the key object. | |
| #define | MCUXCLKEY_LOADOPTION_RFU_MASK |
| Defines for RFU bits. | |
Defines all key load options (slots, others) of mcuxClKey.
| #define MCUXCLKEY_LOADOPTION_SLOT_MASK |
Defines for supported key slots.
| #define MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_0 |
SGI key slot 0. Reserved for CL internal key usage.
| #define MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_1 |
SGI key slot 1. Reserved for CL internal key usage.
| #define MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_2 |
| #define MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_3 |
SGI key slot 3.
| #define MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_4 |
SGI key slot 4.
| #define MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_5 |
SGI key slot 5.
| #define MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_6 |
| #define MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_7 |
SGI key slot 7.
| #define MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_UNWRAP |
Sgi key slot containing an RFC3394 unwrapped key.
| #define MCUXCLKEY_LOADOPTION_ALREADYLOADED_MASK |
Defines for other key options that can be encoded in a slot.
| #define MCUXCLKEY_LOADOPTION_ALREADYLOADED |
Option: the key is already loaded; only set the fields in the key object.
| #define MCUXCLKEY_LOADOPTION_RFU_MASK |
Defines for RFU bits.