MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClMemory_Endianness

These macros implement endianess management on integers. More...

Macros

#define mcuxClMemory_StoreLittleEndian32(destination, value)
 Converts a 32-bit unsigned integer to a little-endian order uint8_t array .
#define mcuxClMemory_StoreBigEndian32(destination, value)
 Converts a 32-bit unsigned integer to a big-endian order uint8_t array.
#define mcuxClMemory_LoadLittleEndian32(source)
 Converts a little-endian order uint8_t array to a 32-bit unsigned integer.
#define mcuxClMemory_LoadBigEndian32(source)
 Converts a big-endian order uint8_t array to a 32-bit unsigned integer.
#define MCUXCLMEMORY_SWITCH_4BYTE_ENDIANNESS(input)
 MACRO that switches byte endianness of given CPU word.

Detailed Description

These macros implement endianess management on integers.

Macro Definition Documentation

◆ mcuxClMemory_StoreLittleEndian32

#define mcuxClMemory_StoreLittleEndian32 ( destination,
value )

Converts a 32-bit unsigned integer to a little-endian order uint8_t array .

Note
Implementation is platform independent.
Parameters
[out]destinationpointer to a 4 byte buffer were 32-bit integer in little-endian will be encoded.
[in]valuepointer to the 32-bit integer to be encoded.

◆ mcuxClMemory_StoreBigEndian32

#define mcuxClMemory_StoreBigEndian32 ( destination,
value )

Converts a 32-bit unsigned integer to a big-endian order uint8_t array.

Note
Implementation is platform independent.
Parameters
[in]sourcepointer to a 4 byte big-endian order uint8_t buffer that will be converted to an unsigned integer

◆ mcuxClMemory_LoadLittleEndian32

#define mcuxClMemory_LoadLittleEndian32 ( source)

Converts a little-endian order uint8_t array to a 32-bit unsigned integer.

Note
Implementation is platform independent.
Parameters
[in]sourcepointer to a 4 byte little-endian order uint8_t buffer that will be converted to an unsigned integer

◆ mcuxClMemory_LoadBigEndian32

#define mcuxClMemory_LoadBigEndian32 ( source)

Converts a big-endian order uint8_t array to a 32-bit unsigned integer.

Parameters
[in]destinationpointer to a 4 byte buffer were 32-bit integer in big-endian will be decoded.
Returns
a 32-bit unsigned integer

◆ MCUXCLMEMORY_SWITCH_4BYTE_ENDIANNESS

#define MCUXCLMEMORY_SWITCH_4BYTE_ENDIANNESS ( input)

MACRO that switches byte endianness of given CPU word.

Parameters
[in]inputa 32-bit unsigned integer whose endianness will be reversed.