MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClSgi_Types

Defines the types and associated constants of the mcuxClSgi component. More...

Typedefs

typedef uint32_t mcuxClSgi_Status_t
 SGI status code.

Detailed Description

Defines the types and associated constants of the mcuxClSgi component.

Typedef Documentation

◆ mcuxClSgi_Status_t

typedef uint32_t mcuxClSgi_Status_t

SGI status code.

This type provides information about the status of the SGI operation that has been performed.