Flow protection handling core functionality. More...
Macros | |
| #define | MCUX_CSSL_FP_COUNTER_STMT(statement) |
| A statement which is only evaluated if a secure counter is used. | |
Flow protection handling core functionality.
This subset of Flow protection macros is common to all code flow patterns to be protected.
| #define MCUX_CSSL_FP_COUNTER_STMT | ( | statement | ) |
A statement which is only evaluated if a secure counter is used.
This macro can be applied to create or use supporting variables that are only needed if the active configuration uses a secure counter, to avoid warnings about unused variables.
This should only be required if a codebase is used with different backend classes for different build configurations.
| statement | The statement to be conditionally included. |