MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxCsslMemory_SecureSet Function Definitions

mcuxCsslMemory_SecureSet Function Definitions More...

Functions

mcuxCsslMemory_Status_t mcuxCsslMemory_SecureSet (mcuxCsslParamIntegrity_Checksum_t chk, void *pDst, uint8_t val, uint32_t length, uint32_t bufLength)
 Set length bytes of data at pDst.

Detailed Description

mcuxCsslMemory_SecureSet Function Definitions

Function Documentation

◆ mcuxCsslMemory_SecureSet()

mcuxCsslMemory_Status_t mcuxCsslMemory_SecureSet ( mcuxCsslParamIntegrity_Checksum_t chk,
void * pDst,
uint8_t val,
uint32_t length,
uint32_t bufLength )

Set length bytes of data at pDst.

The implementation is secure in the following aspects: Parameter integrity protection: the function returns immediately in case of an incorrect parameter checksum. Data is first overwritten with random data before being set to the new value Code flow protection: the function call is protected. Buffer overflow protection: no data is written to pDst beyond bufLength bytes.

Parameters
[in]chkThe parameter checksum, generated with #MCUX_CSSL_PI_PROTECT.
[in]pDstThe destination pointer to buffer to be set. Must not be NULL.
[in]valThe byte value to be set.
[in]lengthThe size in bytes to set.
[in]bufLengthThe buffer size (if bufLength < length, only bufLength bytes are set).
Returns
A status code encapsulated in a flow-protection type.
Return values
MCUXCSSLMEMORY_STATUS_OKIf val set length times at pDst.
MCUXCSSLMEMORY_STATUS_INVALID_PARAMETERIf one of the parameters is invalid.
MCUXCSSLMEMORY_STATUS_FAULTIf a fault was detected, included invalid checksum chk.
Attention
The function uses PRNG, which has to be available and ready for generation.
Examples
mcuxCsslMemory_SecureSet_example.c.