Defines the memory consumption for the mcuxClEcc component. More...
Topics | |
| MCUXCLECC_WACPU_ | |
| Define the CPU workarea size required by mcuxClEcc APIs. | |
| MCUXCLECC_MONTDH_WACPU_ | |
| Define the CPU workarea size required by mcuxClEcc MontDH APIs. | |
| MCUXCLECC_EDDSA_WACPU_ | |
| Define the CPU workarea size required by mcuxClEcc EdDSA APIs. | |
| MCUXCLECC_WAPKC_ | |
| Define the PKC workarea size required by mcuxClEcc APIs. | |
| MCUXCLECC_MONTDH_WAPKC_ | |
| Define the PKC workarea size required by mcuxClEcc_Mont APIs. | |
| MCUXCLECC_EDDSA_WAPKC_ | |
| Define the PKC workarea size required by mcuxClEcc EdDSA APIs. | |
| MCUXCLECC_EDDSA_GENKEYPAIR_DESC_SIZE_ | |
| Define for the EdDSA key pair generation descriptor size. | |
| MCUXCLECC_EDDSA_SIGNATURE_PROTOCOL_DESC_SIZE_ | |
| Define for the EdDSA signature protocol descriptor size. | |
| MCUXCLECC_EDDSA_SIGNATURE_MODE_SIZE_ | |
| Define for the EdDSA signature protocol descriptor size. | |
Macros | |
| #define | MCUXCLECC_CUSTOMWEIERECCDOMAINPARAMS_SIZE(byteLenP, byteLenN) |
| Define for the buffer size (in bytes) for optimized custom ECC Weierstrass domain parameters. | |
Defines the memory consumption for the mcuxClEcc component.
| #define MCUXCLECC_CUSTOMWEIERECCDOMAINPARAMS_SIZE | ( | byteLenP, | |
| byteLenN ) |
Define for the buffer size (in bytes) for optimized custom ECC Weierstrass domain parameters.