mcuxClEcc return code definitions More...
Macros | |
| #define | MCUXCLECC_STATUS_OK |
| Operation was successful. | |
| #define | MCUXCLECC_STATUS_INVALID_PARAMS |
| Parameters are invalid. | |
| #define | MCUXCLECC_STATUS_SCALAR_ZERO |
| Internal scalar for point multiplication is zero (mod n). | |
| #define | MCUXCLECC_STATUS_INVALID_SIGNATURE |
| ECDSA Signature is invalid. | |
| #define | MCUXCLECC_STATUS_NEUTRAL_POINT |
| The result of the point operation is the neutral point. | |
| #define | MCUXCLECC_STATUS_FAULT_ATTACK |
| Fault attack (unexpected behavior) is detected. | |
| #define | MCUXCLECC_STATUS_SMALL_SUBGROUP_ATTACK |
| MONTDH public key lies in small subgroup. | |
mcuxClEcc return code definitions
| #define MCUXCLECC_STATUS_OK |
Operation was successful.
| #define MCUXCLECC_STATUS_INVALID_PARAMS |
Parameters are invalid.
| #define MCUXCLECC_STATUS_SCALAR_ZERO |
Internal scalar for point multiplication is zero (mod n).
| #define MCUXCLECC_STATUS_INVALID_SIGNATURE |
ECDSA Signature is invalid.
| #define MCUXCLECC_STATUS_NEUTRAL_POINT |
The result of the point operation is the neutral point.
| #define MCUXCLECC_STATUS_FAULT_ATTACK |
Fault attack (unexpected behavior) is detected.
| #define MCUXCLECC_STATUS_SMALL_SUBGROUP_ATTACK |
MONTDH public key lies in small subgroup.