MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
McuxClEcc_ECDSADescriptors

mcuxClEcc definitions of ECDSA variant descriptors More...

Variables

const mcuxClSignature_ModeDescriptor_t mcuxClSignature_ModeDescriptor_ECDSA
 ECDSA Signature mode descriptor.
static mcuxClSignature_Mode_t mcuxClSignature_Mode_ECDSA
 ECDSA Signature mode.

Detailed Description

mcuxClEcc definitions of ECDSA variant descriptors

Variable Documentation

◆ mcuxClSignature_ModeDescriptor_ECDSA

const mcuxClSignature_ModeDescriptor_t mcuxClSignature_ModeDescriptor_ECDSA
extern

ECDSA Signature mode descriptor.

#ifdef MCUXCL_FEATURE_SIGNATURE_VERIFY_PARAMETER_PROTECTION This mode requires that mcuxClSignature_verify is called with additional protection on pIn and inSize parameters. mode, pIn and inSize parameters must be protected using mcuxClSignature_verify_recordParam function before executing mcuxClSignature_verify. #endif

#ifdef MCUXCL_FEATURE_SESSION_SECURITYOPTIONS_CRC When the MCUXCLSESSION_SECURITYOPTIONS_SAVE_CRC_FOR_EXTERNAL_VERIFICATION_ENABLE security option is active, the mcuxClSignature_verify function saves the CRC32 of the R value of the computed signature in the session for extra verification. The CRC on user side can be computed with the function mcuxClCrc_computeCRC32 and with the function mcuxClSession_getCrcForExternalVerification, the user can obtain the reference CRC for the verification. #endif

◆ mcuxClSignature_Mode_ECDSA