Example for the mcuxClCipherModes component.
#include <mcuxClToolchain.h>
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_Session_Helper.h>
#include <mcuxClExample_RNG_Helper.h>
static const uint8_t plain[62] = {
0x61u, 0x62u, 0x63u, 0x64u, 0x65u, 0x66u, 0x67u, 0x68u,
0x69u, 0x6Au, 0x6Bu, 0x6Cu, 0x6Du, 0x6Eu, 0x6Fu, 0x70u,
0x62u, 0x63u, 0x64u, 0x65u, 0x66u, 0x67u, 0x68u, 0x69u,
0x6Au, 0x6Bu, 0x6Cu, 0x6Du, 0x6Eu, 0x6Fu, 0x70u, 0x71u,
0x63u, 0x64u, 0x65u, 0x66u, 0x67u, 0x68u, 0x69u, 0x6Au,
0x6Bu, 0x6Cu, 0x6Du, 0x6Eu, 0x6Fu, 0x70u, 0x71u, 0x72u,
0x64u, 0x65u, 0x66u, 0x67u, 0x68u, 0x69u, 0x6Au, 0x6Bu,
0x6Cu, 0x6Du, 0x6Eu, 0x6Fu, 0x70u, 0x71u
};
static const uint8_t encryptedRef[64] = {
0xe6u, 0xd4u, 0xe7u, 0xdau, 0x9eu, 0x63u, 0xc6u, 0x67u,
0xfbu, 0xa0u, 0x43u, 0x2au, 0xadu, 0x45u, 0x4bu, 0x7du,
0xf2u, 0xb7u, 0x91u, 0x4eu, 0x89u, 0xe1u, 0x07u, 0xe1u,
0xa0u, 0x0eu, 0xe2u, 0x52u, 0xccu, 0xbau, 0xbbu, 0x1fu,
0x69u, 0x4au, 0x00u, 0xe4u, 0x2eu, 0x89u, 0xfbu, 0x43u,
0x79u, 0x8bu, 0x28u, 0x38u, 0x6bu, 0x7cu, 0xecu, 0x7fu,
0xa3u, 0x04u, 0x9fu, 0x04u, 0x93u, 0xe1u, 0x41u, 0xbdu,
0x88u, 0xeau, 0xb9u, 0xe5u, 0x5au, 0xd5u, 0x85u, 0x59u
};
static const uint8_t iv[16] = {
0x7Au, 0x79u, 0x78u, 0x77u, 0x76u, 0x75u, 0x74u, 0x73u,
0x72u, 0x71u, 0x70u, 0x6Fu, 0x6Eu, 0x6Du, 0x6Cu, 0x6Bu,
};
static const uint8_t keyBytes[16] = {
0x6Bu, 0x6Cu, 0x6Du, 0x6Eu, 0x6Fu, 0x70u, 0x71u, 0x72u,
0x73u, 0x74u, 0x75u, 0x76u, 0x77u, 0x78u, 0x79u, 0x7Au,
};
MCUXCLEXAMPLE_FUNCTION(mcuxClCipherModes_Cbc_Aes128_Multipart_PaddingISO_example)
{
mcuxClSession_Descriptor_t sessionDesc;
#define MCUXCLCIPHERMODES_CPU_WA MCUXCLCIPHER_AES_PROCESS_CPU_WA_BUFFER_SIZE
#define MCUXCLCIPHERMODES_CONTEXT_SIZE MCUXCLCIPHER_AES_CONTEXT_SIZE
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION(session, MCUXCLEXAMPLE_MAX_WA(MCUXCLCIPHERMODES_CPU_WA, MCUXCLRANDOM_NCINIT_WACPU_SIZE), 0u);
MCUXCLEXAMPLE_INITIALIZE_PRNG(session);
uint32_t keyDesc[MCUXCLKEY_DESCRIPTOR_SIZE_IN_WORDS];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
session,
key,
keyBytes,
sizeof(keyBytes))
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
uint32_t outLength = 0u;
uint32_t encryptedSize = 0u;
uint8_t encryptedData[sizeof(encryptedRef)];
ALIGNED uint8_t ctxBuf[MCUXCLCIPHERMODES_CONTEXT_SIZE];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
session,
ctx,
key,
ivBuf,
sizeof(iv))
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClCipher_init_encrypt")
ctx,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
plainBuf,
sizeof(plain) / 2u,
encryptedDataBuf,
&outLength)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUX_CSSL_ANALYSIS_START_SUPPRESS_INTEGER_OVERFLOW("Calculation does not overflow")
encryptedSize += outLength;
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_INTEGER_OVERFLOW()
session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClCipher_init_encrypt")
ctx,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
plainBuf,
sizeof(plain) - sizeof(plain) / 2u,
encryptedDataBuf,
&outLength)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUX_CSSL_ANALYSIS_START_SUPPRESS_INTEGER_OVERFLOW("Calculation does not overflow")
encryptedSize += outLength;
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_INTEGER_OVERFLOW()
MCUXCLBUFFER_SET(encryptedDataBuf, &encryptedData[encryptedSize], sizeof(encryptedData) );
session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClCipher_init_encrypt")
ctx,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
encryptedDataBuf,
&outLength)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUX_CSSL_ANALYSIS_START_SUPPRESS_INTEGER_OVERFLOW("Calculation does not overflow")
encryptedSize += outLength;
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_INTEGER_OVERFLOW()
uint32_t decryptedSize = 0u;
uint8_t decryptedData[sizeof(plain)];
session,
ctx,
key,
ivBuf,
sizeof(iv))
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClCipher_init_decrypt")
ctx,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
encryptedSize / 3u,
decryptedDataBuf,
&outLength)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUX_CSSL_ANALYSIS_START_SUPPRESS_INTEGER_OVERFLOW("Calculation does not overflow")
decryptedSize += outLength;
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_INTEGER_OVERFLOW()
session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClCipher_init_decrypt")
ctx,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
MCUX_CSSL_ANALYSIS_START_SUPPRESS_INTEGER_OVERFLOW("Calculation does not wrap")
encryptedSize - encryptedSize / 3u,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_INTEGER_OVERFLOW()
decryptedDataBuf,
&outLength)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUX_CSSL_ANALYSIS_START_SUPPRESS_INTEGER_OVERFLOW("Calculation does not overflow")
decryptedSize += outLength;
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_INTEGER_OVERFLOW()
MCUXCLBUFFER_SET(decryptedDataBuf, &decryptedData[decryptedSize], sizeof(decryptedData) );
session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClCipher_init_decrypt")
ctx,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
decryptedDataBuf,
&outLength)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUX_CSSL_ANALYSIS_START_SUPPRESS_INTEGER_OVERFLOW("Calculation does not overflow")
decryptedSize += outLength;
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_INTEGER_OVERFLOW()
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(sizeof(encryptedRef) != encryptedSize)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(!mcuxClCore_assertEqual(encryptedRef, encryptedData, sizeof(encryptedRef)))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(sizeof(plain) != decryptedSize)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(!mcuxClCore_assertEqual(plain, decryptedData, sizeof(plain)))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
return MCUXCLEXAMPLE_STATUS_OK;
}
Top-level include file for the mcuxClAes component.
Top-level include file for the mcuxClBuffer component.
Top-level include file for the mcuxClCipher component.
Top-level include file for the mcuxClCipherModes component.
Definition of function identifiers for the flow protection mechanism.
Top-level include file for the mcuxClKey component.
Top-level include file for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.
static const mcuxClKey_Type_t mcuxClKey_Type_Aes128
Key type pointer for AES-128 based keys.
Definition mcuxClAes_KeyTypes.h:51
#define MCUXCLBUFFER_INIT(name, info, ptr, size)
Initialize an input/output buffer (mcuxCl_Buffer_t).
Definition mcuxClBuffer.h:67
#define MCUXCLBUFFER_INIT_RO(name, info, ptr, size)
Initialize an input buffer (mcuxCl_InputBuffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:84
#define MCUXCLBUFFER_UPDATE(name, offset)
Update the buffer pointer with the given offset.
Definition mcuxClBuffer.h:201
#define MCUXCLBUFFER_SET(name, ptr, size)
Update the buffer pointer the a new memory location.
Definition mcuxClBuffer.h:240
const uint8_t * mcuxCl_InputBuffer_t
Input buffer type.
Definition mcuxClBuffer_Pointer.h:38
#define MCUXCLCIPHER_STATUS_OK
Blocking operation finished successfully.
Definition mcuxClCipher_Constants.h:35
mcuxClCipher_Status_t mcuxClCipher_process(mcuxClSession_Handle_t session, mcuxClCipher_Context_t *const pContext, mcuxCl_InputBuffer_t pIn, uint32_t inLength, mcuxCl_Buffer_t pOut, uint32_t *const pOutLength)
Multi-part encryption/decryption processing function.
mcuxClCipher_Status_t mcuxClCipher_init_encrypt(mcuxClSession_Handle_t session, mcuxClCipher_Context_t *const pContext, mcuxClKey_Handle_t key, mcuxClCipher_Mode_t mode, mcuxCl_InputBuffer_t pIv, uint32_t ivLength)
Multi-part encryption initialization function.
mcuxClCipher_Status_t mcuxClCipher_finish(mcuxClSession_Handle_t session, mcuxClCipher_Context_t *const pContext, mcuxCl_Buffer_t pOut, uint32_t *const pOutLength)
Multi-part encryption/decryption finalization function.
mcuxClCipher_Status_t mcuxClCipher_init_decrypt(mcuxClSession_Handle_t session, mcuxClCipher_Context_t *const pContext, mcuxClKey_Handle_t key, mcuxClCipher_Mode_t mode, mcuxCl_InputBuffer_t pIv, uint32_t ivLength)
Multi-part decryption initialization function.
struct mcuxClCipher_Context mcuxClCipher_Context_t
Cipher context type.
Definition mcuxClCipher_Types.h:100
static mcuxClCipher_Mode_t mcuxClCipher_Mode_AES_CBC_PaddingISO9797_1_Method2
AES-CBC mode with ISO/IEC 9797-1 padding method 2.
Definition mcuxClCipherModes_Modes.h:229
#define MCUXCLKEY_STATUS_OK
Key operation successful.
Definition mcuxClKey_Constants.h:40
mcuxClKey_Status_t mcuxClKey_init(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClKey_Type_t type, const uint8_t *pKeyData, uint32_t keyDataLength)
Initializes a key handle.
mcuxClKey_Descriptor_t *const mcuxClKey_Handle_t
Key handle type.
Definition mcuxClKey_Types.h:91
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658