Example for the mcuxClCipherModes component.
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_Session_Helper.h>
#include <mcuxClExample_RNG_Helper.h>
static const uint8_t plain[64] = {
0x6bu, 0xc1u, 0xbeu, 0xe2u, 0x2eu, 0x40u, 0x9fu, 0x96u,
0xe9u, 0x3du, 0x7eu, 0x11u, 0x73u, 0x93u, 0x17u, 0x2au,
0xaeu, 0x2du, 0x8au, 0x57u, 0x1eu, 0x03u, 0xacu, 0x9cu,
0x9eu, 0xb7u, 0x6fu, 0xacu, 0x45u, 0xafu, 0x8eu, 0x51u,
0x30u, 0xc8u, 0x1cu, 0x46u, 0xa3u, 0x5cu, 0xe4u, 0x11u,
0xe5u, 0xfbu, 0xc1u, 0x19u, 0x1au, 0x0au, 0x52u, 0xefu,
0xf6u, 0x9fu, 0x24u, 0x45u, 0xdfu, 0x4fu, 0x9bu, 0x17u,
0xadu, 0x2bu, 0x41u, 0x7bu, 0xe6u, 0x6cu, 0x37u, 0x10u
};
static const uint8_t encryptedRef[64] = {
0x87u, 0x4du, 0x61u, 0x91u, 0xb6u, 0x20u, 0xe3u, 0x26u,
0x1bu, 0xefu, 0x68u, 0x64u, 0x99u, 0x0du, 0xb6u, 0xceu,
0x98u, 0x06u, 0xf6u, 0x6bu, 0x79u, 0x70u, 0xfdu, 0xffu,
0x86u, 0x17u, 0x18u, 0x7bu, 0xb9u, 0xffu, 0xfdu, 0xffu,
0x5au, 0xe4u, 0xdfu, 0x3eu, 0xdbu, 0xd5u, 0xd3u, 0x5eu,
0x5bu, 0x4fu, 0x09u, 0x02u, 0x0du, 0xb0u, 0x3eu, 0xabu,
0x1eu, 0x03u, 0x1du, 0xdau, 0x2fu, 0xbeu, 0x03u, 0xd1u,
0x79u, 0x21u, 0x70u, 0xa0u, 0xf3u, 0x00u, 0x9cu, 0xeeu
};
static const uint8_t keyBytes[16] = {
0x2bu, 0x7eu, 0x15u, 0x16u, 0x28u, 0xaeu, 0xd2u, 0xa6u,
0xabu, 0xf7u, 0x15u, 0x88u, 0x09u, 0xcfu, 0x4fu, 0x3cu
};
static const uint8_t iv[16] = {
0xf0u, 0xf1u, 0xf2u, 0xf3u, 0xf4u, 0xf5u, 0xf6u, 0xf7u,
0xf8u, 0xf9u, 0xfau, 0xfbu, 0xfcu, 0xfdu, 0xfeu, 0xffu
};
MCUXCLEXAMPLE_FUNCTION(mcuxClCipherModes_Ctr_Aes128_Oneshot_example)
{
mcuxClSession_Descriptor_t sessionDesc;
#define MCUXCLCIPHERMODES_CPU_WA MCUXCLEXAMPLE_MAX_WA(MCUXCLCIPHER_AES_ENCRYPT_CPU_WA_BUFFER_SIZE, MCUXCLCIPHER_AES_DECRYPT_CPU_WA_BUFFER_SIZE)
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION(session, MCUXCLEXAMPLE_MAX_WA(MCUXCLCIPHERMODES_CPU_WA, MCUXCLRANDOM_NCINIT_WACPU_SIZE), 0u);
MCUXCLEXAMPLE_INITIALIZE_PRNG(session);
uint32_t keyDesc[MCUXCLKEY_DESCRIPTOR_SIZE_IN_WORDS];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
session,
key,
keyBytes,
sizeof(keyBytes))
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
uint32_t encryptedSize = 0u;
uint8_t encryptedData[sizeof(encryptedRef)];
session,
key,
ivBuf,
sizeof(iv),
plainBuf,
sizeof(plain),
encryptedDataBuf,
&encryptedSize)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
uint32_t decryptedSize = 0u;
uint8_t decryptedData[sizeof(plain)];
session,
key,
ivBuf,
sizeof(iv),
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by MCUXCLBUFFER_INIT")
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
encryptedSize,
decryptedDataBuf,
&decryptedSize)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(encryptedSize != sizeof(plain))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(encryptedSize != decryptedSize)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("encryptedData initialized by mcuxClCipher_encrypt")
if(!mcuxClCore_assertEqual(encryptedRef, encryptedData, sizeof(plain)))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
if(sizeof(plain) != decryptedSize)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("decryptedData initialized by mcuxClCipher_decrypt")
if(!mcuxClCore_assertEqual(plain, decryptedData, sizeof(plain)))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
return MCUXCLEXAMPLE_STATUS_OK;
}
Top-level include file for the mcuxClAes component.
Top-level include file for the mcuxClBuffer component.
Top-level include file for the mcuxClCipher component.
Top-level include file for the mcuxClCipherModes component.
Definition of function identifiers for the flow protection mechanism.
Top-level include file for the mcuxClKey component.
Top-level include file for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.
static const mcuxClKey_Type_t mcuxClKey_Type_Aes128
Key type pointer for AES-128 based keys.
Definition mcuxClAes_KeyTypes.h:51
#define MCUXCLBUFFER_INIT(name, info, ptr, size)
Initialize an input/output buffer (mcuxCl_Buffer_t).
Definition mcuxClBuffer.h:67
#define MCUXCLBUFFER_INIT_RO(name, info, ptr, size)
Initialize an input buffer (mcuxCl_InputBuffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:84
uint8_t * mcuxCl_Buffer_t
Input/output buffer type.
Definition mcuxClBuffer_Pointer.h:47
#define MCUXCLCIPHER_STATUS_OK
Blocking operation finished successfully.
Definition mcuxClCipher_Constants.h:35
mcuxClCipher_Status_t mcuxClCipher_encrypt(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClCipher_Mode_t mode, mcuxCl_InputBuffer_t pIv, uint32_t ivLength, mcuxCl_InputBuffer_t pIn, uint32_t inLength, mcuxCl_Buffer_t pOut, uint32_t *const pOutLength)
One-shot encryption function.
mcuxClCipher_Status_t mcuxClCipher_decrypt(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClCipher_Mode_t mode, mcuxCl_InputBuffer_t pIv, uint32_t ivLength, mcuxCl_InputBuffer_t pIn, uint32_t inLength, mcuxCl_Buffer_t pOut, uint32_t *const pOutLength)
One-shot decryption function.
static mcuxClCipher_Mode_t mcuxClCipher_Mode_AES_CTR
AES-CTR mode.
Definition mcuxClCipherModes_Modes.h:347
#define MCUXCLKEY_STATUS_OK
Key operation successful.
Definition mcuxClKey_Constants.h:40
mcuxClKey_Status_t mcuxClKey_init(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClKey_Type_t type, const uint8_t *pKeyData, uint32_t keyDataLength)
Initializes a key handle.
mcuxClKey_Descriptor_t *const mcuxClKey_Handle_t
Key handle type.
Definition mcuxClKey_Types.h:91
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658