MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClCipherModes_Ecb_Aes128_Multipart_PaddingZero_Dma_NonBlocking_example.c

Example for the mcuxClCipherModes component.

Example for the mcuxClCipherModes component

/*--------------------------------------------------------------------------*/
/* Copyright 2023-2026 NXP */
/* */
/* NXP Confidential and Proprietary. This software is owned or controlled */
/* by NXP and may only be used strictly in accordance with the applicable */
/* license terms. By expressly accepting such terms or by downloading, */
/* installing, activating and/or otherwise using the software, you are */
/* agreeing that you have read, and that you agree to comply with and are */
/* bound by, such license terms. If you do not agree to be bound by the */
/* applicable license terms, then you may not retain, install, activate or */
/* otherwise use the software. */
/*--------------------------------------------------------------------------*/
#include <mcuxClToolchain.h>
#include <mcuxClSession.h>
#include <mcuxClKey.h>
#include <mcuxClAes.h> // Interface to AES-related definitions and types
#include <mcuxClCipher.h> // Interface to the entire mcuxClCipher component
#include <mcuxClCipherModes.h> // Interface to the entire mcuxClCipherModes component
#include <mcuxClCore_FunctionIdentifiers.h> // Code flow protection
#include <mcuxClBuffer.h>
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_OS.h>
#include <mcuxClExample_Session_Helper.h>
#include <mcuxClExample_RNG_Helper.h>
#include <platform_specific_headers.h> // needed for DMA interrupts
/************************************************************************************/
/* Reference data to process and check results */
/************************************************************************************/
/* ECB encrypted data */
static const uint8_t encryptedRef[64] = {
0x82u, 0x4fu, 0x7au, 0xb3u, 0xdfu, 0x5eu, 0x73u, 0x42u,
0x35u, 0xbbu, 0xcfu, 0xeau, 0xdau, 0x7eu, 0x74u, 0xc1u,
0x7au, 0x08u, 0x34u, 0x2du, 0x49u, 0xacu, 0xadu, 0x72u,
0x0eu, 0xb3u, 0x23u, 0xb6u, 0x49u, 0x42u, 0x01u, 0xf2u,
0x06u, 0x87u, 0x58u, 0xcfu, 0x41u, 0xb0u, 0xd6u, 0x63u,
0x66u, 0x50u, 0x1bu, 0xe8u, 0x05u, 0x66u, 0xa8u, 0xfbu,
0x34u, 0x58u, 0x0fu, 0x26u, 0x91u, 0x9du, 0x02u, 0x75u,
0xf7u, 0x2du, 0x90u, 0x97u, 0x0eu, 0xf3u, 0x9du, 0x7bu
};
/* Decrypted zero padded data */
static const uint8_t decryptedRef[64] = {
0x61u, 0x62u, 0x63u, 0x64u, 0x65u, 0x66u, 0x67u, 0x68u,
0x69u, 0x6Au, 0x6Bu, 0x6Cu, 0x6Du, 0x6Eu, 0x6Fu, 0x70u,
0x62u, 0x63u, 0x64u, 0x65u, 0x66u, 0x67u, 0x68u, 0x69u,
0x6Au, 0x6Bu, 0x6Cu, 0x6Du, 0x6Eu, 0x6Fu, 0x70u, 0x71u,
0x63u, 0x64u, 0x65u, 0x66u, 0x67u, 0x68u, 0x69u, 0x6Au,
0x6Bu, 0x6Cu, 0x6Du, 0x6Eu, 0x6Fu, 0x70u, 0x71u, 0x72u,
0x64u, 0x65u, 0x66u, 0x67u, 0x68u, 0x69u, 0x6Au, 0x6Bu,
0x6Cu, 0x6Du, 0x6Eu, 0x6Fu, 0x70u, 0x71u, 0x00u, 0x00u
};
static const uint8_t keyBytes[16] = {
0x6Bu, 0x6Cu, 0x6Du, 0x6Eu, 0x6Fu, 0x70u, 0x71u, 0x72u,
0x73u, 0x74u, 0x75u, 0x76u, 0x77u, 0x78u, 0x79u, 0x7Au,
};
/************************************************************************************/
/* Helper code to synchronize example flow with nonBlocking background computation */
/************************************************************************************/
#define MCUXCLCIPHER_STATUS_CALLBACK_NOT_EXECUTED ((uint32_t) 0xDEADBEEFu)
/* This variable is used to keep track of callbacks triggered by the non-blocking API. */
static volatile uint32_t cipherStatus_nonBlockingCallback = MCUXCLCIPHER_STATUS_CALLBACK_NOT_EXECUTED;
/* This function is called after the nonBlocking operation has finished */
static void user_callback(uint32_t status, void * data)
{
(void)data;
cipherStatus_nonBlockingCallback = status;
}
#define MCUXCLCIPHER_FLAG_DMA_INTERRUPT_NOT_TRIGGERED ((uint32_t) 0xDEADBEEFu)
/* This variable is a flag to notify the caller that an interrupt happened.
It will contain the DMA channel ID of the respective channel that had an interrupt. */
static volatile uint32_t flag_interruptNumber = MCUXCLCIPHER_FLAG_DMA_INTERRUPT_NOT_TRIGGERED;
/**************************************************************************/
/* Interrupt configuration code */
/**************************************************************************/
/* Global resource context to handle status and session for the available HW resources.
It shall be global and therefor only allocated once, for all sessions.
Note that the examples create a "static" version of this global context, which is done
solely to make sure examples are self-contained and do not conflict with each other. */
/* TODO CLNS-16969: Use one global resource ctx for all examples */
static uint32_t resourceContext[MCUXCLRESOURCE_CONTEXT_SIZE/sizeof(uint32_t)];
static mcuxClResource_Context_t * resourceCtxHandle = (mcuxClResource_Context_t *) &resourceContext;
/* This is the Interrupt handler for DMA done and error interrupts on the input channel.
This function only sets the interrupt number as a global flag, the actual handler
mcuxClResource_handle_interrupt needs to be called afterwards to wrap-up the CLib operation. */
static void handleDmaInterrupt_channel0(void)
{
MCUX_CSSL_ANALYSIS_START_PATTERN_SFR_ACCESS()
/* Clear DMA interrupt request status, W1C. Needed for DONE interrupts. */
DMA0->CH[0].CH_INT = 1U;
/* Clear the DMA error interrupt request status, W1C. Needed for ERROR interrupts. */
uint32_t chCsr = DMA0->CH[0].CH_CSR;
/* 1. Unset the DONE bit, to not accidentally perform a W1C. CLib needs this bit for internal checks. */
chCsr &= ~((uint32_t)DMA_CH_CSR_DONE_MASK);
/* 2. Clear the EEI bit. */
chCsr &= ~((uint32_t)DMA_CH_CSR_EEI_MASK);
/* 3. Write to CH_CSR */
DMA0->CH[0].CH_CSR = chCsr;
MCUX_CSSL_ANALYSIS_STOP_PATTERN_SFR_ACCESS()
/* DMA_CH0 caused the interrupt */
flag_interruptNumber = GET_DMA_CHX_IRQ_NUMBER(0U);
}
/* This is the Interrupt handler for DMA done and error interrupts on the output channel.
This function only sets the interrupt number as a global flag, the actual handler
mcuxClResource_handle_interrupt needs to be called afterwards to wrap-up the CLib operation. */
static void handleDmaInterrupt_channel1(void)
{
MCUX_CSSL_ANALYSIS_START_PATTERN_SFR_ACCESS()
/* Clear DMA interrupt request status, W1C. Needed for DONE interrupts. */
DMA0->CH[1].CH_INT = 1U;
/* Clear the DMA error interrupt request status, W1C. Needed for ERROR interrupts. */
uint32_t chCsr = DMA0->CH[1].CH_CSR;
/* 1. Unset the DONE bit, to not accidentally perform a W1C. CLib needs this bit for internal checks. */
chCsr &= ~((uint32_t)DMA_CH_CSR_DONE_MASK);
/* 2. Clear the EEI bit. */
chCsr &= ~((uint32_t)DMA_CH_CSR_EEI_MASK);
/* 3. Write to CH_CSR */
DMA0->CH[1].CH_CSR = chCsr;
MCUX_CSSL_ANALYSIS_STOP_PATTERN_SFR_ACCESS()
/* DMA_CH1 caused the interrupt */
flag_interruptNumber = GET_DMA_CHX_IRQ_NUMBER(1U);
}
/* Initialize (install, enable) the interrupts */
static void interruptInit(void)
{
/* Enable interrupts for the input channel */
mcuxClExample_OS_Interrupt_Callback_Install(handleDmaInterrupt_channel0, GET_DMA_CHX_IRQ_NUMBER(0U));
/* Enable interrupts for the output channel */
mcuxClExample_OS_Interrupt_Callback_Install(handleDmaInterrupt_channel1, GET_DMA_CHX_IRQ_NUMBER(1U));
/* Enable the interrupts in the controller */
mcuxClExample_OS_Interrupt_Enable(GET_DMA_CHX_IRQ_NUMBER(0U));
mcuxClExample_OS_Interrupt_Enable(GET_DMA_CHX_IRQ_NUMBER(1U));
}
/* Uninitialize (disable) the interrupts */
static void interruptUninit(void)
{
/* Disable the interrupts in the controller */
mcuxClExample_OS_Interrupt_Disable(GET_DMA_CHX_IRQ_NUMBER(0U));
mcuxClExample_OS_Interrupt_Disable(GET_DMA_CHX_IRQ_NUMBER(1U));
}
/***************************************************************************/
/* Example for non-blocking multipart ECB encryption and decryption */
/* with zero padding */
/* */
/* The example shows which functions need to be called to configure the */
/* non-blocking flow. Its important that the interrupt is triggered on */
/* input channel. To show the non-blocking interrupt flow a polling-loop */
/* is used to wait for the user-callback to be triggered by an interrupt. */
/***************************************************************************/
MCUXCLEXAMPLE_FUNCTION(mcuxClCipherModes_Ecb_Aes128_Multipart_PaddingZero_Dma_NonBlocking_example)
{
/**************************************************************************/
/* General Preparation */
/**************************************************************************/
/* Enable DMA interrupt and set callback */
interruptInit();
/* Note: input buffer needs to be on the stack because DMA cannot access ROM */
const uint8_t plain[62] = {
0x61u, 0x62u, 0x63u, 0x64u, 0x65u, 0x66u, 0x67u, 0x68u,
0x69u, 0x6Au, 0x6Bu, 0x6Cu, 0x6Du, 0x6Eu, 0x6Fu, 0x70u,
0x62u, 0x63u, 0x64u, 0x65u, 0x66u, 0x67u, 0x68u, 0x69u,
0x6Au, 0x6Bu, 0x6Cu, 0x6Du, 0x6Eu, 0x6Fu, 0x70u, 0x71u,
0x63u, 0x64u, 0x65u, 0x66u, 0x67u, 0x68u, 0x69u, 0x6Au,
0x6Bu, 0x6Cu, 0x6Du, 0x6Eu, 0x6Fu, 0x70u, 0x71u, 0x72u,
0x64u, 0x65u, 0x66u, 0x67u, 0x68u, 0x69u, 0x6Au, 0x6Bu,
0x6Cu, 0x6Du, 0x6Eu, 0x6Fu, 0x70u, 0x71u
};
mcuxClSession_Descriptor_t sessionDesc;
mcuxClSession_Handle_t session = &sessionDesc;
/* Allocate and initialize session */
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION_NONBLOCKING(session, MCUXCLEXAMPLE_MAX_WA(MCUXCLCIPHER_AES_PROCESS_CPU_WA_BUFFER_SIZE, MCUXCLRANDOM_NCINIT_WACPU_SIZE), 0u);
/* Initialize the PRNG */
MCUXCLEXAMPLE_INITIALIZE_PRNG(session);
/* Initialize the key */
uint32_t keyDesc[MCUXCLKEY_DESCRIPTOR_SIZE_IN_WORDS];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClKey_Handle_t key: */ key,
/* mcuxClKey_Type_t type: */ mcuxClKey_Type_Aes128,
/* uint8_t * pKeyData: */ keyBytes,
/* uint32_t keyDataLength: */ sizeof(keyBytes))
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/**************************************************************************/
/* Non-Blocking Preparation */
/**************************************************************************/
/* Configure the DMA channels that should be used.
* Use DMA channel 0 for HW input operations, and DMA channel 1 for HW output operations */
mcuxClSession_Channels_t dmaChannels = {
.input = (mcuxClSession_Channel_t) 0u,
.output = (mcuxClSession_Channel_t) 1u
};
/* Set DMA channels and user callback function */
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClSession_Channels_t dmaChannels, */ dmaChannels,
/* mcuxClSession_Callback_t pUserCallback, */ user_callback,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_NULL_POINTER_CONSTANT("NULL is used in code")
/* void * pUserData */ NULL)
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_NULL_POINTER_CONSTANT()
);
/* Initialize resource context and add it to the session */
if(!mcuxClExample_Session_InitAndSetResourceCtx(session, resourceCtxHandle))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/**************************************************************************/
/* Encryption */
/**************************************************************************/
uint32_t outLength = 0u;
uint32_t encryptedSize = 0u;
uint8_t encryptedData[sizeof(encryptedRef)];
/* Create a buffer for the context */
ALIGNED uint8_t ctxBuf[MCUXCLCIPHER_AES_CONTEXT_SIZE];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
/* Multipart encrypt init */
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClCipher_Context_t * const pContext:*/ ctx,
/* const mcuxClKey_Handle_t key: */ key,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_NULL_POINTER_CONSTANT("NULL is used in code")
/* mcuxCl_InputBuffer_t pIv: */ NULL,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_NULL_POINTER_CONSTANT()
/* uint32_t ivLength: */ 0)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUXCLBUFFER_INIT_DMA_RO(plainBuf, session, plain, sizeof(plain));
MCUXCLBUFFER_INIT_DMA(encryptedDataBuf, session, encryptedData, sizeof(encryptedData));
/* Multipart encrypt process */
/* mcuxClSession_Handle_t session: */ session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClCipher_init_encrypt")
/* mcuxClCipher_Context_t * const pContext:*/ ctx,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
/* mcuxCl_InputBuffer_t pIn: */ plainBuf,
/* uint32_t inLength: */ sizeof(plain),
/* mcuxCl_Buffer_t pOut: */ encryptedDataBuf,
/* uint32_t * const outLength: */ &outLength)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
{
/* A non-blocking job was started. Wait for the interrupt */
while(MCUXCLCIPHER_FLAG_DMA_INTERRUPT_NOT_TRIGGERED == flag_interruptNumber) {};
/* Call the resource interrupt handler to finish the non-blocking operation.
* On normal operation flow, this will trigger the user_callback function at the end,
* which sets cipherStatus_nonBlockingCallback to the status code of the Cipher operation.
* On error, mcuxClResource_handle_interrupt returns an ERROR code without triggering
* the user_callback. */
MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(rhi_status, rhi_token, mcuxClResource_handle_interrupt(resourceCtxHandle, flag_interruptNumber));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(MCUXCLCIPHER_STATUS_JOB_COMPLETED != cipherStatus_nonBlockingCallback)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* Reset polling loop condition and the status code */
flag_interruptNumber = MCUXCLCIPHER_FLAG_DMA_INTERRUPT_NOT_TRIGGERED;
cipherStatus_nonBlockingCallback = MCUXCLCIPHER_STATUS_CALLBACK_NOT_EXECUTED;
}
MCUX_CSSL_ANALYSIS_START_SUPPRESS_INTEGER_OVERFLOW("Calculation does not overflow")
encryptedSize += outLength;
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_INTEGER_OVERFLOW()
MCUXCLBUFFER_UPDATE(encryptedDataBuf, encryptedSize);
/* Multipart encrypt finish */
/* mcuxClSession_Handle_t session: */ session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClCipher_init_encrypt")
/* mcuxClCipher_Context_t * const pContext:*/ ctx,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
/* mcuxCl_Buffer_t pOut: */ encryptedDataBuf,
/* uint32_t * const outLength: */ &outLength)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUX_CSSL_ANALYSIS_START_SUPPRESS_INTEGER_OVERFLOW("Calculation does not overflow")
encryptedSize += outLength;
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_INTEGER_OVERFLOW()
/**************************************************************************/
/* Decryption */
/**************************************************************************/
uint32_t decryptedSize = 0u;
uint8_t decryptedData[sizeof(decryptedRef)];
/* Multipart decrypt init */
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClCipher_Context_t * const pContext:*/ ctx,
/* const mcuxClKey_Handle_t key: */ key,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_NULL_POINTER_CONSTANT("NULL is used in code")
/* mcuxCl_InputBuffer_t pIv: */ NULL,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_NULL_POINTER_CONSTANT()
/* uint32_t ivLength: */ 0)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUXCLBUFFER_SET(encryptedDataBuf, encryptedData, sizeof(encryptedData) /* unused */);
MCUXCLBUFFER_INIT_DMA(decryptedDataBuf, session, decryptedData, sizeof(decryptedData));
/* Multipart decrypt process */
/* mcuxClSession_Handle_t session: */ session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClCipher_init_decrypt")
/* mcuxClCipher_Context_t * const pContext:*/ ctx,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
/* mcuxCl_InputBuffer_t pIn: */ (mcuxCl_InputBuffer_t) encryptedDataBuf,
/* uint32_t inLength: */ encryptedSize,
/* mcuxCl_Buffer_t pOut: */ decryptedDataBuf,
/* uint32_t * const outLength: */ &outLength)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
{
/* A non-blocking job was started. Wait for the interrupt */
while(MCUXCLCIPHER_FLAG_DMA_INTERRUPT_NOT_TRIGGERED == flag_interruptNumber) {};
/* Call the resource interrupt handler to finish the non-blocking operation.
* On normal operation flow, this will trigger the user_callback function at the end,
* which sets cipherStatus_nonBlockingCallback to the status code of the Cipher operation.
* On error, mcuxClResource_handle_interrupt returns an ERROR code without triggering
* the user_callback. */
MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(rhi_status, rhi_token, mcuxClResource_handle_interrupt(resourceCtxHandle, flag_interruptNumber));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(MCUXCLCIPHER_STATUS_JOB_COMPLETED != cipherStatus_nonBlockingCallback)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* Reset polling loop condition and the status code */
flag_interruptNumber = MCUXCLCIPHER_FLAG_DMA_INTERRUPT_NOT_TRIGGERED;
cipherStatus_nonBlockingCallback = MCUXCLCIPHER_STATUS_CALLBACK_NOT_EXECUTED;
}
MCUX_CSSL_ANALYSIS_START_SUPPRESS_INTEGER_OVERFLOW("Calculation does not overflow")
decryptedSize += outLength;
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_INTEGER_OVERFLOW()
MCUXCLBUFFER_UPDATE(decryptedDataBuf, decryptedSize);
/* Multipart decrypt finish */
/* mcuxClSession_Handle_t session: */ session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClCipher_init_decrypt")
/* mcuxClCipher_Context_t * const pContext:*/ ctx,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
/* mcuxCl_Buffer_t pOut: */ decryptedDataBuf,
/* uint32_t * const outLength: */ &outLength)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUX_CSSL_ANALYSIS_START_SUPPRESS_INTEGER_OVERFLOW("Calculation does not overflow")
decryptedSize += outLength;
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_INTEGER_OVERFLOW()
/**************************************************************************/
/* Destroy the current session and clean-up */
/**************************************************************************/
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* Disable the interrupts */
interruptUninit();
/**************************************************************************/
/* Verification */
/**************************************************************************/
if(sizeof(encryptedRef) != encryptedSize)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(!mcuxClCore_assertEqual(encryptedRef, encryptedData, sizeof(encryptedRef)))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(sizeof(decryptedRef) != decryptedSize)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by MCUXCLBUFFER_INIT_DMA")
if(!mcuxClCore_assertEqual(decryptedRef, decryptedData, sizeof(decryptedRef)))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
return MCUXCLEXAMPLE_STATUS_OK;
}
Top-level include file for the mcuxClAes component.
Top-level include file for the mcuxClBuffer component.
Top-level include file for the mcuxClCipher component.
Top-level include file for the mcuxClCipherModes component.
Definition of function identifiers for the flow protection mechanism.
Top-level include file for the mcuxClKey component.
Top-level include file for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.
#define MCUXCLRESOURCE_CONTEXT_SIZE
Size (in bytes) of mcuxClResource context.
Definition mcuxClResource_MemoryConsumption.h:24
static const mcuxClKey_Type_t mcuxClKey_Type_Aes128
Key type pointer for AES-128 based keys.
Definition mcuxClAes_KeyTypes.h:51
#define MCUXCLBUFFER_INIT_DMA(name, info, ptr, size)
Initialize an input/output buffer (mcuxCl_Buffer_t) with DMA handling.
Definition mcuxClBuffer.h:157
#define MCUXCLBUFFER_INIT_DMA_RO(name, info, ptr, size)
Initialize an input buffer (mcuxCl_InputBuffer_t) with DMA handling.
Definition mcuxClBuffer.h:120
#define MCUXCLBUFFER_UPDATE(name, offset)
Update the buffer pointer with the given offset.
Definition mcuxClBuffer.h:201
#define MCUXCLBUFFER_SET(name, ptr, size)
Update the buffer pointer the a new memory location.
Definition mcuxClBuffer.h:240
const uint8_t * mcuxCl_InputBuffer_t
Input buffer type.
Definition mcuxClBuffer_Pointer.h:38
#define MCUXCLCIPHER_STATUS_JOB_COMPLETED
Non-blocking operation finished successfully.
Definition mcuxClCipher_Constants.h:37
#define MCUXCLCIPHER_STATUS_JOB_STARTED
Non-blocking operation started successfully.
Definition mcuxClCipher_Constants.h:36
#define MCUXCLCIPHER_STATUS_OK
Blocking operation finished successfully.
Definition mcuxClCipher_Constants.h:35
mcuxClCipher_Status_t mcuxClCipher_process(mcuxClSession_Handle_t session, mcuxClCipher_Context_t *const pContext, mcuxCl_InputBuffer_t pIn, uint32_t inLength, mcuxCl_Buffer_t pOut, uint32_t *const pOutLength)
Multi-part encryption/decryption processing function.
mcuxClCipher_Status_t mcuxClCipher_init_encrypt(mcuxClSession_Handle_t session, mcuxClCipher_Context_t *const pContext, mcuxClKey_Handle_t key, mcuxClCipher_Mode_t mode, mcuxCl_InputBuffer_t pIv, uint32_t ivLength)
Multi-part encryption initialization function.
mcuxClCipher_Status_t mcuxClCipher_finish(mcuxClSession_Handle_t session, mcuxClCipher_Context_t *const pContext, mcuxCl_Buffer_t pOut, uint32_t *const pOutLength)
Multi-part encryption/decryption finalization function.
mcuxClCipher_Status_t mcuxClCipher_init_decrypt(mcuxClSession_Handle_t session, mcuxClCipher_Context_t *const pContext, mcuxClKey_Handle_t key, mcuxClCipher_Mode_t mode, mcuxCl_InputBuffer_t pIv, uint32_t ivLength)
Multi-part decryption initialization function.
struct mcuxClCipher_Context mcuxClCipher_Context_t
Cipher context type.
Definition mcuxClCipher_Types.h:100
static mcuxClCipher_Mode_t mcuxClCipher_Mode_AES_ECB_PaddingISO9797_1_Method1_NonBlocking
AES-ECB mode with ISO/IEC 9797-1 padding method 1, non-blocking API, using the DMA for I/O operations...
Definition mcuxClCipherModes_Modes.h:140
#define MCUXCLKEY_STATUS_OK
Key operation successful.
Definition mcuxClKey_Constants.h:40
mcuxClKey_Status_t mcuxClKey_init(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClKey_Type_t type, const uint8_t *pKeyData, uint32_t keyDataLength)
Initializes a key handle.
mcuxClKey_Descriptor_t *const mcuxClKey_Handle_t
Key handle type.
Definition mcuxClKey_Types.h:91
mcuxClResource_Status_t mcuxClResource_handle_interrupt(const mcuxClResource_Context_t *pResourceCtx, mcuxClResource_Interrupt_t interrupt)
Resource interrupt handler.
struct mcuxClResource_Context mcuxClResource_Context_t
Resource context type.
Definition mcuxClResource_Types.h:47
#define MCUXCLRESOURCE_STATUS_OK
Resource operation successful.
Definition mcuxClResource_Types.h:82
mcuxClSession_Status_t mcuxClSession_configure_job(mcuxClSession_Handle_t session, mcuxClSession_Channels_t dmaChannels, mcuxClSession_Callback_t pUserCallback, void *pUserData)
Configure the parameters for non-blocking operations (jobs) in this session.
#define MCUXCLSESSION_STATUS_OK
Session operation successful.
Definition mcuxClSession_Types.h:39
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
uint16_t mcuxClSession_Channel_t
Session channel type.
Definition mcuxClSession_Types.h:105
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658
Session channels type.
Definition mcuxClSession_Types.h:113