Example for the mcuxClEcc component.
#include <mcuxClToolchain.h>
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_Session_Helper.h>
#include <mcuxClExample_RNG_Helper.h>
#define BN256_BYTE_LEN_P (32u)
#define BN256_BYTE_LEN_N (32u)
static const ALIGNED uint8_t BN_P256_P[BN256_BYTE_LEN_P] =
{
0xFFu, 0xFFu, 0xFFu, 0xFFu, 0xFFu, 0xFCu, 0xF0u, 0xCDu,
0x46u, 0xE5u, 0xF2u, 0x5Eu, 0xEEu, 0x71u, 0xA4u, 0x9Fu,
0x0Cu, 0xDCu, 0x65u, 0xFBu, 0x12u, 0x98u, 0x0Au, 0x82u,
0xD3u, 0x29u, 0x2Du, 0xDBu, 0xAEu, 0xD3u, 0x30u, 0x13u};
static const ALIGNED uint8_t BN_P256_A[BN256_BYTE_LEN_P] =
{
0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u,
0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u,
0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u,
0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u
};
static const ALIGNED uint8_t BN_P256_B[BN256_BYTE_LEN_P] =
{
0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u,
0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u,
0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u,
0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x03u
};
static const ALIGNED uint8_t BN_P256_G[2u * BN256_BYTE_LEN_P] =
{
0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u,
0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u,
0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u,
0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x01u,
0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u,
0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u,
0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u,
0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x00u, 0x02u
};
static const ALIGNED uint8_t BN_P256_N[BN256_BYTE_LEN_N] =
{
0xFFu, 0xFFu, 0xFFu, 0xFFu, 0xFFu, 0xFCu, 0xF0u, 0xCDu,
0x46u, 0xE5u, 0xF2u, 0x5Eu, 0xEEu, 0x71u, 0xA4u, 0x9Eu,
0x0Cu, 0xDCu, 0x65u, 0xFBu, 0x12u, 0x99u, 0x92u, 0x1Au,
0xF6u, 0x2Du, 0x53u, 0x6Cu, 0xD1u, 0x0Bu, 0x50u, 0x0Du
};
#define MAX_CPUWA_SIZE MCUXCLCORE_MAX(MCUXCLRANDOM_NCINIT_WACPU_SIZE, \
MCUXCLCORE_MAX(MCUXCLRANDOMMODES_INIT_WACPU_SIZE, \
MCUXCLCORE_MAX(MCUXCLECC_WEIERECC_GENERATEDOMAINPARAMS_WACPU_SIZE, \
MCUXCLKEY_GENERATEKEYPAIR_WEIERECC_WACPU_SIZE)))
#define MAX_PKCWA_SIZE MCUXCLCORE_MAX(MCUXCLECC_WEIERECC_GENERATEDOMAINPARAMS_WAPKC_SIZE_256, \
MCUXCLKEY_GENERATEKEYPAIR_WEIERECC_WAPKC_SIZE_256)
MCUXCLEXAMPLE_FUNCTION(mcuxClEcc_WeierECC_CustomEccWeierType_BN256_example)
{
mcuxClSession_Descriptor_t sessionDesc;
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION(session, MAX_CPUWA_SIZE, MAX_PKCWA_SIZE);
EccWeierBasicDomainParams.
pP = buffP;
EccWeierBasicDomainParams.
pLen = BN256_BYTE_LEN_P;
EccWeierBasicDomainParams.
pA = buffA;
EccWeierBasicDomainParams.
pB = buffB;
EccWeierBasicDomainParams.
pG = buffG;
EccWeierBasicDomainParams.
pN = buffN;
EccWeierBasicDomainParams.
nLen = BN256_BYTE_LEN_N;
pEccWeierDomainParams,
&EccWeierBasicDomainParams,
MCUXCLECC_OPTION_GENERATEPRECPOINT_YES)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
uint32_t customPrivKeyTypeDescriptor[MCUXCLKEY_CUSTOMTYPEDESCRIPTOR_SIZE_IN_WORDS] = {0};
customPrivKeyType,
(void *) pEccWeierDomainParams,
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
uint32_t customPubKeyTypeDescriptor[MCUXCLKEY_CUSTOMTYPEDESCRIPTOR_SIZE_IN_WORDS] = {0};
customPubKeyType,
(void *) pEccWeierDomainParams,
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
uint32_t privKeyDesc[MCUXCLKEY_DESCRIPTOR_SIZE_IN_WORDS];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
session,
privKey,
customPrivKeyType,
pPrivKeyData,
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
uint32_t pubKeyDesc[MCUXCLKEY_DESCRIPTOR_SIZE_IN_WORDS];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
ALIGNED uint8_t pPubKeyData[MCUXCLECC_WEIERECC_NIST_P256_SIZE_PUBLICKEY];
session,
pubKey,
customPubKeyType,
pPubKeyData,
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_RNG(session, MCUXCLRANDOMMODES_CTR_DRBG_AES256_CONTEXT_SIZE, mcuxClRandomModes_Mode_CtrDrbg_AES256_DRG3);
session,
privKey,
pubKey)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
return MCUXCLEXAMPLE_STATUS_OK;
}
Top-level include file for the mcuxClBuffer component.
Definition of function identifiers for the flow protection mechanism.
Top level header of mcuxClEcc component.
#define mcuxClEcc_Encoding_WeierECC_PrivateKey_Plain
Key encoding for a WeierECC private key.
Definition mcuxClEcc_KeyEncodingMechanisms.h:41
#define mcuxClEcc_Encoding_WeierECC_PublicKey_Plain
Key encoding for a WeierECC public key.
Definition mcuxClEcc_KeyEncodingMechanisms.h:50
Top-level include file for the mcuxClKey component.
Top level header of mcuxClRandom component.
Top level header of mcuxClRandomModes component.
Top-level include file for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.
#define MCUXCLBUFFER_INIT_RO(name, info, ptr, size)
Initialize an input buffer (mcuxCl_InputBuffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:84
mcuxClEcc_Status_t mcuxClEcc_WeierECC_GenerateDomainParams(mcuxClSession_Handle_t pSession, mcuxClEcc_Weier_DomainParams_t *pEccWeierDomainParams, mcuxClEcc_Weier_BasicDomainParams_t *pEccWeierBasicDomainParams, uint32_t options)
ECC Weierstrass custom domain parameter generation function.
mcuxClEcc_Status_t mcuxClEcc_WeierECC_GenerateCustomKeyType(mcuxClKey_CustomType_t customType, mcuxClKey_AlgorithmId_t algoId, mcuxClKey_Size_t size, void *pCustomParams, mcuxClKey_Encoding_t plainEncoding)
Key type constructor.
static mcuxClKey_Generation_t mcuxClKey_Generation_ECDSA
ECDSA Key generation algorithm.
Definition mcuxClEcc_KeyTypes.h:1207
struct mcuxClEcc_Weier_DomainParams mcuxClEcc_Weier_DomainParams_t
Type for Weierstrass ECC domain parameters.
Definition mcuxClEcc_Types.h:83
#define MCUXCLKEY_STATUS_OK
Key operation successful.
Definition mcuxClKey_Constants.h:40
#define MCUXCLKEY_ALGO_ID_PRIVATE_KEY
Private key.
Definition mcuxClKey_Constants.h:97
#define MCUXCLKEY_ALGO_ID_PUBLIC_KEY
Public key.
Definition mcuxClKey_Constants.h:96
#define MCUXCLKEY_ALGO_ID_ECC_SHWS_GFP_STATIC_CUSTOM
ECC key using Short Weierstrass Curve over GF(p) with static custom domain parameters.
Definition mcuxClKey_Constants.h:88
#define MCUXCLKEY_SIZE_256
256 bit key, size in bytes
Definition mcuxClKey_Constants.h:118
#define MCUXCLKEY_SIZE_512
512 bit key, size in bytes
Definition mcuxClKey_Constants.h:121
mcuxClKey_Status_t mcuxClKey_init(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClKey_Type_t type, const uint8_t *pKeyData, uint32_t keyDataLength)
Initializes a key handle.
mcuxClKey_Status_t mcuxClKey_generate_keypair(mcuxClSession_Handle_t session, mcuxClKey_Generation_t generation, mcuxClKey_Handle_t privKey, mcuxClKey_Handle_t pubKey)
Key-pair generation function.
mcuxClKey_TypeDescriptor_t * mcuxClKey_CustomType_t
Custom key type handle type.
Definition mcuxClKey_Types.h:121
mcuxClKey_Descriptor_t *const mcuxClKey_Handle_t
Key handle type.
Definition mcuxClKey_Types.h:91
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658
#define MCUXCLECC_CUSTOMWEIERECCDOMAINPARAMS_SIZE(byteLenP, byteLenN)
Define for the buffer size (in bytes) for optimized custom ECC Weierstrass domain parameters.
Definition mcuxClEcc_MemoryConsumption.h:240
#define MCUXCLECC_STATUS_OK
Operation was successful.
Definition mcuxClEcc_Constants.h:46
Structure to define basic custom domain parameters for (short) Weierstrass curves with cofactor 1.
Definition mcuxClEcc_Types.h:116