Example for the mcuxClEcc component.
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_Session_Helper.h>
static const uint8_t pCompressedPoint[MCUXCLECC_WEIERECC_BRAINPOOLP384R1_SIZE_ENCPOINT_SEC_COMPRESSED] =
{
0x03u,
0x64u, 0x60u, 0xF9u, 0x55u, 0xEFu, 0xDCu, 0xBFu, 0x3Bu,
0xF7u, 0x39u, 0x30u, 0x81u, 0xDDu, 0xF0u, 0x4Au, 0x64u,
0x74u, 0x77u, 0x81u, 0xBCu, 0x89u, 0x56u, 0xC1u, 0xE5u,
0xFFu, 0x47u, 0xBEu, 0x52u, 0x2Fu, 0x7Fu, 0x75u, 0x82u,
0x44u, 0xAEu, 0x05u, 0x4Eu, 0x91u, 0xE8u, 0xAAu, 0x16u,
0x0Cu, 0x76u, 0xDCu, 0x73u, 0x02u, 0xBCu, 0xF1u, 0x81u
};
static const uint8_t pRefDecodedPoint[MCUXCLECC_WEIERECC_BRAINPOOLP384R1_SIZE_PRIMEP * 2u] =
{
0x64u, 0x60u, 0xF9u, 0x55u, 0xEFu, 0xDCu, 0xBFu, 0x3Bu,
0xF7u, 0x39u, 0x30u, 0x81u, 0xDDu, 0xF0u, 0x4Au, 0x64u,
0x74u, 0x77u, 0x81u, 0xBCu, 0x89u, 0x56u, 0xC1u, 0xE5u,
0xFFu, 0x47u, 0xBEu, 0x52u, 0x2Fu, 0x7Fu, 0x75u, 0x82u,
0x44u, 0xAEu, 0x05u, 0x4Eu, 0x91u, 0xE8u, 0xAAu, 0x16u,
0x0Cu, 0x76u, 0xDCu, 0x73u, 0x02u, 0xBCu, 0xF1u, 0x81u,
0x7Au, 0x30u, 0xD2u, 0xAFu, 0x92u, 0x19u, 0xE4u, 0x3Du,
0x33u, 0xBEu, 0x0Bu, 0x51u, 0x5Au, 0x36u, 0xF3u, 0xC9u,
0x5Cu, 0x17u, 0xB1u, 0x7Du, 0xCAu, 0xD5u, 0x68u, 0xEFu,
0x85u, 0xF5u, 0x1Eu, 0xAEu, 0x54u, 0x65u, 0x7Cu, 0x72u,
0xEDu, 0x3Cu, 0xA9u, 0x97u, 0x2Du, 0xD9u, 0x0Du, 0xA5u,
0xFCu, 0x54u, 0x20u, 0x78u, 0x24u, 0xDBu, 0x41u, 0x87u
};
#define MAX_CPUWA_SIZE MCUXCLECC_WEIERECC_DECODEPOINT_WACPU_SIZE
#define MAX_PKCWA_SIZE MCUXCLECC_WEIERECC_DECODEPOINT_WAPKC_SIZE_384
MCUXCLEXAMPLE_FUNCTION(mcuxClEcc_WeierECC_DecodePoint_brainpoolP384r1_example)
{
mcuxClSession_Descriptor_t sessionDesc;
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION(pSession, MAX_CPUWA_SIZE, MAX_PKCWA_SIZE);
uint8_t pDecodedPoint[MCUXCLECC_WEIERECC_BRAINPOOLP384R1_SIZE_PRIMEP * 2u] = {0};
MCUXCLBUFFER_INIT(buffDecodedPoint, NULL, pDecodedPoint, (MCUXCLECC_WEIERECC_BRAINPOOLP384R1_SIZE_PRIMEP * 2u));
pSession,
buffCompressedPoint,
buffDecodedPoint,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_DISCARD_CONST_QUALIFIER()
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_DISCARD_CONST_QUALIFIER())
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(!mcuxClCore_assertEqual(pDecodedPoint, pRefDecodedPoint, MCUXCLECC_WEIERECC_BRAINPOOLP384R1_SIZE_PRIMEP * 2u))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(!mcuxClExample_Session_Clean(pSession))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
return MCUXCLEXAMPLE_STATUS_OK;
}
Definition of function identifiers for the flow protection mechanism.
Top level header of mcuxClEcc component.
Top-level include file for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.
#define MCUXCLBUFFER_INIT(name, info, ptr, size)
Initialize an input/output buffer (mcuxCl_Buffer_t).
Definition mcuxClBuffer.h:67
#define MCUXCLBUFFER_INIT_RO(name, info, ptr, size)
Initialize an input buffer (mcuxCl_InputBuffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:84
mcuxClEcc_Status_t mcuxClEcc_WeierECC_DecodePoint(mcuxClSession_Handle_t pSession, mcuxCl_InputBuffer_t pEncodedPoint, mcuxCl_Buffer_t pDecodedPoint, mcuxClEcc_WeierECC_PointEncType_t pointEncType, mcuxClEcc_Weier_DomainParams_t *pEccWeierDomainParams)
Point decoding function.
struct mcuxClEcc_Weier_DomainParams mcuxClEcc_Weier_DomainParams_t
Type for Weierstrass ECC domain parameters.
Definition mcuxClEcc_Types.h:83
const mcuxClEcc_Weier_DomainParams_t mcuxClEcc_Weier_DomainParams_brainpoolP384r1
brainpoolP384r1 domain parameters
static const mcuxClEcc_WeierECC_PointEncType_t mcuxClEcc_WeierECC_PointEncType_SEC
Point encoding type to be used for Weierstrass curve points as specified in SEC 1: Elliptic Curve Cry...
Definition mcuxClEcc_Types.h:626
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658
#define MCUXCLECC_STATUS_OK
Operation was successful.
Definition mcuxClEcc_Constants.h:46