Example for the mcuxClEcc component.
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_Session_Helper.h>
#define MAX_CPUWA_SIZE MCUXCLECC_WEIERECC_PUBLICKEYVALIDATION_WACPU_SIZE
#define MAX_PKCWA_SIZE MCUXCLECC_WEIERECC_PUBLICKEYVALIDATION_WAPKC_SIZE_256
static const uint8_t pPubKeyData_InvalidPoint[MCUXCLECC_WEIERECC_NIST_P256_SIZE_PUBLICKEY]
__attribute__ ((aligned (4))) = {
0x0Cu, 0xB2u, 0x52u, 0x2Fu, 0x18u, 0xF9u, 0xB5u, 0xA3u,
0xADu, 0x3Au, 0xE0u, 0x99u, 0x75u, 0x5Au, 0x49u, 0xCDu,
0xCEu, 0x4Bu, 0x05u, 0x14u, 0xB5u, 0xC6u, 0x15u, 0x07u,
0xF0u, 0xC6u, 0x39u, 0xE7u, 0x1Au, 0xB4u, 0x4Cu, 0xDEu,
0x68u, 0xF8u, 0xDFu, 0x58u, 0xA9u, 0xC0u, 0xF8u, 0x62u,
0x35u, 0x9Cu, 0xB2u, 0x36u, 0xF9u, 0x29u, 0xABu, 0x9Fu,
0x89u, 0xB1u, 0xA7u, 0xA2u, 0x34u, 0xC1u, 0xE4u, 0x57u,
0x23u, 0xC7u, 0xE9u, 0x41u, 0x25u, 0x80u, 0x46u, 0xBAu,
};
static const uint8_t pPubKeyData_Valid[MCUXCLECC_WEIERECC_NIST_P256_SIZE_PUBLICKEY]
__attribute__ ((aligned (4))) = {
0x0Cu, 0xB2u, 0x52u, 0x2Fu, 0x18u, 0xF9u, 0xB5u, 0xA3u,
0xADu, 0x3Au, 0xE0u, 0x99u, 0x75u, 0x5Au, 0x49u, 0xCDu,
0xCEu, 0x4Bu, 0x05u, 0x14u, 0xB5u, 0xC6u, 0x15u, 0x07u,
0xF0u, 0xC6u, 0x39u, 0xE7u, 0x1Au, 0xB4u, 0x4Cu, 0xDEu,
0x68u, 0xF8u, 0xDFu, 0x58u, 0xA9u, 0xC0u, 0xF8u, 0x62u,
0x35u, 0x9Cu, 0xB2u, 0x36u, 0xF9u, 0x29u, 0xABu, 0x9Fu,
0x89u, 0xB1u, 0xA7u, 0xA2u, 0x34u, 0xC1u, 0xE4u, 0x57u,
0x23u, 0xC7u, 0xE9u, 0x41u, 0x25u, 0x80u, 0x46u, 0xBBu,
};
MCUXCLEXAMPLE_FUNCTION(mcuxClEcc_Weier_KeyValidation_PublicKey_example)
{
mcuxClSession_Descriptor_t sessionDesc;
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION(session, MAX_CPUWA_SIZE, MAX_PKCWA_SIZE);
uint32_t pubKeyDesc[(MCUXCLKEY_DESCRIPTOR_SIZE + (sizeof(uint32_t)) - 1u) / (sizeof(uint32_t))];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
session,
pubKey,
pPubKeyData_InvalidPoint,
MCUXCLECC_WEIERECC_NIST_P256_SIZE_PUBLICKEY));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
session,
pubKey));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
session,
pubKey,
pPubKeyData_Valid,
MCUXCLECC_WEIERECC_NIST_P256_SIZE_PUBLICKEY));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
session,
pubKey));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
return MCUXCLEXAMPLE_STATUS_OK;
}
Definition of function identifiers for the flow protection mechanism.
Top level header of mcuxClEcc component.
Top-level include file for the mcuxClKey component.
Top-level include file for the memory operations.
Top-level include file for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.
static const mcuxClKey_Type_t mcuxClKey_Type_WeierECC_NIST_P256_Pub
Key type pointer for public ECC Weierstrass keys for Weierstrass curve NIST P-256.
Definition mcuxClEcc_KeyTypes.h:453
static mcuxClKey_Validation_t mcuxClKey_Validation_WeierECC_PublicKey
Key validation type for a public key used for ECC on a Weierstrass curve.
Definition mcuxClEcc_KeyTypes.h:1319
#define MCUXCLKEY_STATUS_OK
Key operation successful.
Definition mcuxClKey_Constants.h:40
#define MCUXCLKEY_STATUS_VALIDATION_PASSED
Key validation successful.
Definition mcuxClKey_Constants.h:48
#define MCUXCLKEY_STATUS_VALIDATION_FAILED
Key validation failed.
Definition mcuxClKey_Constants.h:49
mcuxClKey_Status_t mcuxClKey_init(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClKey_Type_t type, const uint8_t *pKeyData, uint32_t keyDataLength)
Initializes a key handle.
mcuxClKey_Status_t mcuxClKey_validate(mcuxClSession_Handle_t session, mcuxClKey_Validation_t validation, mcuxClKey_Handle_t key)
Key validation function.
mcuxClKey_Descriptor_t *const mcuxClKey_Handle_t
Key handle type.
Definition mcuxClKey_Types.h:91
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658
Structure type for Rsa key entries, specifying key entry length and data.
Definition mcuxClRsa_Types.h:104