Example for the mcuxClEcc component.
#include <mcuxClToolchain.h>
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_Session_Helper.h>
#define MAX_CPUWA_SIZE MCUXCLECC_WEIERECC_PRIVATEKEYVALIDATION_WACPU_SIZE
#define MAX_PKCWA_SIZE MCUXCLECC_WEIERECC_PRIVATEKEYVALIDATION_WAPKC_SIZE_256
static const uint8_t pPrivKeyData_Invalid[MCUXCLECC_WEIERECC_SECP192R1_SIZE_PRIVATEKEY]
__attribute__ ((aligned (4))) =
{
0xFFu, 0xFFu, 0xFFu, 0xFFu, 0xFFu, 0xFFu, 0xFFu, 0xFFu,
0xFFu, 0xFFu, 0xFFu, 0xFFu, 0x99u, 0xDEu, 0xF8u, 0x36u,
0x14u, 0x6Bu, 0xC9u, 0xB1u, 0xB4u, 0xD2u, 0x28u, 0x31u
};
static const uint8_t pPrivKeyData_Valid[MCUXCLECC_WEIERECC_SECP192R1_SIZE_PRIVATEKEY]
__attribute__ ((aligned (4))) =
{
0x72u, 0xBBu, 0x52u, 0x76u, 0xD8u, 0xA3u, 0x0Fu, 0x37u,
0x85u, 0x6Eu, 0xB1u, 0x04u, 0x62u, 0xE4u, 0xA2u, 0x56u,
0x22u, 0xB2u, 0x41u, 0x01u, 0xA1u, 0x23u, 0xDFu, 0x24u
};
MCUXCLEXAMPLE_FUNCTION(mcuxClEcc_Weier_KeyValidation_PrivateKey_example)
{
mcuxClSession_Descriptor_t sessionDesc;
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION(session, MAX_CPUWA_SIZE, MAX_PKCWA_SIZE);
uint32_t privKeyDesc[MCUXCLKEY_DESCRIPTOR_SIZE_IN_WORDS];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
session,
privKey,
pPrivKeyData_Invalid,
MCUXCLECC_WEIERECC_SECP192R1_SIZE_PRIVATEKEY));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
session,
privKey));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
session,
privKey,
pPrivKeyData_Valid,
MCUXCLECC_WEIERECC_SECP192R1_SIZE_PRIVATEKEY));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
session,
privKey));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
return MCUXCLEXAMPLE_STATUS_OK;
}
Definition of function identifiers for the flow protection mechanism.
Top level header of mcuxClEcc component.
Top-level include file for the mcuxClKey component.
Top-level include file for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.
static const mcuxClKey_Type_t mcuxClKey_Type_WeierECC_secp192r1_Priv
Key type pointer for private ECC keys for Weierstrass curve secp192r1.
Definition mcuxClEcc_KeyTypes.h:214
static mcuxClKey_Validation_t mcuxClKey_Validation_WeierECC_PrivateKey
Key validation type for a private key used for ECC on a Weierstrass curve.
Definition mcuxClEcc_KeyTypes.h:1334
#define MCUXCLKEY_STATUS_OK
Key operation successful.
Definition mcuxClKey_Constants.h:40
#define MCUXCLKEY_STATUS_VALIDATION_PASSED
Key validation successful.
Definition mcuxClKey_Constants.h:48
#define MCUXCLKEY_STATUS_VALIDATION_FAILED
Key validation failed.
Definition mcuxClKey_Constants.h:49
mcuxClKey_Status_t mcuxClKey_init(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClKey_Type_t type, const uint8_t *pKeyData, uint32_t keyDataLength)
Initializes a key handle.
mcuxClKey_Status_t mcuxClKey_validate(mcuxClSession_Handle_t session, mcuxClKey_Validation_t validation, mcuxClKey_Handle_t key)
Key validation function.
mcuxClKey_Descriptor_t *const mcuxClKey_Handle_t
Key handle type.
Definition mcuxClKey_Types.h:91
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658
Structure type for Rsa key entries, specifying key entry length and data.
Definition mcuxClRsa_Types.h:104