Example for the mcuxClEcc component.
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_Session_Helper.h>
#include <mcuxClExample_RNG_Helper.h>
#define MAX_CPUWA_SIZE MCUXCLCORE_MAX(MCUXCLRANDOM_NCINIT_WACPU_SIZE, \
MCUXCLKEY_AGREEMENT_ECDH_WACPU_SIZE)
#define MAX_PKCWA_SIZE (MCUXCLKEY_AGREEMENT_ECDH_WAPKC_SIZE_256)
static const uint8_t pAlicePrivKeyData[MCUXCLECC_WEIERECC_NIST_P256_SIZE_PRIVATEKEY]
__attribute__ ((aligned (4))) = {
0x5Du, 0x37u, 0x8Du, 0xFDu, 0x5Cu, 0xDDu, 0x7Au, 0x37u,
0xE7u, 0x0Fu, 0x1Au, 0xF7u, 0xFEu, 0x99u, 0xA5u, 0x16u,
0xD4u, 0xE0u, 0xC4u, 0x34u, 0xD8u, 0x49u, 0x85u, 0xFBu,
0x12u, 0x50u, 0x32u, 0x06u, 0x73u, 0x9Au, 0x96u, 0xF4u,
};
static const uint8_t pAlicePubKeyData[MCUXCLECC_WEIERECC_NIST_P256_SIZE_PUBLICKEY]
__attribute__ ((aligned (4))) = {
0x0Cu, 0xB2u, 0x52u, 0x2Fu, 0x18u, 0xF9u, 0xB5u, 0xA3u,
0xADu, 0x3Au, 0xE0u, 0x99u, 0x75u, 0x5Au, 0x49u, 0xCDu,
0xCEu, 0x4Bu, 0x05u, 0x14u, 0xB5u, 0xC6u, 0x15u, 0x07u,
0xF0u, 0xC6u, 0x39u, 0xE7u, 0x1Au, 0xB4u, 0x4Cu, 0xDEu,
0x68u, 0xF8u, 0xDFu, 0x58u, 0xA9u, 0xC0u, 0xF8u, 0x62u,
0x35u, 0x9Cu, 0xB2u, 0x36u, 0xF9u, 0x29u, 0xABu, 0x9Fu,
0x89u, 0xB1u, 0xA7u, 0xA2u, 0x34u, 0xC1u, 0xE4u, 0x57u,
0x23u, 0xC7u, 0xE9u, 0x41u, 0x25u, 0x80u, 0x46u, 0xBBu,
};
static const uint8_t pBobPrivKeyData[MCUXCLECC_WEIERECC_NIST_P256_SIZE_PRIVATEKEY]
__attribute__ ((aligned (4))) = {
0x90u, 0xA1u, 0x2Cu, 0xEDu, 0x78u, 0x9Au, 0x4Fu, 0x82u,
0x95u, 0xBAu, 0x2Fu, 0x79u, 0x3Du, 0x52u, 0x15u, 0xABu,
0xDEu, 0x98u, 0x4Cu, 0x4Bu, 0x08u, 0x87u, 0xBFu, 0x6Fu,
0x75u, 0x1Bu, 0x1Bu, 0x19u, 0xF2u, 0xFDu, 0x76u, 0x03u
};
static const uint8_t pBobPubKeyData[MCUXCLECC_WEIERECC_NIST_P256_SIZE_PUBLICKEY]
__attribute__ ((aligned (4))) = {
0xF4u, 0x7Au, 0x9Au, 0xA6u, 0x2Du, 0x6Bu, 0x5Cu, 0x57u,
0x1Eu, 0xC6u, 0x6Au, 0xDFu, 0x00u, 0x1Eu, 0x2Cu, 0x2Du,
0x21u, 0x72u, 0xDEu, 0x07u, 0x2Bu, 0xA5u, 0xB9u, 0xB4u,
0xB2u, 0xB5u, 0xC3u, 0xEBu, 0xC9u, 0x50u, 0xE0u, 0x21u,
0x12u, 0xF9u, 0xD0u, 0xA3u, 0xA8u, 0x85u, 0x0Bu, 0x9Bu,
0xA6u, 0xE1u, 0x4Bu, 0x3Bu, 0x7Du, 0x54u, 0xD8u, 0x7Bu,
0xF9u, 0x82u, 0xECu, 0x38u, 0x1Bu, 0x81u, 0x5Bu, 0x7Du,
0x9Fu, 0x29u, 0x51u, 0x9Fu, 0x52u, 0x95u, 0x24u, 0xD6u
};
MCUXCLEXAMPLE_FUNCTION(mcuxClEcc_ECDH_KeyAgreement_NIST_P256_example)
{
mcuxClSession_Descriptor_t sessionDesc;
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION(session,
MAX_CPUWA_SIZE,
MAX_PKCWA_SIZE);
uint32_t alicePrivKeyDesc[(MCUXCLKEY_DESCRIPTOR_SIZE + (sizeof(uint32_t)) - 1u) / (sizeof(uint32_t))];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
session,
alicePrivKey,
pAlicePrivKeyData,
MCUXCLECC_WEIERECC_NIST_P256_SIZE_PRIVATEKEY));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
uint32_t alicePubKeyDesc[(MCUXCLKEY_DESCRIPTOR_SIZE + (sizeof(uint32_t)) - 1u) / (sizeof(uint32_t))];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
session,
alicePubKey,
pAlicePubKeyData,
MCUXCLECC_WEIERECC_NIST_P256_SIZE_PUBLICKEY));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
uint32_t bobPrivKeyDesc[(MCUXCLKEY_DESCRIPTOR_SIZE + (sizeof(uint32_t)) - 1u) / (sizeof(uint32_t))];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
session,
bobPrivKey,
pBobPrivKeyData,
MCUXCLECC_WEIERECC_NIST_P256_SIZE_PRIVATEKEY));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
uint32_t bobPubKeyDesc[(MCUXCLKEY_DESCRIPTOR_SIZE + (sizeof(uint32_t)) - 1u) / (sizeof(uint32_t))];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
session,
bobPubKey,
pBobPubKeyData,
MCUXCLECC_WEIERECC_NIST_P256_SIZE_PUBLICKEY));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUXCLEXAMPLE_INITIALIZE_PRNG(session);
uint32_t numberOfInputs = 0u;
uint8_t aliceSharedSecret[MCUXCLECC_WEIERECC_NIST_P256_SIZE_SHAREDSECRET];
uint32_t aliceSharedSecretSize = 0u;
session,
alicePrivKey,
bobPubKey,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_NULL_POINTER_CONSTANT("NULL is used in code")
NULL,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_NULL_POINTER_CONSTANT()
numberOfInputs,
aliceSharedSecret,
&aliceSharedSecretSize));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
uint8_t bobSharedSecret[MCUXCLECC_WEIERECC_NIST_P256_SIZE_SHAREDSECRET];
uint32_t bobSharedSecretSize = 0u;
session,
bobPrivKey,
alicePubKey,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_NULL_POINTER_CONSTANT("NULL is used in code")
NULL,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_NULL_POINTER_CONSTANT()
numberOfInputs,
bobSharedSecret,
&bobSharedSecretSize));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(!mcuxClCore_assertEqual(bobSharedSecret, aliceSharedSecret, MCUXCLECC_WEIERECC_NIST_P256_SIZE_SHAREDSECRET))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
return MCUXCLEXAMPLE_STATUS_OK;
}
Definition of function identifiers for the flow protection mechanism.
Top level header of mcuxClEcc component.
Top-level include file for the mcuxClHash component.
Top-level include file for the mcuxClKey component.
Top level header of mcuxClRandom component.
Top level header of mcuxClRandomModes component.
Top-level include file for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.
static const mcuxClKey_Type_t mcuxClKey_Type_WeierECC_NIST_P256_Pub
Key type pointer for public ECC Weierstrass keys for Weierstrass curve NIST P-256.
Definition mcuxClEcc_KeyTypes.h:453
static const mcuxClKey_Type_t mcuxClKey_Type_WeierECC_NIST_P256_Priv
Key type pointer for private ECC keys for Weierstrass curve NIST P-256.
Definition mcuxClEcc_KeyTypes.h:469
static mcuxClKey_Agreement_t mcuxClKey_Agreement_ECDH
ECDH Key agreement algorithm.
Definition mcuxClEcc_KeyTypes.h:1277
#define MCUXCLKEY_STATUS_OK
Key operation successful.
Definition mcuxClKey_Constants.h:40
mcuxClKey_Status_t mcuxClKey_init(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClKey_Type_t type, const uint8_t *pKeyData, uint32_t keyDataLength)
Initializes a key handle.
mcuxClKey_Status_t mcuxClKey_agreement(mcuxClSession_Handle_t session, mcuxClKey_Agreement_t agreement, mcuxClKey_Handle_t key, mcuxClKey_Handle_t otherKey, mcuxClKey_Agreement_AdditionalInput_t additionalInputs[], uint32_t numberOfInputs, uint8_t *pOut, uint32_t *const pOutLength)
Key agreement function.
mcuxClKey_Descriptor_t *const mcuxClKey_Handle_t
Key handle type.
Definition mcuxClKey_Types.h:91
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658
Structure type for Rsa key entries, specifying key entry length and data.
Definition mcuxClRsa_Types.h:104