Example for the mcuxClEcc component.
#include <mcuxClToolchain.h>
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_Session_Helper.h>
#include <mcuxClExample_RNG_Helper.h>
static const uint8_t digest[] = {
0xC4u, 0x93u, 0xCFu, 0x6Bu, 0xE5u, 0x11u, 0x35u, 0x22u,
0x1Au, 0x3Fu, 0x5Cu, 0x7Bu, 0xCFu, 0xF4u, 0x6Du, 0xC6u,
0x10u, 0x77u, 0x6Eu, 0x2Cu, 0x04u, 0xA3u, 0xB9u, 0x9Du,
0x39u, 0x3Bu, 0x4Bu, 0xEEu, 0xD5u, 0xDDu, 0x88u, 0x86u
};
#define MAX_CPUWA_SIZE MCUXCLCORE_MAX(MCUXCLRANDOM_NCINIT_WACPU_SIZE, \
MCUXCLCORE_MAX(MCUXCLRANDOMMODES_INIT_WACPU_SIZE, \
MCUXCLCORE_MAX(MCUXCLKEY_GENERATEKEYPAIR_WEIERECC_WACPU_SIZE, \
MCUXCLCORE_MAX(MCUXCLSIGNATURE_SIGN_ECDSA_WACPU_SIZE, \
MCUXCLSIGNATURE_VERIFY_ECDSA_WACPU_SIZE))))
#define MAX_PKCWA_SIZE MCUXCLCORE_MAX(MCUXCLKEY_GENERATEKEYPAIR_WEIERECC_WAPKC_SIZE_256, \
MCUXCLCORE_MAX(MCUXCLSIGNATURE_SIGN_ECDSA_WAPKC_SIZE_256, \
MCUXCLSIGNATURE_VERIFY_ECDSA_WAPKC_SIZE_256))
MCUXCLEXAMPLE_FUNCTION(mcuxClEcc_ECDSA_GeneratedKeys_NIST_P256_example)
{
mcuxClSession_Descriptor_t sessionDesc;
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION(session, MAX_CPUWA_SIZE, MAX_PKCWA_SIZE);
uint32_t privKeyDesc[MCUXCLKEY_DESCRIPTOR_SIZE_IN_WORDS];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
ALIGNED uint8_t pPrivKeyData[MCUXCLECC_WEIERECC_NIST_P256_SIZE_PRIVATEKEY];
session,
privKey,
pPrivKeyData,
MCUXCLECC_WEIERECC_NIST_P256_SIZE_PRIVATEKEY)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
uint32_t pubKeyDesc[MCUXCLKEY_DESCRIPTOR_SIZE_IN_WORDS];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
ALIGNED uint8_t pPubKeyData[MCUXCLECC_WEIERECC_NIST_P256_SIZE_PUBLICKEY];
session,
pubKey,
pPubKeyData,
MCUXCLECC_WEIERECC_NIST_P256_SIZE_PUBLICKEY)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_RNG(session, MCUXCLRANDOMMODES_CTR_DRBG_AES256_CONTEXT_SIZE, mcuxClRandomModes_Mode_CtrDrbg_AES256_DRG3);
session,
privKey,
pubKey)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
uint8_t signature[MCUXCLECC_WEIERECC_NIST_P256_SIZE_SIGNATURE];
MCUXCLBUFFER_INIT(buffSignature, NULL, &signature[0],
sizeof(MCUXCLECC_WEIERECC_NIST_P256_SIZE_SIGNATURE));
uint32_t signatureSize = 0u;
session,
privKey,
buffDigest,
sizeof(digest),
buffSignature,
&signatureSize)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(MCUXCLECC_WEIERECC_NIST_P256_SIZE_SIGNATURE != signatureSize)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
session,
buffDigest,
sizeof(digest))
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUXCLBUFFER_INIT_RO(buffSignatureIn, NULL, &signature[0],
sizeof(MCUXCLECC_WEIERECC_NIST_P256_SIZE_SIGNATURE));
session,
pubKey,
buffDigest,
sizeof(digest),
buffSignatureIn,
signatureSize)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
return MCUXCLEXAMPLE_STATUS_OK;
}
Top-level include file for the mcuxClBuffer component.
Definition of function identifiers for the flow protection mechanism.
Top level header of mcuxClEcc component.
Top-level include file for the mcuxClHash component.
Top-level include file for the mcuxClKey component.
Top level header of mcuxClRandom component.
Top level header of mcuxClRandomModes component.
Top-level include file for the mcuxClSession component.
Top-level include file for the mcuxClSignature component.
Provides the API for the CSSL flow protection mechanism.
#define MCUXCLBUFFER_INIT(name, info, ptr, size)
Initialize an input/output buffer (mcuxCl_Buffer_t).
Definition mcuxClBuffer.h:67
#define MCUXCLBUFFER_INIT_RO(name, info, ptr, size)
Initialize an input buffer (mcuxCl_InputBuffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:84
static const mcuxClKey_Type_t mcuxClKey_Type_WeierECC_NIST_P256_Pub
Key type pointer for public ECC Weierstrass keys for Weierstrass curve NIST P-256.
Definition mcuxClEcc_KeyTypes.h:453
static const mcuxClKey_Type_t mcuxClKey_Type_WeierECC_NIST_P256_Priv
Key type pointer for private ECC keys for Weierstrass curve NIST P-256.
Definition mcuxClEcc_KeyTypes.h:469
static mcuxClKey_Generation_t mcuxClKey_Generation_ECDSA
ECDSA Key generation algorithm.
Definition mcuxClEcc_KeyTypes.h:1207
#define MCUXCLKEY_STATUS_OK
Key operation successful.
Definition mcuxClKey_Constants.h:40
mcuxClKey_Status_t mcuxClKey_init(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClKey_Type_t type, const uint8_t *pKeyData, uint32_t keyDataLength)
Initializes a key handle.
mcuxClKey_Status_t mcuxClKey_generate_keypair(mcuxClSession_Handle_t session, mcuxClKey_Generation_t generation, mcuxClKey_Handle_t privKey, mcuxClKey_Handle_t pubKey)
Key-pair generation function.
mcuxClKey_Descriptor_t *const mcuxClKey_Handle_t
Key handle type.
Definition mcuxClKey_Types.h:91
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
mcuxClSignature_Status_t mcuxClSignature_verify(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClSignature_Mode_t mode, mcuxCl_InputBuffer_t pIn, uint32_t inSize, mcuxCl_InputBuffer_t pSignature, uint32_t signatureSize)
One-shot verification function.
mcuxClSignature_Status_t mcuxClSignature_sign(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClSignature_Mode_t mode, mcuxCl_InputBuffer_t pIn, uint32_t inSize, mcuxCl_Buffer_t pSignature, uint32_t *const pSignatureSize)
One-shot signing function.
mcuxClSignature_Status_t mcuxClSignature_verify_recordParam(mcuxClSession_Handle_t pSession, mcuxClSignature_Mode_t mode, mcuxCl_InputBuffer_t pIn, uint32_t inSize)
Record signature verification parameters for protection.
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658
static mcuxClSignature_Mode_t mcuxClSignature_Mode_ECDSA
ECDSA Signature mode.
Definition mcuxClEcc_Types.h:211