MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClEcc_ECDSA_FixedKeys_NIST_P256_example.c

Example for the mcuxClEcc component.

Example for the mcuxClEcc component

/*--------------------------------------------------------------------------*/
/* Copyright 2022-2025 NXP */
/* */
/* NXP Confidential and Proprietary. This software is owned or controlled */
/* by NXP and may only be used strictly in accordance with the applicable */
/* license terms. By expressly accepting such terms or by downloading, */
/* installing, activating and/or otherwise using the software, you are */
/* agreeing that you have read, and that you agree to comply with and are */
/* bound by, such license terms. If you do not agree to be bound by the */
/* applicable license terms, then you may not retain, install, activate or */
/* otherwise use the software. */
/*--------------------------------------------------------------------------*/
#include <mcuxClToolchain.h>
#include <mcuxClSession.h>
#include <mcuxClBuffer.h>
#include <mcuxClKey.h>
#include <mcuxClHash.h>
#include <mcuxClEcc.h>
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_Session_Helper.h>
#include <mcuxClExample_RNG_Helper.h>
#include <mcuxClRandom.h>
#include <mcuxClCore_FunctionIdentifiers.h> // Code flow protection
static const uint8_t digest[] = {
0xC4u, 0x93u, 0xCFu, 0x6Bu, 0xE5u, 0x11u, 0x35u, 0x22u,
0x1Au, 0x3Fu, 0x5Cu, 0x7Bu, 0xCFu, 0xF4u, 0x6Du, 0xC6u,
0x10u, 0x77u, 0x6Eu, 0x2Cu, 0x04u, 0xA3u, 0xB9u, 0x9Du,
0x39u, 0x3Bu, 0x4Bu, 0xEEu, 0xD5u, 0xDDu, 0x88u, 0x86u
};
static const ALIGNED uint8_t pPrivKeyData[MCUXCLECC_WEIERECC_NIST_P256_SIZE_PRIVATEKEY] = {
0x5Du, 0x37u, 0x8Du, 0xFDu, 0x5Cu, 0xDDu, 0x7Au, 0x37u,
0xE7u, 0x0Fu, 0x1Au, 0xF7u, 0xFEu, 0x99u, 0xA5u, 0x16u,
0xD4u, 0xE0u, 0xC4u, 0x34u, 0xD8u, 0x49u, 0x85u, 0xFBu,
0x12u, 0x50u, 0x32u, 0x06u, 0x73u, 0x9Au, 0x96u, 0xF4u
};
static const uint8_t pPubKeyData[MCUXCLECC_WEIERECC_NIST_P256_SIZE_PUBLICKEY] = {
0x0Cu, 0xB2u, 0x52u, 0x2Fu, 0x18u, 0xF9u, 0xB5u, 0xA3u,
0xADu, 0x3Au, 0xE0u, 0x99u, 0x75u, 0x5Au, 0x49u, 0xCDu,
0xCEu, 0x4Bu, 0x05u, 0x14u, 0xB5u, 0xC6u, 0x15u, 0x07u,
0xF0u, 0xC6u, 0x39u, 0xE7u, 0x1Au, 0xB4u, 0x4Cu, 0xDEu,
0x68u, 0xF8u, 0xDFu, 0x58u, 0xA9u, 0xC0u, 0xF8u, 0x62u,
0x35u, 0x9Cu, 0xB2u, 0x36u, 0xF9u, 0x29u, 0xABu, 0x9Fu,
0x89u, 0xB1u, 0xA7u, 0xA2u, 0x34u, 0xC1u, 0xE4u, 0x57u,
0x23u, 0xC7u, 0xE9u, 0x41u, 0x25u, 0x80u, 0x46u, 0xBBu
};
#define MAX_CPUWA_SIZE MCUXCLCORE_MAX(MCUXCLRANDOM_NCINIT_WACPU_SIZE, \
MCUXCLCORE_MAX(MCUXCLRANDOMMODES_INIT_WACPU_SIZE, \
MCUXCLCORE_MAX(MCUXCLSIGNATURE_SIGN_ECDSA_WACPU_SIZE, \
MCUXCLSIGNATURE_VERIFY_ECDSA_WACPU_SIZE)))
#define MAX_PKCWA_SIZE MCUXCLCORE_MAX(MCUXCLSIGNATURE_SIGN_ECDSA_WAPKC_SIZE_256, \
MCUXCLSIGNATURE_VERIFY_ECDSA_WAPKC_SIZE_256)
MCUXCLEXAMPLE_FUNCTION(mcuxClEcc_ECDSA_FixedKeys_NIST_P256_example)
{
/**************************************************************************/
/* Preparation */
/**************************************************************************/
/* Setup one session to be used by all functions called */
mcuxClSession_Descriptor_t sessionDesc;
mcuxClSession_Handle_t session = &sessionDesc;
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION(session, MAX_CPUWA_SIZE, MAX_PKCWA_SIZE);
/* Allocate space for and initialize private key handle for an ECDSA NIST P-256 private key */
uint32_t privKeyDesc[MCUXCLKEY_DESCRIPTOR_SIZE_IN_WORDS];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
mcuxClKey_Handle_t privKey = (mcuxClKey_Handle_t) &privKeyDesc;
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(ki_priv_status, ki_priv_token, mcuxClKey_init(
/* mcuxClSession_Handle_t session */ session,
/* mcuxClKey_Handle_t key */ privKey,
/* mcuxClKey_Type_t type */ mcuxClKey_Type_WeierECC_NIST_P256_Priv,
/* const uint8_t * pKeyData */ pPrivKeyData,
/* uint32_t keyDataLength */ MCUXCLECC_WEIERECC_NIST_P256_SIZE_PRIVATEKEY)
);
if((MCUX_CSSL_FP_FUNCTION_CALLED(mcuxClKey_init) != ki_priv_token) || (MCUXCLKEY_STATUS_OK != ki_priv_status))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* Allocate space for and initialize private key handle for an ECDSA NIST P-256 public key */
uint32_t pubKeyDesc[MCUXCLKEY_DESCRIPTOR_SIZE_IN_WORDS];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
mcuxClKey_Handle_t pubKey = (mcuxClKey_Handle_t) &pubKeyDesc;
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(ki_pub_status, ki_pub_token, mcuxClKey_init(
/* mcuxClSession_Handle_t session */ session,
/* mcuxClKey_Handle_t key */ pubKey,
/* mcuxClKey_Type_t type */ mcuxClKey_Type_WeierECC_NIST_P256_Pub,
/* const uint8_t * pKeyData */ pPubKeyData,
/* uint32_t keyDataLength */ MCUXCLECC_WEIERECC_NIST_P256_SIZE_PUBLICKEY)
);
if((MCUX_CSSL_FP_FUNCTION_CALLED(mcuxClKey_init) != ki_pub_token) || (MCUXCLKEY_STATUS_OK != ki_pub_status))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* Initialize the RNG context and Initialize the PRNG */
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_RNG(session, MCUXCLRANDOMMODES_CTR_DRBG_AES256_CONTEXT_SIZE, mcuxClRandomModes_Mode_CtrDrbg_AES256_DRG3);
/**************************************************************************/
/* ECDSA signature generation on NIST P-256 */
/**************************************************************************/
uint8_t signature[MCUXCLECC_WEIERECC_NIST_P256_SIZE_SIGNATURE];
MCUXCLBUFFER_INIT(buffSignature, NULL, signature, sizeof(MCUXCLECC_WEIERECC_NIST_P256_SIZE_SIGNATURE));
uint32_t signatureSize = 0u;
MCUXCLBUFFER_INIT_RO(buffDigest, NULL, digest, sizeof(digest));
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClKey_Handle_t key: */ privKey,
/* mcuxClSignature_Mode_t mode: */ mcuxClSignature_Mode_ECDSA,
/* mcuxCl_InputBuffer_t pIn: */ buffDigest,
/* uint32_t inSize: */ sizeof(digest),
/* mcuxCl_Buffer_t pSignature: */ buffSignature,
/* uint32_t * const pSignatureSize: */ &signatureSize)
);
if((MCUX_CSSL_FP_FUNCTION_CALLED(mcuxClSignature_sign) != ss_token) || (MCUXCLSIGNATURE_STATUS_OK != ss_status))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(MCUXCLECC_WEIERECC_NIST_P256_SIZE_SIGNATURE != signatureSize)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/**************************************************************************/
/* ECDSA signature verification on NIST P-256 */
/**************************************************************************/
MCUXCLBUFFER_INIT_RO(buffSignatureToVerify, NULL, signature, sizeof(MCUXCLECC_WEIERECC_NIST_P256_SIZE_SIGNATURE));
/* Record critical parameters for additional protection */
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClSignature_Mode_t mode: */ mcuxClSignature_Mode_ECDSA,
/* mcuxCl_InputBuffer_t pIn: */ buffDigest,
/* uint32_t inSize: */ sizeof(digest))
);
if((MCUX_CSSL_FP_FUNCTION_CALLED(mcuxClSignature_verify_recordParam) != rp_token) || (MCUXCLSIGNATURE_STATUS_OK != rp_status))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClKey_Handle_t key: */ pubKey,
/* mcuxClSignature_Mode_t mode: */ mcuxClSignature_Mode_ECDSA,
/* mcuxCl_InputBuffer_t pIn: */ buffDigest,
/* uint32_t inSize: */ sizeof(digest),
/* mcuxCl_InputBuffer_t pSignature: */ buffSignatureToVerify,
/* uint32_t signatureSize: */ signatureSize)
);
if((MCUX_CSSL_FP_FUNCTION_CALLED(mcuxClSignature_verify) != sv_token) || (MCUXCLSIGNATURE_STATUS_OK != sv_status))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* Clean ecc verify session. */
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
return MCUXCLEXAMPLE_STATUS_OK;
}
Top-level include file for the mcuxClBuffer component.
Definition of function identifiers for the flow protection mechanism.
Definition of macros.
Top level header of mcuxClEcc component.
Top-level include file for the mcuxClHash component.
Top-level include file for the mcuxClKey component.
Top level header of mcuxClRandom component.
Top level header of mcuxClRandomModes component.
Top-level include file for the mcuxClSession component.
Top-level include file for the mcuxClSignature component.
Provides the API for the CSSL flow protection mechanism.
#define MCUXCLBUFFER_INIT(name, info, ptr, size)
Initialize an input/output buffer (mcuxCl_Buffer_t).
Definition mcuxClBuffer.h:67
#define MCUXCLBUFFER_INIT_RO(name, info, ptr, size)
Initialize an input buffer (mcuxCl_InputBuffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:84
static const mcuxClKey_Type_t mcuxClKey_Type_WeierECC_NIST_P256_Pub
Key type pointer for public ECC Weierstrass keys for Weierstrass curve NIST P-256.
Definition mcuxClEcc_KeyTypes.h:453
static const mcuxClKey_Type_t mcuxClKey_Type_WeierECC_NIST_P256_Priv
Key type pointer for private ECC keys for Weierstrass curve NIST P-256.
Definition mcuxClEcc_KeyTypes.h:469
#define MCUXCLKEY_STATUS_OK
Key operation successful.
Definition mcuxClKey_Constants.h:40
mcuxClKey_Status_t mcuxClKey_init(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClKey_Type_t type, const uint8_t *pKeyData, uint32_t keyDataLength)
Initializes a key handle.
mcuxClKey_Descriptor_t *const mcuxClKey_Handle_t
Key handle type.
Definition mcuxClKey_Types.h:91
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
mcuxClSignature_Status_t mcuxClSignature_verify(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClSignature_Mode_t mode, mcuxCl_InputBuffer_t pIn, uint32_t inSize, mcuxCl_InputBuffer_t pSignature, uint32_t signatureSize)
One-shot verification function.
mcuxClSignature_Status_t mcuxClSignature_sign(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClSignature_Mode_t mode, mcuxCl_InputBuffer_t pIn, uint32_t inSize, mcuxCl_Buffer_t pSignature, uint32_t *const pSignatureSize)
One-shot signing function.
mcuxClSignature_Status_t mcuxClSignature_verify_recordParam(mcuxClSession_Handle_t pSession, mcuxClSignature_Mode_t mode, mcuxCl_InputBuffer_t pIn, uint32_t inSize)
Record signature verification parameters for protection.
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658
static mcuxClSignature_Mode_t mcuxClSignature_Mode_ECDSA
ECDSA Signature mode.
Definition mcuxClEcc_Types.h:211