Example for the mcuxClEcc component.
#include <mcuxClToolchain.h>
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_Session_Helper.h>
static const uint8_t data[] = {
0xCAu, 0x83u, 0x5Fu, 0x5Bu, 0x0Bu, 0x44u, 0x33u, 0x32u, 0x11u, 0x4Eu, 0xEAu, 0xA5u, 0x9Au, 0xE5u, 0x56u, 0x7Eu, 0x4Fu, 0x86u, 0xAFu, 0x72u, 0xF1u, 0x1Cu, 0xB4u, 0xE6u, 0x71u, 0xD9u, 0x13u, 0xDEu, 0x03u, 0xD4u, 0xC5u, 0xB7u
};
static const uint8_t pubKeyBytes[MCUXCLECC_WEIERECC_NIST_P256_SIZE_PUBLICKEY] = {
0xE8u, 0x19u, 0xC6u, 0x90u, 0x80u, 0xFEu, 0x45u, 0x2Fu,
0x12u, 0x3Du, 0xA0u, 0x2Cu, 0xC7u, 0xB1u, 0x8Du, 0x54u,
0xE1u, 0x83u, 0x95u, 0x82u, 0xF9u, 0xF4u, 0x0Du, 0x90u,
0xBBu, 0x77u, 0xF3u, 0x8Cu, 0x60u, 0x84u, 0x37u, 0xC6u,
0x85u, 0x62u, 0xAAu, 0xA4u, 0x8Du, 0x2Du, 0x61u, 0x1Fu,
0xF1u, 0xEFu, 0x58u, 0x50u, 0x6Bu, 0x08u, 0xC2u, 0x62u,
0x01u, 0x2Bu, 0xC0u, 0xC1u, 0x3Eu, 0xD7u, 0x37u, 0x72u,
0x44u, 0x65u, 0xB3u, 0x2Cu, 0x02u, 0x79u, 0x85u, 0x9Au
};
static const uint8_t signature[MCUXCLECC_WEIERECC_NIST_P256_SIZE_SIGNATURE] = {
0x28u, 0xF7u, 0xA7u, 0x1Au, 0xADu, 0xEAu, 0x35u, 0x2Au,
0x41u, 0x33u, 0xB5u, 0x3Au, 0x79u, 0x1Cu, 0x69u, 0x33u,
0x38u, 0x2Au, 0xE3u, 0x74u, 0xBDu, 0xA7u, 0xB6u, 0x50u,
0x20u, 0xE0u, 0xF6u, 0x8Du, 0x1Bu, 0x1Bu, 0x35u, 0x46u,
0xF8u, 0x61u, 0x71u, 0x93u, 0xA9u, 0x3Au, 0xB6u, 0x22u,
0xD0u, 0x03u, 0xBFu, 0xC0u, 0x77u, 0xB8u, 0x41u, 0xD9u,
0x91u, 0xDFu, 0xFCu, 0xC5u, 0xEFu, 0x34u, 0xE2u, 0x53u,
0xBFu, 0xB5u, 0x9Eu, 0xA7u, 0xC7u, 0xAFu, 0x40u, 0x13u
};
#define MAX_CPUWA_SIZE MCUXCLSIGNATURE_VERIFY_ECDSA_WACPU_SIZE
#define MAX_PKCWA_SIZE MCUXCLSIGNATURE_VERIFY_ECDSA_WAPKC_SIZE_256
MCUXCLEXAMPLE_FUNCTION(mcuxClEcc_ECDSA_VerifyOnly_NIST_P256_example)
{
mcuxClSession_Descriptor_t sessionDesc;
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION(session, MAX_CPUWA_SIZE, MAX_PKCWA_SIZE);
uint32_t pubKeyDesc[MCUXCLKEY_DESCRIPTOR_SIZE_IN_WORDS];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
session,
pubKey,
pubKeyBytes,
MCUXCLECC_WEIERECC_NIST_P256_SIZE_PUBLICKEY)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION")
session,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
buffData,
sizeof(data))
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
session,
pubKey,
buffData,
sizeof(data),
buffSignature,
sizeof(signature))
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
return MCUXCLEXAMPLE_STATUS_OK;
}
Top-level include file for the mcuxClBuffer component.
Definition of function identifiers for the flow protection mechanism.
Top level header of mcuxClEcc component.
Top-level include file for the mcuxClHash component.
Top-level include file for the mcuxClKey component.
Top-level include file for the mcuxClSession component.
Top-level include file for the mcuxClSignature component.
Provides the API for the CSSL flow protection mechanism.
#define MCUXCLBUFFER_INIT_RO(name, info, ptr, size)
Initialize an input buffer (mcuxCl_InputBuffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:84
static const mcuxClKey_Type_t mcuxClKey_Type_WeierECC_NIST_P256_Pub
Key type pointer for public ECC Weierstrass keys for Weierstrass curve NIST P-256.
Definition mcuxClEcc_KeyTypes.h:453
#define MCUXCLKEY_STATUS_OK
Key operation successful.
Definition mcuxClKey_Constants.h:40
mcuxClKey_Status_t mcuxClKey_init(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClKey_Type_t type, const uint8_t *pKeyData, uint32_t keyDataLength)
Initializes a key handle.
mcuxClKey_Descriptor_t *const mcuxClKey_Handle_t
Key handle type.
Definition mcuxClKey_Types.h:91
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
mcuxClSignature_Status_t mcuxClSignature_verify(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClSignature_Mode_t mode, mcuxCl_InputBuffer_t pIn, uint32_t inSize, mcuxCl_InputBuffer_t pSignature, uint32_t signatureSize)
One-shot verification function.
mcuxClSignature_Status_t mcuxClSignature_verify_recordParam(mcuxClSession_Handle_t pSession, mcuxClSignature_Mode_t mode, mcuxCl_InputBuffer_t pIn, uint32_t inSize)
Record signature verification parameters for protection.
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658
static mcuxClSignature_Mode_t mcuxClSignature_Mode_ECDSA
ECDSA Signature mode.
Definition mcuxClEcc_Types.h:211