MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClHashModes_sha224_oneshot_example.c

mcuxClHashModes example application

mcuxClHashModes example application

/*--------------------------------------------------------------------------*/
/* Copyright 2022-2025 NXP */
/* */
/* NXP Confidential and Proprietary. This software is owned or controlled */
/* by NXP and may only be used strictly in accordance with the applicable */
/* license terms. By expressly accepting such terms or by downloading, */
/* installing, activating and/or otherwise using the software, you are */
/* agreeing that you have read, and that you agree to comply with and are */
/* bound by, such license terms. If you do not agree to be bound by the */
/* applicable license terms, then you may not retain, install, activate or */
/* otherwise use the software. */
/*--------------------------------------------------------------------------*/
#include <mcuxClToolchain.h>
#include <mcuxClSession.h> // Interface to the entire mcuxClSession component
#include <mcuxClHash.h> // Interface to the entire mcuxClHash component
#include <mcuxClCore_FunctionIdentifiers.h> // Code flow protection
#include <mcuxClToolchain.h> // memory segment definitions
#include <mcuxClExample_Session_Helper.h>
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_RNG_Helper.h>
static const ALIGNED uint8_t data[3] = {
0x61u, 0x62u, 0x63u
};
static const ALIGNED uint8_t hashExpected[28] = {
0x23u, 0x09u, 0x7Du, 0x22u, 0x34u, 0x05u, 0xD8u, 0x22u,
0x86u, 0x42u, 0xA4u, 0x77u, 0xBDu, 0xA2u, 0x55u, 0xB3u,
0x2Au, 0xADu, 0xBCu, 0xE4u, 0xBDu, 0xA0u, 0xB3u, 0xF7u,
0xE3u, 0x6Cu, 0x9Du, 0xA7u
};
MCUXCLEXAMPLE_FUNCTION(mcuxClHashModes_sha224_oneshot_example)
{
/**************************************************************************/
/* Preparation */
/**************************************************************************/
/* Initialize session */
mcuxClSession_Descriptor_t sessionDesc;
mcuxClSession_Handle_t session = &sessionDesc;
/* Allocate and initialize session */
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION(session, MCUXCLEXAMPLE_MAX_WA(MCUXCLHASH_MAX_CPU_WA_BUFFER_SIZE, MCUXCLRANDOM_NCINIT_WACPU_SIZE), 0u);
/* Initialize the PRNG */
MCUXCLEXAMPLE_INITIALIZE_PRNG(session);
/**************************************************************************/
/* Hash computation */
/**************************************************************************/
ALIGNED uint8_t hash[MCUXCLHASH_OUTPUT_SIZE_SHA_224];
MCUXCLBUFFER_INIT_RW(hashBuf, session, hash, sizeof(hash));
MCUXCLBUFFER_INIT_RO(dataBuf, session, data, sizeof(data));
uint32_t hashOutputSize = 0u;
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClHash_Algo_t algorithm: */ mcuxClHash_Algorithm_Sha224,
/* mcuxCl_InputBuffer_t pIn: */ dataBuf,
/* uint32_t inSize: */ sizeof(data),
/* mcuxCl_Buffer_t pOut */ hashBuf,
/* uint32_t *const pOutSize, */ &hashOutputSize
));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(sizeof(hash) != hashOutputSize)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/**************************************************************************/
/* Verification */
/**************************************************************************/
for(size_t i = 0U; i < sizeof(hash); i++)
{
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by MCUXCLBUFFER_INIT_RW")
if(hashExpected[i] != hash[i]) // Expect that the resulting hash matches our expected output
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
}
/**************************************************************************/
/* Session clean-up */
/**************************************************************************/
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
return MCUXCLEXAMPLE_STATUS_OK;
}
Definition of function identifiers for the flow protection mechanism.
Top-level include file for the mcuxClHash component.
Top-level include file for the mcuxClHashModes component.
Top-level include file for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.
#define MCUXCLHASH_MAX_CPU_WA_BUFFER_SIZE
Defines the max workarea size required for this component.
Definition mcuxClHash_MemoryConsumption.h:27
#define MCUXCLBUFFER_INIT_RW(name, info, ptr, size)
Initialize an input/output buffer (mcuxCl_Buffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:101
#define MCUXCLBUFFER_INIT_RO(name, info, ptr, size)
Initialize an input buffer (mcuxCl_InputBuffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:84
#define MCUXCLHASH_STATUS_OK
Hash operation successful.
Definition mcuxClHash_Constants.h:35
mcuxClHash_Status_t mcuxClHash_compute(mcuxClSession_Handle_t session, mcuxClHash_Algo_t algorithm, mcuxCl_InputBuffer_t pIn, uint32_t inSize, mcuxCl_Buffer_t pOut, uint32_t *const pOutSize)
One-shot Hash computation function.
static mcuxClHash_Algo_t mcuxClHash_Algorithm_Sha224
Sha-224 algorithm descriptor Sha-224 hash calculation using the Hash functionality SGI.
Definition mcuxClHashModes_Algorithms.h:61
#define MCUXCLHASH_OUTPUT_SIZE_SHA_224
SHA-224 output size: 224 bit (28 bytes).
Definition mcuxClHashModes_Constants.h:37
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658