#include <mcuxClToolchain.h>
#include <mcuxClToolchain.h>
#include <mcuxClExample_Session_Helper.h>
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_RNG_Helper.h>
static const ALIGNED uint8_t data[3] = {
0x61u, 0x62u, 0x63u
};
static const ALIGNED uint8_t hashExpected[32] = {
0xbau, 0x78u, 0x16u, 0xbfu, 0x8fu, 0x01u, 0xcfu, 0xeau,
0x41u, 0x41u, 0x40u, 0xdeu, 0x5du, 0xaeu, 0x22u, 0x23u,
0xb0u, 0x03u, 0x61u, 0xa3u, 0x96u, 0x17u, 0x7au, 0x9cu,
0xb4u, 0x10u, 0xffu, 0x61u, 0xf2u, 0x00u, 0x15u, 0xadu
};
MCUXCLEXAMPLE_FUNCTION(mcuxClHashModes_sha256_oneshot_example)
{
mcuxClSession_Descriptor_t sessionDesc;
MCUXCLEXAMPLE_INITIALIZE_PRNG(session);
uint32_t hashOutputSize = 0u;
session,
dataBuf,
sizeof(data),
hashBuf,
&hashOutputSize
));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(sizeof(hash) != hashOutputSize)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
for(size_t i = 0U; i < sizeof(hash); i++)
{
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by MCUXCLBUFFER_INIT_RW")
if(hashExpected[i] != hash[i])
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
}
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
return MCUXCLEXAMPLE_STATUS_OK;
}
Definition of function identifiers for the flow protection mechanism.
Top-level include file for the mcuxClHash component.
Top-level include file for the mcuxClHashModes component.
Top-level include file for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.
#define MCUXCLHASH_MAX_CPU_WA_BUFFER_SIZE
Defines the max workarea size required for this component.
Definition mcuxClHash_MemoryConsumption.h:27
#define MCUXCLBUFFER_INIT_RW(name, info, ptr, size)
Initialize an input/output buffer (mcuxCl_Buffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:101
#define MCUXCLBUFFER_INIT_RO(name, info, ptr, size)
Initialize an input buffer (mcuxCl_InputBuffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:84
#define MCUXCLHASH_STATUS_OK
Hash operation successful.
Definition mcuxClHash_Constants.h:35
mcuxClHash_Status_t mcuxClHash_compute(mcuxClSession_Handle_t session, mcuxClHash_Algo_t algorithm, mcuxCl_InputBuffer_t pIn, uint32_t inSize, mcuxCl_Buffer_t pOut, uint32_t *const pOutSize)
One-shot Hash computation function.
static mcuxClHash_Algo_t mcuxClHash_Algorithm_Sha256
Sha-256 algorithm descriptor Sha-256 hash calculation using the Hash functionality SGI.
Definition mcuxClHashModes_Algorithms.h:96
#define MCUXCLHASH_OUTPUT_SIZE_SHA_256
SHA-256 output size: 256 bit (32 bytes).
Definition mcuxClHashModes_Constants.h:38
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658