#include <mcuxClToolchain.h>
#include <mcuxClExample_Session_Helper.h>
#include <mcuxClExample_OS.h>
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_RNG_Helper.h>
#include <platform_specific_headers.h>
0x3cu, 0x59u, 0x3au, 0xa5u, 0x39u, 0xfdu, 0xcdu, 0xaeu,
0x51u, 0x6cu, 0xdfu, 0x2fu, 0x15u, 0x00u, 0x0fu, 0x66u,
0x34u, 0x18u, 0x5cu, 0x88u, 0xf5u, 0x05u, 0xb3u, 0x97u,
0x75u, 0xfbu, 0x9au, 0xb1u, 0x37u, 0xa1u, 0x0au, 0xa2u
};
#define MCUXCLHASH_STATUS_CALLBACK_NOT_EXECUTED ((uint32_t) 0xDEADBEEFu)
static volatile uint32_t sha2APInonBlockingStatus_callback = MCUXCLHASH_STATUS_CALLBACK_NOT_EXECUTED;
#define MCUXCLHASH_FLAG_DMA_INTERRUPT_NOT_TRIGGERED ((uint32_t) 0xDEADBEEFu)
static volatile uint32_t flag_interruptNumber = MCUXCLHASH_FLAG_DMA_INTERRUPT_NOT_TRIGGERED;
static void user_callback(uint32_t status, void * data)
{
(void)data;
sha2APInonBlockingStatus_callback = status;
}
static void handleDmaInterrupt_channel0(void)
{
MCUX_CSSL_ANALYSIS_START_PATTERN_SFR_ACCESS()
DMA0->CH[0].CH_INT = 1U;
uint32_t chCsr = DMA0->CH[0].CH_CSR;
chCsr &= ~((uint32_t)DMA_CH_CSR_DONE_MASK);
chCsr &= ~((uint32_t)DMA_CH_CSR_EEI_MASK);
DMA0->CH[0].CH_CSR = chCsr;
MCUX_CSSL_ANALYSIS_STOP_PATTERN_SFR_ACCESS()
flag_interruptNumber = GET_DMA_CHX_IRQ_NUMBER(0U);
}
static void interruptInit(void)
{
mcuxClExample_OS_Interrupt_Callback_Install(handleDmaInterrupt_channel0, GET_DMA_CHX_IRQ_NUMBER(0U));
mcuxClExample_OS_Interrupt_Enable(GET_DMA_CHX_IRQ_NUMBER(0U));
}
static void interruptUninit(void)
{
mcuxClExample_OS_Interrupt_Disable(GET_DMA_CHX_IRQ_NUMBER(0U));
}
MCUXCLEXAMPLE_FUNCTION(mcuxClHashModes_sha256_oneshot_dma_nonBlocking_example)
{
uint8_t longData[] = {
0x45u, 0x11u, 0x01u, 0x25u, 0x0eu, 0xc6u, 0xf2u, 0x66u,
0x52u, 0x24u, 0x9du, 0x59u, 0xdcu, 0x97u, 0x4bu, 0x73u,
0x61u, 0xd5u, 0x71u, 0xa8u, 0x10u, 0x1cu, 0xdfu, 0xd3u,
0x6au, 0xbau, 0x3bu, 0x58u, 0x54u, 0xd3u, 0xaeu, 0x08u,
0x6bu, 0x5fu, 0xddu, 0x45u, 0x97u, 0x72u, 0x1bu, 0x66u,
0xe3u, 0xc0u, 0xdcu, 0x5du, 0x8cu, 0x60u, 0x6du, 0x96u,
0x57u, 0xd0u, 0xe3u, 0x23u, 0x28u, 0x3au, 0x52u, 0x17u,
0xd1u, 0xf5u, 0x3fu, 0x2fu, 0x28u, 0x4fu, 0x57u, 0xb8u,
0x5cu, 0x8au, 0x61u, 0xacu, 0x89u, 0x24u, 0x71u, 0x1fu,
0x89u, 0x5cu, 0x5eu, 0xd9u, 0x0eu, 0xf1u, 0x77u, 0x45u,
0xedu, 0x2du, 0x72u, 0x8au, 0xbdu, 0x22u, 0xa5u, 0xf7u,
0xa1u, 0x34u, 0x79u, 0xa4u, 0x62u, 0xd7u, 0x1bu, 0x56u,
0xc1u, 0x9au, 0x74u, 0xa4u, 0x0bu, 0x65u, 0x5cu, 0x58u,
0xedu, 0xfeu, 0x0au, 0x18u, 0x8au, 0xd2u, 0xcfu, 0x46u,
0xcbu, 0xf3u, 0x05u, 0x24u, 0xf6u, 0x5du, 0x42u, 0x3cu,
0x83u, 0x7du, 0xd1u, 0xffu, 0x2bu, 0xf4u, 0x62u, 0xacu,
0x41u, 0x98u, 0x00u, 0x73u, 0x45u, 0xbbu, 0x44u, 0xdbu,
0xb7u, 0xb1u, 0xc8u, 0x61u, 0x29u, 0x8cu, 0xdfu, 0x61u,
0x98u, 0x2au, 0x83u, 0x3au, 0xfcu, 0x72u, 0x8fu, 0xaeu,
0x1eu, 0xdau, 0x2fu, 0x87u, 0xaau, 0x2cu, 0x94u, 0x80u,
0x85u, 0x8bu, 0xecu
};
interruptInit();
sha2APInonBlockingStatus_callback = MCUXCLHASH_STATUS_CALLBACK_NOT_EXECUTED;
mcuxClSession_Descriptor_t sessionDesc;
MCUXCLEXAMPLE_INITIALIZE_PRNG(session);
};
session,
dmaChannels,
user_callback,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_NULL_POINTER_CONSTANT("NULL is used in code")
NULL)
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_NULL_POINTER_CONSTANT()
);
if(!mcuxClExample_Session_InitAndSetResourceCtx(session, resourceCtxHandle))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
uint32_t hashOutputSize = 0u;
session,
longDataBuf,
sizeof(longData),
hashBuf,
&hashOutputSize
));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
{
while(MCUXCLHASH_FLAG_DMA_INTERRUPT_NOT_TRIGGERED == flag_interruptNumber) {};
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
flag_interruptNumber = MCUXCLHASH_FLAG_DMA_INTERRUPT_NOT_TRIGGERED;
sha2APInonBlockingStatus_callback = MCUXCLHASH_STATUS_CALLBACK_NOT_EXECUTED;
}
else
{
}
if(sizeof(hash) != hashOutputSize)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
for(size_t i = 0U; i < sizeof(hash); i++)
{
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by MCUXCLBUFFER_INIT_DMA_RW")
if(longHashExpected[i] != hash[i])
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
}
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
interruptUninit();
return MCUXCLEXAMPLE_STATUS_OK;
}
Definition of function identifiers for the flow protection mechanism.
Top-level include file for the mcuxClHash component.
Top-level include file for the mcuxClHashModes component.
Top-level include file for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.
#define MCUXCLRESOURCE_CONTEXT_SIZE
Size (in bytes) of mcuxClResource context.
Definition mcuxClResource_MemoryConsumption.h:24
#define MCUXCLBUFFER_INIT_DMA_RO(name, info, ptr, size)
Initialize an input buffer (mcuxCl_InputBuffer_t) with DMA handling.
Definition mcuxClBuffer.h:120
#define MCUXCLBUFFER_INIT_DMA_RW(name, info, ptr, size)
Initialize an input/output buffer (mcuxCl_Buffer_t) with DMA handling.
Definition mcuxClBuffer.h:139
#define MCUXCLHASH_STATUS_JOB_COMPLETED
Job started in coprocessor has completed successfully.
Definition mcuxClHash_Constants.h:46
#define MCUXCLHASH_STATUS_JOB_STARTED
There is ongoing job in coprocessor which will trigger user callback on exit.
Definition mcuxClHash_Constants.h:45
#define MCUXCLHASH_STATUS_OK
Hash operation successful.
Definition mcuxClHash_Constants.h:35
mcuxClHash_Status_t mcuxClHash_compute(mcuxClSession_Handle_t session, mcuxClHash_Algo_t algorithm, mcuxCl_InputBuffer_t pIn, uint32_t inSize, mcuxCl_Buffer_t pOut, uint32_t *const pOutSize)
One-shot Hash computation function.
static mcuxClHash_Algo_t mcuxClHash_Algorithm_Sha256_Dma_NonBlocking
Sha-256 algorithm descriptor Sha-256 hash calculation using the Hash non-blocking functionality SGI.
Definition mcuxClHashModes_Algorithms.h:114
#define MCUXCLHASH_OUTPUT_SIZE_SHA_256
SHA-256 output size: 256 bit (32 bytes).
Definition mcuxClHashModes_Constants.h:38
mcuxClResource_Status_t mcuxClResource_handle_interrupt(const mcuxClResource_Context_t *pResourceCtx, mcuxClResource_Interrupt_t interrupt)
Resource interrupt handler.
struct mcuxClResource_Context mcuxClResource_Context_t
Resource context type.
Definition mcuxClResource_Types.h:47
#define MCUXCLRESOURCE_STATUS_OK
Resource operation successful.
Definition mcuxClResource_Types.h:82
mcuxClSession_Status_t mcuxClSession_configure_job(mcuxClSession_Handle_t session, mcuxClSession_Channels_t dmaChannels, mcuxClSession_Callback_t pUserCallback, void *pUserData)
Configure the parameters for non-blocking operations (jobs) in this session.
#define MCUXCLSESSION_STATUS_OK
Session operation successful.
Definition mcuxClSession_Types.h:39
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
uint16_t mcuxClSession_Channel_t
Session channel type.
Definition mcuxClSession_Types.h:105
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658
#define MCUXCLHASH_COMPUTE_NONBLOCKING_CPU_WA_BUFFER_SIZE_SHA2_256
Defines the workarea size required for mcuxClHash_compute on SHA2-256.
Definition mcuxClHashModes_MemoryConsumption.h:40
Session channels type.
Definition mcuxClSession_Types.h:113