MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClHashModes_sha256_longMsgOneshot_example.c

mcuxClHashModes example application

mcuxClHashModes example application

/*--------------------------------------------------------------------------*/
/* Copyright 2022-2025 NXP */
/* */
/* NXP Confidential and Proprietary. This software is owned or controlled */
/* by NXP and may only be used strictly in accordance with the applicable */
/* license terms. By expressly accepting such terms or by downloading, */
/* installing, activating and/or otherwise using the software, you are */
/* agreeing that you have read, and that you agree to comply with and are */
/* bound by, such license terms. If you do not agree to be bound by the */
/* applicable license terms, then you may not retain, install, activate or */
/* otherwise use the software. */
/*--------------------------------------------------------------------------*/
#include <mcuxClToolchain.h>
#include <mcuxClSession.h> // Interface to the entire mcuxClSession component
#include <mcuxClHash.h> // Interface to the entire mcuxClHash component
#include <mcuxClCore_FunctionIdentifiers.h> // Code flow protection
#include <mcuxClToolchain.h> // memory segment definitions
#include <mcuxClExample_Session_Helper.h>
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_RNG_Helper.h>
/* Test vector from CAVS 11.0 "SHA-256 LongMsg" */
static const ALIGNED uint8_t data[] = {
0x45u, 0x11u, 0x01u, 0x25u, 0x0eu, 0xc6u, 0xf2u, 0x66u,
0x52u, 0x24u, 0x9du, 0x59u, 0xdcu, 0x97u, 0x4bu, 0x73u,
0x61u, 0xd5u, 0x71u, 0xa8u, 0x10u, 0x1cu, 0xdfu, 0xd3u,
0x6au, 0xbau, 0x3bu, 0x58u, 0x54u, 0xd3u, 0xaeu, 0x08u,
0x6bu, 0x5fu, 0xddu, 0x45u, 0x97u, 0x72u, 0x1bu, 0x66u,
0xe3u, 0xc0u, 0xdcu, 0x5du, 0x8cu, 0x60u, 0x6du, 0x96u,
0x57u, 0xd0u, 0xe3u, 0x23u, 0x28u, 0x3au, 0x52u, 0x17u,
0xd1u, 0xf5u, 0x3fu, 0x2fu, 0x28u, 0x4fu, 0x57u, 0xb8u,
0x5cu, 0x8au, 0x61u, 0xacu, 0x89u, 0x24u, 0x71u, 0x1fu,
0x89u, 0x5cu, 0x5eu, 0xd9u, 0x0eu, 0xf1u, 0x77u, 0x45u,
0xedu, 0x2du, 0x72u, 0x8au, 0xbdu, 0x22u, 0xa5u, 0xf7u,
0xa1u, 0x34u, 0x79u, 0xa4u, 0x62u, 0xd7u, 0x1bu, 0x56u,
0xc1u, 0x9au, 0x74u, 0xa4u, 0x0bu, 0x65u, 0x5cu, 0x58u,
0xedu, 0xfeu, 0x0au, 0x18u, 0x8au, 0xd2u, 0xcfu, 0x46u,
0xcbu, 0xf3u, 0x05u, 0x24u, 0xf6u, 0x5du, 0x42u, 0x3cu,
0x83u, 0x7du, 0xd1u, 0xffu, 0x2bu, 0xf4u, 0x62u, 0xacu,
0x41u, 0x98u, 0x00u, 0x73u, 0x45u, 0xbbu, 0x44u, 0xdbu,
0xb7u, 0xb1u, 0xc8u, 0x61u, 0x29u, 0x8cu, 0xdfu, 0x61u,
0x98u, 0x2au, 0x83u, 0x3au, 0xfcu, 0x72u, 0x8fu, 0xaeu,
0x1eu, 0xdau, 0x2fu, 0x87u, 0xaau, 0x2cu, 0x94u, 0x80u,
0x85u, 0x8bu, 0xecu
};
static const ALIGNED uint8_t hashExpected[MCUXCLHASH_OUTPUT_SIZE_SHA_256] = {
0x3cu, 0x59u, 0x3au, 0xa5u, 0x39u, 0xfdu, 0xcdu, 0xaeu,
0x51u, 0x6cu, 0xdfu, 0x2fu, 0x15u, 0x00u, 0x0fu, 0x66u,
0x34u, 0x18u, 0x5cu, 0x88u, 0xf5u, 0x05u, 0xb3u, 0x97u,
0x75u, 0xfbu, 0x9au, 0xb1u, 0x37u, 0xa1u, 0x0au, 0xa2u
};
MCUXCLEXAMPLE_FUNCTION(mcuxClHashModes_sha256_longMsgOneshot_example)
{
/**************************************************************************/
/* Preparation */
/**************************************************************************/
/* Initialize session */
mcuxClSession_Descriptor_t sessionDesc;
mcuxClSession_Handle_t session = &sessionDesc;
/* Allocate and initialize session */
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION(session, MCUXCLEXAMPLE_MAX_WA(MCUXCLHASH_MAX_CPU_WA_BUFFER_SIZE, MCUXCLRANDOM_NCINIT_WACPU_SIZE), 0u);
/* Initialize the PRNG */
MCUXCLEXAMPLE_INITIALIZE_PRNG(session);
/**************************************************************************/
/* Hash computation */
/**************************************************************************/
ALIGNED uint8_t hash[MCUXCLHASH_OUTPUT_SIZE_SHA_256];
MCUXCLBUFFER_INIT_RW(hashBuf, session, hash, sizeof(hash));
MCUXCLBUFFER_INIT_RO(dataBuf, session, data, sizeof(data));
uint32_t hashOutputSize = 0u;
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClHash_Algo_t algorithm: */ mcuxClHash_Algorithm_Sha256,
/* mcuxCl_InputBuffer_t pIn: */ dataBuf,
/* uint32_t inSize: */ sizeof(data),
/* mcuxCl_Buffer_t pOut */ hashBuf,
/* uint32_t *const pOutSize, */ &hashOutputSize
));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(sizeof(hash) != hashOutputSize)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/**************************************************************************/
/* Verification */
/**************************************************************************/
for(size_t i = 0U; i < sizeof(hash); i++)
{
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by MCUXCLBUFFER_INIT_RW")
if(hashExpected[i] != hash[i]) // Expect that the resulting hash matches our expected output
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
}
/**************************************************************************/
/* Session clean-up */
/**************************************************************************/
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
return MCUXCLEXAMPLE_STATUS_OK;
}
Definition of function identifiers for the flow protection mechanism.
Top-level include file for the mcuxClHash component.
Top-level include file for the mcuxClHashModes component.
Top-level include file for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.
#define MCUXCLHASH_MAX_CPU_WA_BUFFER_SIZE
Defines the max workarea size required for this component.
Definition mcuxClHash_MemoryConsumption.h:27
#define MCUXCLBUFFER_INIT_RW(name, info, ptr, size)
Initialize an input/output buffer (mcuxCl_Buffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:101
#define MCUXCLBUFFER_INIT_RO(name, info, ptr, size)
Initialize an input buffer (mcuxCl_InputBuffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:84
#define MCUXCLHASH_STATUS_OK
Hash operation successful.
Definition mcuxClHash_Constants.h:35
mcuxClHash_Status_t mcuxClHash_compute(mcuxClSession_Handle_t session, mcuxClHash_Algo_t algorithm, mcuxCl_InputBuffer_t pIn, uint32_t inSize, mcuxCl_Buffer_t pOut, uint32_t *const pOutSize)
One-shot Hash computation function.
static mcuxClHash_Algo_t mcuxClHash_Algorithm_Sha256
Sha-256 algorithm descriptor Sha-256 hash calculation using the Hash functionality SGI.
Definition mcuxClHashModes_Algorithms.h:96
#define MCUXCLHASH_OUTPUT_SIZE_SHA_256
SHA-256 output size: 256 bit (32 bytes).
Definition mcuxClHashModes_Constants.h:38
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658