MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClHashModes_sha256_streaming_dma_nonBlocking_example.c

mcuxClHashModes example application

mcuxClHashModes example application

/*--------------------------------------------------------------------------*/
/* Copyright 2023-2025 NXP */
/* */
/* NXP Confidential and Proprietary. This software is owned or controlled */
/* by NXP and may only be used strictly in accordance with the applicable */
/* license terms. By expressly accepting such terms or by downloading, */
/* installing, activating and/or otherwise using the software, you are */
/* agreeing that you have read, and that you agree to comply with and are */
/* bound by, such license terms. If you do not agree to be bound by the */
/* applicable license terms, then you may not retain, install, activate or */
/* otherwise use the software. */
/*--------------------------------------------------------------------------*/
#include <mcuxClSession.h> // Interface to the entire mcuxClSession component
#include <mcuxClHash.h> // Interface to the entire mcuxClHash component
#include <mcuxClCore_FunctionIdentifiers.h> // Code flow protection
#include <mcuxClToolchain.h> // memory segment definitions
#include <mcuxClExample_Session_Helper.h>
#include <mcuxClExample_OS.h>
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_RNG_Helper.h>
#include <platform_specific_headers.h> // needed for DMA interrupts
static const uint8_t longHashExpected[MCUXCLHASH_OUTPUT_SIZE_SHA_256] = {
0x3cu, 0x59u, 0x3au, 0xa5u, 0x39u, 0xfdu, 0xcdu, 0xaeu,
0x51u, 0x6cu, 0xdfu, 0x2fu, 0x15u, 0x00u, 0x0fu, 0x66u,
0x34u, 0x18u, 0x5cu, 0x88u, 0xf5u, 0x05u, 0xb3u, 0x97u,
0x75u, 0xfbu, 0x9au, 0xb1u, 0x37u, 0xa1u, 0x0au, 0xa2u
};
/************************************************************************************/
/* Helper code to synchronize example flow with nonBlocking background computation */
/************************************************************************************/
#define MCUXCLHASH_STATUS_CALLBACK_NOT_EXECUTED ((uint32_t) 0xDEADBEEFu)
/* This variable is used to keep track of callbacks triggered by the non-blocking API. */
static volatile uint32_t sha2MultipartnonBlockingStatus_callback = MCUXCLHASH_STATUS_CALLBACK_NOT_EXECUTED;
#define MCUXCLHASH_FLAG_DMA_INTERRUPT_NOT_TRIGGERED ((uint32_t) 0xDEADBEEFu)
/* This variable is a flag to notify the caller that an interrupt happened.
It will contain the IRQ number associated with the DMA channel ID of the respective channel that had an interrupt. */
static volatile uint32_t flag_interruptNumber = MCUXCLHASH_FLAG_DMA_INTERRUPT_NOT_TRIGGERED;
/* This function is called after the nonBlocking operation has finished */
static void user_callback(uint32_t status, void * data)
{
(void)data;
sha2MultipartnonBlockingStatus_callback = status;
}
/**************************************************************************/
/* Interrupt configuration code */
/**************************************************************************/
// TODO-CLNS-16969: fix global resourceCtx
/* Global resource context to handle status and session for the available hw resources
As it is global it should be only allocated once */
static uint32_t resourceContext[MCUXCLRESOURCE_CONTEXT_SIZE/sizeof(uint32_t)];
static mcuxClResource_Context_t * resourceCtxHandle = (mcuxClResource_Context_t *) &resourceContext;
/* This is the Interrupt handler for DMA done and error interrupts on the input channel.
This function only sets the interrupt number as a global flag, the actual handler
mcuxClResource_handle_interrupt needs to be called afterwards to wrap-up the CLib operation. */
static void handleDmaInterrupt_channel0(void)
{
MCUX_CSSL_ANALYSIS_START_PATTERN_SFR_ACCESS()
/* Clear DMA interrupt request status, W1C. Needed for DONE interrupts. */
DMA0->CH[0].CH_INT = 1U;
/* Clear the DMA error interrupt request status, W1C. Needed for ERROR interrupts. */
uint32_t chCsr = DMA0->CH[0].CH_CSR;
/* 1. Unset the DONE bit, to not accidentally perform a W1C. CLib needs this bit for internal checks. */
chCsr &= ~((uint32_t)DMA_CH_CSR_DONE_MASK);
/* 2. Clear the EEI bit. */
chCsr &= ~((uint32_t)DMA_CH_CSR_EEI_MASK);
/* 3. Write to CH_CSR */
DMA0->CH[0].CH_CSR = chCsr;
MCUX_CSSL_ANALYSIS_STOP_PATTERN_SFR_ACCESS()
flag_interruptNumber = GET_DMA_CHX_IRQ_NUMBER(0U);
}
/* Initialize (install, enable) the interrupts */
static void interruptInit(void)
{
/* Enable interrupts for the input channel */
mcuxClExample_OS_Interrupt_Callback_Install(handleDmaInterrupt_channel0, GET_DMA_CHX_IRQ_NUMBER(0U));
/* Enable the interrupts in the controller */
mcuxClExample_OS_Interrupt_Enable(GET_DMA_CHX_IRQ_NUMBER(0U));
}
/* Uninitialize (disable) the interrupts */
static void interruptUninit(void)
{
/* Disable the interrupts in the controller */
mcuxClExample_OS_Interrupt_Disable(GET_DMA_CHX_IRQ_NUMBER(0U));
}
MCUXCLEXAMPLE_FUNCTION(mcuxClHashModes_sha256_streaming_dma_nonBlocking_example)
{
/**************************************************************************/
/* Preparation */
/**************************************************************************/
/* Test vector from CAVS 11.0 "SHA-256 LongMsg" */
uint8_t data1[] = {
0x45u, 0x11u, 0x01u, 0x25u, 0x0eu, 0xc6u, 0xf2u, 0x66u,
0x52u, 0x24u, 0x9du, 0x59u, 0xdcu, 0x97u, 0x4bu, 0x73u,
0x61u, 0xd5u, 0x71u, 0xa8u, 0x10u, 0x1cu, 0xdfu, 0xd3u,
0x6au, 0xbau, 0x3bu, 0x58u, 0x54u, 0xd3u, 0xaeu, 0x08u,
0x6bu, 0x5fu, 0xddu, 0x45u, 0x97u, 0x72u, 0x1bu, 0x66u,
0xe3u, 0xc0u, 0xdcu, 0x5du, 0x8cu, 0x60u, 0x6du, 0x96u,
0x57u, 0xd0u, 0xe3u, 0x23u, 0x28u, 0x3au, 0x52u, 0x17u,
0xd1u, 0xf5u, 0x3fu, 0x2fu, 0x28u, 0x4fu, 0x57u, 0xb8u
};
uint8_t data2[] = {
0x5cu, 0x8au, 0x61u, 0xacu, 0x89u, 0x24u, 0x71u, 0x1fu
};
uint8_t data3[] = {
0x89u, 0x5cu, 0x5eu, 0xd9u, 0x0eu, 0xf1u, 0x77u, 0x45u,
0xedu, 0x2du, 0x72u, 0x8au, 0xbdu, 0x22u, 0xa5u, 0xf7u,
0xa1u, 0x34u, 0x79u, 0xa4u, 0x62u, 0xd7u, 0x1bu, 0x56u,
0xc1u, 0x9au, 0x74u, 0xa4u, 0x0bu, 0x65u, 0x5cu, 0x58u,
0xedu, 0xfeu, 0x0au, 0x18u, 0x8au, 0xd2u, 0xcfu, 0x46u,
0xcbu, 0xf3u, 0x05u, 0x24u, 0xf6u, 0x5du, 0x42u, 0x3cu,
0x83u, 0x7du, 0xd1u, 0xffu, 0x2bu, 0xf4u, 0x62u, 0xacu,
0x41u, 0x98u
};
uint8_t data4[] = {
0x00u, 0x73u, 0x45u, 0xbbu, 0x44u, 0xdbu,
0xb7u, 0xb1u, 0xc8u, 0x61u, 0x29u, 0x8cu, 0xdfu, 0x61u,
0x98u, 0x2au, 0x83u, 0x3au, 0xfcu, 0x72u, 0x8fu
};
uint8_t data5[] = {
0xaeu, 0x1eu, 0xdau, 0x2fu, 0x87u, 0xaau, 0x2cu, 0x94u, 0x80u,
0x85u, 0x8bu, 0xecu
};
/* Enable DMA interrupt and set callback */
interruptInit();
/* Set status of pooling variable to not executed */
sha2MultipartnonBlockingStatus_callback = MCUXCLHASH_STATUS_CALLBACK_NOT_EXECUTED;
/* Initialize session */
mcuxClSession_Descriptor_t sessionDesc;
mcuxClSession_Handle_t session = &sessionDesc;
/* Allocate and initialize session */
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION(
session,
MCUXCLRANDOM_NCINIT_WACPU_SIZE)),
0u);
/* Initialize the PRNG */
MCUXCLEXAMPLE_INITIALIZE_PRNG(session);
/* Configure the DMA channels that should be used. For Sha2 operations, the two channels will never be used at the same time.
* Use DMA channel 0 for HW input operations. */
mcuxClSession_Channels_t dmaChannels = {
.input = (mcuxClSession_Channel_t) 0u,
.output = (mcuxClSession_Channel_t) 0u
};
/* Set DMA channels and user callback function */
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClSession_Channels_t dmaChannels, */ dmaChannels,
/* mcuxClSession_Callback_t pUserCallback, */ user_callback,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_NULL_POINTER_CONSTANT("NULL is used in code")
/* void * pUserData */ NULL)
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_NULL_POINTER_CONSTANT()
);
/* Initialize resource context and add it to the session */
if(!mcuxClExample_Session_InitAndSetResourceCtx(session, resourceCtxHandle))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
uint32_t context[MCUXCLHASH_CONTEXT_SIZE_SHA2_256_IN_WORDS];
/* mcuxCLSession_Handle_t session: */ session,
/* mcuxClHash_Context_t context: */ (mcuxClHash_Context_t) context,
/* mcuxClHash_Algo_t algorithm: */ mcuxClHash_Algorithm_Sha256_Dma_NonBlocking
));
// mcuxClHash_init is a flow-protected function: Check the protection token and the return value
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUXCLBUFFER_INIT_DMA_RO(data1Buf, session, data1, sizeof(data1));
/* mcuxCLSession_Handle_t session: */ session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClHash_init")
/* mcuxClHash_Context_t context: */ (mcuxClHash_Context_t) context,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
/* mcuxCl_InputBuffer_t in: */ data1Buf,
/* uint32_t inSize: */ sizeof(data1)
));
// mcuxClHash_process is a flow-protected function: Check the protection token and the return value
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
{
/* A non-blocking job was started. Wait for the interrupt. */
while(MCUXCLHASH_FLAG_DMA_INTERRUPT_NOT_TRIGGERED == flag_interruptNumber) {};
/* Call the resource interrupt handler to finish the non-blocking operation.
* On normal operation flow, this will trigger the user_callback function at the end,
* which sets hashAPInonBlockingStatus_callback to the status code of the Hash operation.
* On error, mcuxClResource_handle_interrupt returns an ERROR code without triggering
* the user_callback. */
MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(rhi_status, rhi_token, mcuxClResource_handle_interrupt(resourceCtxHandle, flag_interruptNumber));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(MCUXCLHASH_STATUS_JOB_COMPLETED != sha2MultipartnonBlockingStatus_callback)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* Reset polling loop condition and the status code */
flag_interruptNumber = MCUXCLHASH_FLAG_DMA_INTERRUPT_NOT_TRIGGERED;
sha2MultipartnonBlockingStatus_callback = MCUXCLHASH_STATUS_CALLBACK_NOT_EXECUTED;
}
else
{
/* Entering here means that all operations executed successfully without starting non-blocking job,
Here no action is required and we can continue. */
}
MCUXCLBUFFER_INIT_DMA_RO(data2Buf, session, data2, sizeof(data2));
/* mcuxCLSession_Handle_t session: */ session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClHash_init")
/* mcuxClHash_Context_t context: */ (mcuxClHash_Context_t) context,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
/* mcuxCl_InputBuffer_t in: */ data2Buf,
/* uint32_t inSize: */ sizeof(data2)
));
// mcuxClHash_process is a flow-protected function: Check the protection token and the return value
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
{
/* A non-blocking job was started. Wait for the interrupt. */
while(MCUXCLHASH_FLAG_DMA_INTERRUPT_NOT_TRIGGERED == flag_interruptNumber) {};
/* Call the resource interrupt handler to finish the non-blocking operation.
* On normal operation flow, this will trigger the user_callback function at the end,
* which sets hashAPInonBlockingStatus_callback to the status code of the Hash operation.
* On error, mcuxClResource_handle_interrupt returns an ERROR code without triggering
* the user_callback. */
MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(rhi_status, rhi_token, mcuxClResource_handle_interrupt(resourceCtxHandle, flag_interruptNumber));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(MCUXCLHASH_STATUS_JOB_COMPLETED != sha2MultipartnonBlockingStatus_callback)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* Reset polling loop condition and the status code */
flag_interruptNumber = MCUXCLHASH_FLAG_DMA_INTERRUPT_NOT_TRIGGERED;
sha2MultipartnonBlockingStatus_callback = MCUXCLHASH_STATUS_CALLBACK_NOT_EXECUTED;
}
else
{
/* Entering here means that all operations executed successfully without starting non-blocking job,
Here no action is required and we can continue. */
}
MCUXCLBUFFER_INIT_DMA_RO(data3Buf, session, data3, sizeof(data3));
/* mcuxCLSession_Handle_t session: */ session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClHash_init")
/* mcuxClHash_Context_t context: */ (mcuxClHash_Context_t) context,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
/* mcuxCl_InputBuffer_t in: */ data3Buf,
/* uint32_t inSize: */ sizeof(data3)
));
// mcuxClHash_process is a flow-protected function: Check the protection token and the return value
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
{
/* A non-blocking job was started. Wait for the interrupt. */
while(MCUXCLHASH_FLAG_DMA_INTERRUPT_NOT_TRIGGERED == flag_interruptNumber) {};
/* Call the resource interrupt handler to finish the non-blocking operation.
* On normal operation flow, this will trigger the user_callback function at the end,
* which sets hashAPInonBlockingStatus_callback to the status code of the Hash operation.
* On error, mcuxClResource_handle_interrupt returns an ERROR code without triggering
* the user_callback. */
MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(rhi_status, rhi_token, mcuxClResource_handle_interrupt(resourceCtxHandle, flag_interruptNumber));
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(MCUXCLHASH_STATUS_JOB_COMPLETED != sha2MultipartnonBlockingStatus_callback)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* Reset polling loop condition and the status code */
flag_interruptNumber = MCUXCLHASH_FLAG_DMA_INTERRUPT_NOT_TRIGGERED;
sha2MultipartnonBlockingStatus_callback = MCUXCLHASH_STATUS_CALLBACK_NOT_EXECUTED;
}
else
{
/* Entering here means that all operations executed successfully without starting non-blocking job,
Here no action is required and we can continue. */
}
MCUXCLBUFFER_INIT_DMA_RO(data4Buf, session, data4, sizeof(data4));
/* mcuxCLSession_Handle_t session: */ session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClHash_init")
/* mcuxClHash_Context_t context: */ (mcuxClHash_Context_t) context,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
/* mcuxCl_InputBuffer_t in: */ data4Buf,
/* uint32_t inSize: */ sizeof(data4)
));
// mcuxClHash_process is a flow-protected function: Check the protection token and the return value
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
{
/* A non-blocking job was started. A polling loop is used to wait for the user callback. */
while(MCUXCLHASH_STATUS_CALLBACK_NOT_EXECUTED == sha2MultipartnonBlockingStatus_callback) {};
}
else
{
/* Entering here means that all operations executed successfully without starting non-blocking job,
Here no action is required and we can continue. */
}
MCUXCLBUFFER_INIT_DMA_RO(data5Buf, session, data5, sizeof(data5));
/* mcuxCLSession_Handle_t session: */ session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClHash_init")
/* mcuxClHash_Context_t context: */ (mcuxClHash_Context_t) context,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
/* mcuxCl_InputBuffer_t in: */ data5Buf,
/* uint32_t inSize: */ sizeof(data5)
));
// mcuxClHash_process is a flow-protected function: Check the protection token and the return value
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
{
/* A non-blocking job was started. A polling loop is used to wait for the user callback. */
while(MCUXCLHASH_STATUS_CALLBACK_NOT_EXECUTED == sha2MultipartnonBlockingStatus_callback) {};
}
else
{
/* Entering here means that all operations executed successfully without starting non-blocking job,
Here no action is required and we can continue. */
}
ALIGNED uint8_t hash[MCUXCLHASH_OUTPUT_SIZE_SHA_256];
uint32_t hashOutputSize = 0u;
MCUXCLBUFFER_INIT_DMA_RW(hashBuf, session, hash, sizeof(hash));
/* mcuxCLSession_Handle_t session: */ session,
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by mcuxClHash_init")
/* mcuxClHash_Context_t context: */ (mcuxClHash_Context_t) context,
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
/* mcuxCl_Buffer_t pOut */ hashBuf,
/* uint32_t *const pOutSize, */ &hashOutputSize
));
// mcuxClHash_finish is a flow-protected function: Check the protection token and the return value
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(sizeof(hash) != hashOutputSize)
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/**************************************************************************/
/* Verification */
/**************************************************************************/
for (size_t i = 0U; i < sizeof(hash); i++)
{
if (longHashExpected[i] != hash[i]) // Expect that the resulting hash matches our expected output
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
}
/**************************************************************************/
/* Session clean-up */
/**************************************************************************/
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* Disable the interrupts */
interruptUninit();
return MCUXCLEXAMPLE_STATUS_OK;
}
Definition of function identifiers for the flow protection mechanism.
Top-level include file for the mcuxClHash component.
Top-level include file for the mcuxClHashModes component.
Top-level include file for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.
#define MCUXCLRESOURCE_CONTEXT_SIZE
Size (in bytes) of mcuxClResource context.
Definition mcuxClResource_MemoryConsumption.h:24
#define MCUXCLBUFFER_INIT_DMA_RO(name, info, ptr, size)
Initialize an input buffer (mcuxCl_InputBuffer_t) with DMA handling.
Definition mcuxClBuffer.h:120
#define MCUXCLBUFFER_INIT_DMA_RW(name, info, ptr, size)
Initialize an input/output buffer (mcuxCl_Buffer_t) with DMA handling.
Definition mcuxClBuffer.h:139
#define MCUXCLHASH_STATUS_JOB_COMPLETED
Job started in coprocessor has completed successfully.
Definition mcuxClHash_Constants.h:46
#define MCUXCLHASH_STATUS_JOB_STARTED
There is ongoing job in coprocessor which will trigger user callback on exit.
Definition mcuxClHash_Constants.h:45
#define MCUXCLHASH_STATUS_OK
Hash operation successful.
Definition mcuxClHash_Constants.h:35
mcuxClHash_Status_t mcuxClHash_process(mcuxClSession_Handle_t session, mcuxClHash_Context_t pContext, mcuxCl_InputBuffer_t pIn, uint32_t inSize)
Multi-part Hash processing function.
mcuxClHash_Status_t mcuxClHash_init(mcuxClSession_Handle_t session, mcuxClHash_Context_t pContext, mcuxClHash_Algo_t algorithm)
Multi-part Hash initialization function.
mcuxClHash_Status_t mcuxClHash_finish(mcuxClSession_Handle_t session, mcuxClHash_Context_t pContext, mcuxCl_Buffer_t pOut, uint32_t *const pOutSize)
Multi-part Hash computation finalization function.
mcuxClHash_ContextDescriptor_t * mcuxClHash_Context_t
Hash Context type.
Definition mcuxClHash_Types.h:72
static mcuxClHash_Algo_t mcuxClHash_Algorithm_Sha256_Dma_NonBlocking
Sha-256 algorithm descriptor Sha-256 hash calculation using the Hash non-blocking functionality SGI.
Definition mcuxClHashModes_Algorithms.h:114
#define MCUXCLHASH_OUTPUT_SIZE_SHA_256
SHA-256 output size: 256 bit (32 bytes).
Definition mcuxClHashModes_Constants.h:38
mcuxClResource_Status_t mcuxClResource_handle_interrupt(const mcuxClResource_Context_t *pResourceCtx, mcuxClResource_Interrupt_t interrupt)
Resource interrupt handler.
struct mcuxClResource_Context mcuxClResource_Context_t
Resource context type.
Definition mcuxClResource_Types.h:47
#define MCUXCLRESOURCE_STATUS_OK
Resource operation successful.
Definition mcuxClResource_Types.h:82
mcuxClSession_Status_t mcuxClSession_configure_job(mcuxClSession_Handle_t session, mcuxClSession_Channels_t dmaChannels, mcuxClSession_Callback_t pUserCallback, void *pUserData)
Configure the parameters for non-blocking operations (jobs) in this session.
#define MCUXCLSESSION_STATUS_OK
Session operation successful.
Definition mcuxClSession_Types.h:39
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
uint16_t mcuxClSession_Channel_t
Session channel type.
Definition mcuxClSession_Types.h:105
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658
#define MCUXCLHASH_PROCESS_NONBLOCKING_CPU_WA_BUFFER_SIZE_SHA2_256
Defines the workarea size required for mcuxClHash_process on SHA2-256.
Definition mcuxClHashModes_MemoryConsumption.h:42
#define MCUXCLHASH_FINISH_NONBLOCKING_CPU_WA_BUFFER_SIZE_SHA2_256
Defines the workarea size required for mcuxClHash_finish on SHA2-256.
Definition mcuxClHashModes_MemoryConsumption.h:44
Session channels type.
Definition mcuxClSession_Types.h:113