Example for the mcuxClKey component.
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_Session_Helper.h>
#include <mcuxClExample_RNG_Helper.h>
static const uint8_t plain[64] = {
0x61U, 0x62U, 0x63U, 0x64U, 0x65U, 0x66U, 0x67U, 0x68U,
0x69U, 0x6aU, 0x6bU, 0x6cU, 0x6dU, 0x6eU, 0x6fU, 0x70U,
0x62U, 0x63U, 0x64U, 0x65U, 0x66U, 0x67U, 0x68U, 0x69U,
0x6aU, 0x6bU, 0x6cU, 0x6dU, 0x6eU, 0x6fU, 0x70U, 0x71U,
0x63U, 0x64U, 0x65U, 0x66U, 0x67U, 0x68U, 0x69U, 0x6aU,
0x6bU, 0x6cU, 0x6dU, 0x6eU, 0x6fU, 0x70U, 0x71U, 0x72U,
0x64U, 0x65U, 0x66U, 0x67U, 0x68U, 0x69U, 0x6aU, 0x6bU,
0x6cU, 0x6dU, 0x6eU, 0x6fU, 0x70U, 0x71U, 0x72U, 0x73U,
};
static const uint8_t iv[16] = {
0x7aU, 0x79U, 0x78U, 0x77U, 0x76U, 0x75U, 0x74U, 0x73U,
0x72U, 0x71U, 0x70U, 0x6fU, 0x6eU, 0x6dU, 0x6cU, 0x6bU
};
static const uint8_t encryptedRef[64] = {
0xd4U, 0x43U, 0xbcU, 0x95U, 0x30U, 0xe2U, 0x2eU, 0x9aU,
0xcbU, 0x18U, 0x04U, 0x51U, 0xd1U, 0x08U, 0x95U, 0x80U,
0xd6U, 0xfeU, 0x0aU, 0xe6U, 0xfbU, 0x13U, 0xbcU, 0xc1U,
0x8cU, 0x0aU, 0x5bU, 0x8aU, 0x1dU, 0x0fU, 0xceU, 0x55U,
0xc7U, 0xfcU, 0x1bU, 0xc6U, 0x4eU, 0x2dU, 0xf6U, 0x78U,
0x04U, 0x4cU, 0xdfU, 0xccU, 0x82U, 0x9eU, 0x24U, 0x59U,
0x99U, 0xcdU, 0x52U, 0xc1U, 0xb0U, 0x0eU, 0x9aU, 0x0eU,
0xceU, 0xa4U, 0xfdU, 0x3eU, 0xbeU, 0x3eU, 0x0aU, 0xa5U
};
0x00U, 0x11U, 0x22U, 0x33U, 0x44U, 0x55U, 0x66U, 0x77U,
0x88U, 0x99U, 0xaaU, 0xbbU, 0xccU, 0xddU, 0xeeU, 0xffU
};
MCUXCLEXAMPLE_FUNCTION(mcuxClKey_Load_Flush_Sgi_example)
{
mcuxClSession_Descriptor_t sessionDesc;
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION(session, MCUXCLEXAMPLE_MAX_WA(MCUXCLKEY_LOADCOPRO_CPU_WA_SIZE,
MCUXCLEXAMPLE_MAX_WA(MCUXCLCIPHER_AES_ENCRYPT_CPU_WA_BUFFER_SIZE, MCUXCLRANDOM_NCINIT_WACPU_SIZE)
), 0U);
MCUXCLEXAMPLE_INITIALIZE_PRNG(session);
uint32_t keyDesc[MCUXCLKEY_DESCRIPTOR_SIZE_IN_WORDS];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
session,
key,
keyBytes,
sizeof(keyBytes))
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
session,
key,
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
uint32_t encryptedSize = 0U;
uint8_t encryptedData[sizeof(encryptedRef)];
session,
key,
ivBuf,
sizeof(iv),
plainBuf,
sizeof(plain),
encryptedDataBuf,
&encryptedSize)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(encryptedSize != sizeof(encryptedRef))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by MCUXCLBUFFER_INIT")
if(!mcuxClCore_assertEqual(encryptedRef, encryptedData, sizeof(encryptedRef)))
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
session,
key)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
return MCUXCLEXAMPLE_STATUS_OK;
}
Top-level include file for the mcuxClAes component.
Top-level include file for the mcuxClBuffer component.
Top-level include file for the mcuxClCipher component.
Top-level include file for the mcuxClCipherModes component.
Definition of function identifiers for the flow protection mechanism.
Top-level include file for the mcuxClKey component.
Top-level include file for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.
#define MCUXCLAES_AES128_KEY_SIZE
AES-128 key size in bytes.
Definition mcuxClAes_Constants.h:40
static const mcuxClKey_Type_t mcuxClKey_Type_Aes128
Key type pointer for AES-128 based keys.
Definition mcuxClAes_KeyTypes.h:51
#define MCUXCLBUFFER_INIT(name, info, ptr, size)
Initialize an input/output buffer (mcuxCl_Buffer_t).
Definition mcuxClBuffer.h:67
#define MCUXCLBUFFER_INIT_RO(name, info, ptr, size)
Initialize an input buffer (mcuxCl_InputBuffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:84
#define MCUXCLCIPHER_STATUS_OK
Blocking operation finished successfully.
Definition mcuxClCipher_Constants.h:35
mcuxClCipher_Status_t mcuxClCipher_encrypt(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClCipher_Mode_t mode, mcuxCl_InputBuffer_t pIv, uint32_t ivLength, mcuxCl_InputBuffer_t pIn, uint32_t inLength, mcuxCl_Buffer_t pOut, uint32_t *const pOutLength)
One-shot encryption function.
static mcuxClCipher_Mode_t mcuxClCipher_Mode_AES_CBC_NoPadding
AES-CBC mode without padding.
Definition mcuxClCipherModes_Modes.h:199
#define MCUXCLKEY_STATUS_OK
Key operation successful.
Definition mcuxClKey_Constants.h:40
#define MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_2
SGI key slot 2.
Definition mcuxClKey_Constants.h:174
mcuxClKey_Status_t mcuxClKey_init(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClKey_Type_t type, const uint8_t *pKeyData, uint32_t keyDataLength)
Initializes a key handle.
mcuxClKey_Status_t mcuxClKey_flush(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key)
Flush key from destination which can be a key slot of coprocessor or memory buffer.
mcuxClKey_Status_t mcuxClKey_loadCopro(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, uint32_t loadOptions)
Load key into destination key slot of a coprocessor.
mcuxClKey_Descriptor_t *const mcuxClKey_Handle_t
Key handle type.
Definition mcuxClKey_Types.h:91
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658