MCUX CLNS
MCUX Crypto Library Normal Secure
Loading...
Searching...
No Matches
mcuxClKey_Unwrap_Rfc3394_Sgi_example.c

Example for the mcuxClKey component for RFC3394 key unwrap/load into an SGI key slot.

Example for the mcuxClKey component for RFC3394 key unwrap/load into an SGI key slot.

/*--------------------------------------------------------------------------*/
/* Copyright 2024-2025 NXP */
/* */
/* NXP Confidential and Proprietary. This software is owned or controlled */
/* by NXP and may only be used strictly in accordance with the applicable */
/* license terms. By expressly accepting such terms or by downloading, */
/* installing, activating and/or otherwise using the software, you are */
/* agreeing that you have read, and that you agree to comply with and are */
/* bound by, such license terms. If you do not agree to be bound by the */
/* applicable license terms, then you may not retain, install, activate or */
/* otherwise use the software. */
/*--------------------------------------------------------------------------*/
#include <mcuxClSession.h>
#include <mcuxClKey.h>
#include <mcuxClAes.h> // Interface to AES-related definitions and types
#include <mcuxClCipher.h> // Interface to the entire mcuxClCipher component
#include <mcuxClCipherModes.h> // Interface to the entire mcuxClCipherModes component
#include <mcuxClCore_FunctionIdentifiers.h> // Code flow protection
#include <mcuxClBuffer.h>
#include <mcuxClCore_Examples.h>
#include <mcuxClExample_Session_Helper.h>
#include <mcuxClExample_RNG_Helper.h>
// Test vectors are taken from https://datatracker.ietf.org/doc/html/rfc3394
static const uint8_t wrappedKeyData[MCUXCLAES_ENCODING_RFC3394_AES128_KEY_SIZE] = {
0x64U, 0xE8U, 0xC3U, 0xF9U, 0xCEU, 0x0FU, 0x5BU, 0xA2U,
0x63U, 0xE9U, 0x77U, 0x79U, 0x05U, 0x81U, 0x8AU, 0x2AU,
0x93U, 0xC8U, 0x19U, 0x1EU, 0x7DU, 0x6EU, 0x8AU, 0xE7U
};
static const uint8_t kwk256Data[MCUXCLAES_AES256_KEY_SIZE] = {
0x00U, 0x01U, 0x02U, 0x03U, 0x04U, 0x05U, 0x06U, 0x07U,
0x08U, 0x09U, 0x0AU, 0x0BU, 0x0CU, 0x0DU, 0x0EU, 0x0FU,
0x10U, 0x11U, 0x12U, 0x13U, 0x14U, 0x15U, 0x16U, 0x17U,
0x18U, 0x19U, 0x1AU, 0x1BU, 0x1CU, 0x1DU, 0x1EU, 0x1FU
};
/* CBC plain data */
static const uint8_t plain[64] = {
0x61U, 0x62U, 0x63U, 0x64U, 0x65U, 0x66U, 0x67U, 0x68U,
0x69U, 0x6aU, 0x6bU, 0x6cU, 0x6dU, 0x6eU, 0x6fU, 0x70U,
0x62U, 0x63U, 0x64U, 0x65U, 0x66U, 0x67U, 0x68U, 0x69U,
0x6aU, 0x6bU, 0x6cU, 0x6dU, 0x6eU, 0x6fU, 0x70U, 0x71U,
0x63U, 0x64U, 0x65U, 0x66U, 0x67U, 0x68U, 0x69U, 0x6aU,
0x6bU, 0x6cU, 0x6dU, 0x6eU, 0x6fU, 0x70U, 0x71U, 0x72U,
0x64U, 0x65U, 0x66U, 0x67U, 0x68U, 0x69U, 0x6aU, 0x6bU,
0x6cU, 0x6dU, 0x6eU, 0x6fU, 0x70U, 0x71U, 0x72U, 0x73U,
};
/* CBC IV */
static const uint8_t iv[16] = {
0x7aU, 0x79U, 0x78U, 0x77U, 0x76U, 0x75U, 0x74U, 0x73U,
0x72U, 0x71U, 0x70U, 0x6fU, 0x6eU, 0x6dU, 0x6cU, 0x6bU
};
/* CBC encrypted data - plain data encrypted with the expected unwrapped key material.
* Expected unwrapped key material: 00112233445566778899AABBCCDDEEFF */
static const uint8_t encryptedRef[64] = {
0xd4U, 0x43U, 0xbcU, 0x95U, 0x30U, 0xe2U, 0x2eU, 0x9aU,
0xcbU, 0x18U, 0x04U, 0x51U, 0xd1U, 0x08U, 0x95U, 0x80U,
0xd6U, 0xfeU, 0x0aU, 0xe6U, 0xfbU, 0x13U, 0xbcU, 0xc1U,
0x8cU, 0x0aU, 0x5bU, 0x8aU, 0x1dU, 0x0fU, 0xceU, 0x55U,
0xc7U, 0xfcU, 0x1bU, 0xc6U, 0x4eU, 0x2dU, 0xf6U, 0x78U,
0x04U, 0x4cU, 0xdfU, 0xccU, 0x82U, 0x9eU, 0x24U, 0x59U,
0x99U, 0xcdU, 0x52U, 0xc1U, 0xb0U, 0x0eU, 0x9aU, 0x0eU,
0xceU, 0xa4U, 0xfdU, 0x3eU, 0xbeU, 0x3eU, 0x0aU, 0xa5U
};
MCUXCLEXAMPLE_FUNCTION(mcuxClKey_Unwrap_Rfc3394_Sgi_example)
{
/**************************************************************************/
/* Preparation */
/**************************************************************************/
mcuxClSession_Descriptor_t sessionDesc;
mcuxClSession_Handle_t session = &sessionDesc;
/* Allocate and initialize session */
MCUXCLEXAMPLE_ALLOCATE_AND_INITIALIZE_SESSION(session, MCUXCLEXAMPLE_MAX_WA(MCUXCLKEY_LOADCOPRO_CPU_WA_SIZE,
MCUXCLEXAMPLE_MAX_WA(MCUXCLCIPHER_AES_ENCRYPT_CPU_WA_BUFFER_SIZE, MCUXCLRANDOM_NCINIT_WACPU_SIZE)
), 0U);
/* Initialize the PRNG */
MCUXCLEXAMPLE_INITIALIZE_PRNG(session);
/**************************************************************************/
/* Key Init and "load" the key-wrapping key */
/**************************************************************************/
uint32_t keyWrappingKeyDesc[MCUXCLKEY_DESCRIPTOR_SIZE_IN_WORDS];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
mcuxClKey_Handle_t keyWrappingKey = (mcuxClKey_Handle_t) &keyWrappingKeyDesc;
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClKey_Handle_t key: */ keyWrappingKey,
/* mcuxClKey_Type_t type: */ mcuxClKey_Type_Aes256,
/* uint8_t * pKeyData: */ kwk256Data,
/* uint32_t keyDataLength: */ sizeof(kwk256Data))
);
if((MCUX_CSSL_FP_FUNCTION_CALLED(mcuxClKey_init) != kiKwk_token) || (MCUXCLKEY_STATUS_OK != kiKwk_status))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClKey_Handle_t key: */ keyWrappingKey,
/* uint32_t loadOptions: */ MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_6)
);
if((MCUX_CSSL_FP_FUNCTION_CALLED(mcuxClKey_loadCopro) != klKwk_token) || (MCUXCLKEY_STATUS_OK != klKwk_status))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/**************************************************************************/
/* Key Init the wrapped key */
/**************************************************************************/
uint32_t wrappedKeyDesc[MCUXCLKEY_DESCRIPTOR_SIZE_IN_WORDS];
MCUX_CSSL_ANALYSIS_START_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
mcuxClKey_Handle_t wrappedKey = (mcuxClKey_Handle_t) &wrappedKeyDesc;
MCUX_CSSL_ANALYSIS_STOP_PATTERN_REINTERPRET_MEMORY_OF_OPAQUE_TYPES()
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClKey_Handle_t key: */ wrappedKey,
/* mcuxClKey_Type_t type: */ mcuxClKey_Type_Aes128,
/* uint8_t * pKeyData: */ wrappedKeyData,
/* uint32_t keyDataLength: */ sizeof(wrappedKeyData))
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClKey_Handle_t key: */ wrappedKey,
/* mcuxClKey_Encoding_t encoding: */ mcuxClAes_Encoding_Rfc3394,
/* const uint8_t * pAuxData: */ (uint8_t*) keyWrappingKeyDesc,
/* uint32_t auxDataLength: */ sizeof(keyWrappingKeyDesc))
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/**************************************************************************/
/* Key Unwrap using the mcuxClKey_loadCopro API */
/**************************************************************************/
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClKey_Handle_t key: */ wrappedKey,
/* uint32_t loadOptions: */ MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_UNWRAP)
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/**************************************************************************/
/* Crypto Operation */
/**************************************************************************/
/**************************************************************************/
/* Encryption */
/**************************************************************************/
uint32_t encryptedSize = 0U;
uint8_t encryptedData[sizeof(encryptedRef)];
MCUXCLBUFFER_INIT_RO(plainBuf, session, plain, sizeof(plain));
MCUXCLBUFFER_INIT_RO(ivBuf, session, iv, sizeof(iv));
MCUXCLBUFFER_INIT(encryptedDataBuf, session, encryptedData, sizeof(encryptedData));
/* mcuxClSession_Handle_t session: */ session,
/* const mcuxClKey_Handle_t key: */ wrappedKey,
/* mcuxClCipher_Mode_t mode: */ mcuxClCipher_Mode_AES_CBC_NoPadding,
/* mcuxCl_InputBuffer_t pIv: */ ivBuf,
/* uint32_t ivLength: */ sizeof(iv),
/* mcuxCl_InputBuffer_t pIn: */ plainBuf,
/* uint32_t inLength: */ sizeof(plain),
/* mcuxCl_Buffer_t pOut: */ encryptedDataBuf,
/* uint32_t * const outLength: */ &encryptedSize) /* only relevant in case of padding being used */
);
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/**************************************************************************/
/* Verification */
/**************************************************************************/
if(encryptedSize != sizeof(encryptedRef))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
MCUX_CSSL_ANALYSIS_START_SUPPRESS_ALREADY_INITIALIZED("Initialized by MCUXCLBUFFER_INIT")
if(!mcuxClCore_assertEqual(encryptedRef, encryptedData, sizeof(encryptedRef)))
MCUX_CSSL_ANALYSIS_STOP_SUPPRESS_ALREADY_INITIALIZED()
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/**************************************************************************/
/* Flush the loaded keys */
/**************************************************************************/
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClKey_Handle_t key: */ wrappedKey)
);
if((MCUX_CSSL_FP_FUNCTION_CALLED(mcuxClKey_flush) != kf1_token) || (MCUXCLKEY_STATUS_OK != kf1_status))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/* mcuxClSession_Handle_t session: */ session,
/* mcuxClKey_Handle_t key: */ keyWrappingKey)
);
if((MCUX_CSSL_FP_FUNCTION_CALLED(mcuxClKey_flush) != kf2_token) || (MCUXCLKEY_STATUS_OK != kf2_status))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
/**************************************************************************/
/* Destroy the current session */
/**************************************************************************/
if(!mcuxClExample_Session_Clean(session))
{
return MCUXCLEXAMPLE_STATUS_ERROR;
}
return MCUXCLEXAMPLE_STATUS_OK;
}
Top-level include file for the mcuxClAes component.
Top-level include file for the mcuxClBuffer component.
Top-level include file for the mcuxClCipher component.
Top-level include file for the mcuxClCipherModes component.
Definition of function identifiers for the flow protection mechanism.
Top-level include file for the mcuxClKey component.
Top-level include file for the mcuxClSession component.
Provides the API for the CSSL flow protection mechanism.
#define MCUXCLAES_ENCODING_RFC3394_AES128_KEY_SIZE
RFC3394 encoding of AES-128 key material, encoded key size in bytes.
Definition mcuxClAes_Constants.h:49
#define MCUXCLAES_AES256_KEY_SIZE
AES-256 key size in bytes.
Definition mcuxClAes_Constants.h:44
static const mcuxClKey_Encoding_t mcuxClAes_Encoding_Rfc3394
Key encoding for RFC3394 key wrap/unwrap.
Definition mcuxClAes_KeyEncodingMechanisms.h:47
static const mcuxClKey_Type_t mcuxClKey_Type_Aes256
Key type pointer for AES-256 based keys.
Definition mcuxClAes_KeyTypes.h:63
static const mcuxClKey_Type_t mcuxClKey_Type_Aes128
Key type pointer for AES-128 based keys.
Definition mcuxClAes_KeyTypes.h:51
#define MCUXCLBUFFER_INIT(name, info, ptr, size)
Initialize an input/output buffer (mcuxCl_Buffer_t).
Definition mcuxClBuffer.h:67
#define MCUXCLBUFFER_INIT_RO(name, info, ptr, size)
Initialize an input buffer (mcuxCl_InputBuffer_t) with plain CPU handling.
Definition mcuxClBuffer.h:84
#define MCUXCLCIPHER_STATUS_OK
Blocking operation finished successfully.
Definition mcuxClCipher_Constants.h:35
mcuxClCipher_Status_t mcuxClCipher_encrypt(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClCipher_Mode_t mode, mcuxCl_InputBuffer_t pIv, uint32_t ivLength, mcuxCl_InputBuffer_t pIn, uint32_t inLength, mcuxCl_Buffer_t pOut, uint32_t *const pOutLength)
One-shot encryption function.
static mcuxClCipher_Mode_t mcuxClCipher_Mode_AES_CBC_NoPadding
AES-CBC mode without padding.
Definition mcuxClCipherModes_Modes.h:199
#define MCUXCLKEY_STATUS_OK
Key operation successful.
Definition mcuxClKey_Constants.h:40
#define MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_UNWRAP
Sgi key slot containing an RFC3394 unwrapped key.
Definition mcuxClKey_Constants.h:181
#define MCUXCLKEY_LOADOPTION_SLOT_SGI_KEY_6
SGI key slot 6.
Definition mcuxClKey_Constants.h:178
mcuxClKey_Status_t mcuxClKey_init(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClKey_Type_t type, const uint8_t *pKeyData, uint32_t keyDataLength)
Initializes a key handle.
mcuxClKey_Status_t mcuxClKey_flush(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key)
Flush key from destination which can be a key slot of coprocessor or memory buffer.
mcuxClKey_Status_t mcuxClKey_loadCopro(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, uint32_t loadOptions)
Load key into destination key slot of a coprocessor.
mcuxClKey_Status_t mcuxClKey_setEncoding(mcuxClSession_Handle_t session, mcuxClKey_Handle_t key, mcuxClKey_Encoding_t encoding, const uint8_t *pAuxData, uint32_t auxDataLength)
Configures the encoding mechanism for the given key handle.
mcuxClKey_Descriptor_t *const mcuxClKey_Handle_t
Key handle type.
Definition mcuxClKey_Types.h:91
mcuxClSession_Descriptor_t *const mcuxClSession_Handle_t
Type for mcuxClSession Handle.
Definition mcuxClSession_Types.h:98
#define MCUX_CSSL_FP_FUNCTION_CALL_BEGIN(...)
Call a flow protected function and check the protection token.
Definition mcuxCsslFlowProtection.h:623
#define MCUX_CSSL_FP_FUNCTION_CALLED(...)
Expectation of a called function.
Definition mcuxCsslFlowProtection.h:777
#define MCUX_CSSL_FP_FUNCTION_CALL_END(...)
End a function call section started by MCUX_CSSL_FP_FUNCTION_CALL_BEGIN.
Definition mcuxCsslFlowProtection.h:658